最近、Atom IDE(まだC/C++サポートは無い模様)とかVisual Studio Code(C/C++サポートのプレビュー版は有る模様)とか、新しい開発環境が出て来ていますね。ルネサスCS+と連携させる方法を探してみたいですね。Google検索: Atom IDE site:マイナビニュースwww.google.co.jp/search?q=Atom+IDE+site%3Anews.mynavi.jpGoogle検索: Visual Studio Code site:マイナビニュースwww.google.co.jp/search?q=Visual+Studio+Code+site%3Anews.mynavi.jp[リンク]C/C++ for VS Code (Preview)code.visualstudio.com/docs/languages/cpp[案(当面)]・ ビルドはCS+のコマンドラインモードを使用する・ ビルドエラーメッセージパーサはVisual Studio Codeのソースを改造する・ もちろんCS+のコマンドラインモードでビルドした.absファイルはCS+のGUIモードでデバッグ可能・ e² studio同梱のrenesas_cc_converter.exeでCC-RXやCC-RLの.absファイルをGDBで読める.xファイルに変換可能・ e² studio同梱のe2-server-gdb.exeでGDBとE1/E2Lite等を接続可能・ Visual Studio CodeはGDBと接続可能(任意のGDBと接続可能かは分からないが少なくともARM GDBとは接続可能な模様)[案(将来)]・ Visual Studio CodeをルネサスCS+と接続出来れば、、、(出来ればGDBを介さずに、、、)・ Visual Studio CodeをルネサスCS+のmtpjファイル内のソース情報が読めるように改造出来れば、、、
こんにちは。NoMaYです。今回、主に以下の対応をしてみました。ファイル一式を以下のzipファイルに固めました。(ファイルの合わせ込み/修正でRX版も更新しました。)(1) GNURL78とLLVM-RL78に対応させた(1') CC-RL版とファイルを共通にしたので以下の画面コピーのようにVSCode上で“構成”を切り替えて下さい(2) VSCode上からCC-RLのヘルプファイルを開くタスクメニューを追加した(2') なおGNURL78時やLLVM-RL78時にもメニューが表示されてしまいますが、これらではメニューを実行しても何も起きませんvscode_helper_files_rl78_20211227.zipvscode_helper_files_rx_20211227.zip
Visual Studio MCU.elf ← 注: 実装上の事情でVisual Studio 2022の場合と同様な小細工のダミーファイルを追加しました.vscode/c_cpp_intellisense_helper.h.vscode/c_cpp_properties.json.vscode/launch.json.vscode/tasks.json.vscode/VSCode setup for e2 studio.launch.vscode/VSCode start and open this folder.launch.vscode/.script/build.bat.vscode/.script/build.ps1.vscode/.script/exec.bat.vscode/.script/gdb.bat.vscode/.script/gdbserver.bat.vscode/.script/gdb_custom_launch_setup.gdb.vscode/.script/gdb_setup.gdb.vscode/.script/inherit_environments.bat.vscode/.script/update_properties_json.bat
以下、今回のやり方でのVSCodeの画面コピーです。VSCode上で“構成”を切り替えて下さい以下、e2 studioやCC-RLの各種パス設定やプロジェクトの各種設定をまとめた.vscode/c_cpp_properties.jsonファイルの内容です。赤文字箇所がVSCode setup for e2 studio.launchの実行により更新されます。.vscode/c_cpp_properties.jsonCC-RL/GNURL78/LLVM-RL78用
{ // code.visualstudio.com/.../customize-default-settings-cpp // code.visualstudio.com/.../c-cpp-properties-schema-reference "configurations": [ { "name": "CC-RL", "includePath": [ "${env:TCINSTALL}\\inc\\**", "${env:PROJECT_ROOT}\\src\\**" ], "defines": [ ], "compilerPath": "", "cStandard": "c99", "intelliSenseMode": "windows-msvc-x86", "forcedInclude": [ ".vscode\\c_cpp_intellisense_helper.h" ] }, { "name": "GNURL78", "includePath": [ "${env:PROJECT_ROOT}\\src\\**" ], "defines": [ ], "compilerPath": "${env:TCINSTALL}\\bin\\rl78-elf-g++.exe", "compilerArgs": [ "-mg14 -mmul=g14" ], "cStandard": "gnu99", "cppStandard": "gnu++14", "intelliSenseMode": "linux-gcc-x86", "forcedInclude": [ ".vscode\\c_cpp_intellisense_helper.h" ] }, { "name": "LLVM-RL78", "includePath": [ "${env:PROJECT_ROOT}\\src\\**" ], "defines": [ ], "compilerPath": "${env:TCINSTALL}\\bin\\clang++.exe", "compilerArgs": [ "--target=rl78 -mcpu=s3 -frenesas-extensions" ], "cStandard": "gnu99", "cppStandard": "gnu++17", "intelliSenseMode": "windows-clang-x86", "forcedInclude": [ ".vscode\\c_cpp_intellisense_helper.h" ] } ], "env": { // Do not edit the following line if you use 'VSCode setup for e2 studio.launch' program. "PROJECT_NAME": "${workspaceFolderBaseName}", // // Do not edit the following two lines if you use 'VSCode setup for e2 studio.launch' program. "PROGRAM_NAME": "${env.PROJECT_NAME}", "PROGRAM_EXT": ".elf", // // Do not edit the following line if you use 'VSCode setup for e2 studio.launch' program. "E2STUDIO_WORKSPACE_FOLDER": "C:\\Renesas\\GitHubDesktop\\workspaces\\workspace_e2v202110", // "BUILD_CONFIG_RELEASE_NAME": "Release", // Reserved for future use. "BUILD_CONFIG_DEBUG_NAME": "HardwareDebug", // "DEBUG_CONFIG_HARDWAREDEBUG_NAME": "HardwareDebug", "DEBUG_CONFIG_HARDWAREDEBUG_LCFG": "${env.PROJECT_NAME} ${env.DEBUG_CONFIG_HARDWAREDEBUG_NAME}.launch", "DEBUG_CONFIG_HARDWAREDEBUG_SOPT": "-uComPort= COM9", "DEBUG_CONFIG_SIMULATORDEBUG_NAME": "RenesasSimDebug", "DEBUG_CONFIG_SIMULATORDEBUG_LCFG": "${env.PROJECT_NAME} ${env.DEBUG_CONFIG_SIMULATORDEBUG_NAME}.launch", "DEBUG_CONFIG_SIMULATORDEBUG_SOPT": "", // "PROJECT_ROOT": "${workspaceFolder}", "MAKE_OPTIONS": "-r -j8 -k", // // Do not edit the following five lines if you use 'VSCode setup for e2 studio.launch' program. "ECLIPSE_HOME": "C:\\Renesas\\e2studio64_v202110\\eclipse", "SUPPORT_AREA": "C:\\Renesas\\e2studio64\\SupportFiles\\.eclipse\\com.renesas.platform_1643561029", "PYTHONHOME": "${env.ECLIPSE_HOME}\\runtimes\\python\\2.7.12_x86", "TCINSTALL": "C:\\Renesas\\GCCLLVM\\LLVM-RL78\\10.0.0.202111", "TC_NAME": "LLVM-RL78", // "environment": "Renesas_R_CPUs" // Not used but for similarity to Visual Studio's 'CppProperties.json'. }, "version": 4}