2度目の投稿です。よろしくお願いします。
AWSへセルラー通信(MQTT/TLS)で計測データを定期的に送信するデバイス(Synergy-S7G2+BG96)を量産中です。'20年7月より9月に生産したすべてのデバイス(約500台)が正常にAWSへ接続出来ていたのですが,最近(ここ数週間)になってネットには繋がるがその後のAWS接続で失敗するデバイスが多数出ている状態です。成功するデバイスと失敗するデバイスが存在します。また,失敗したデバイスでも証明書を再発行することで接続出来るようになったデバイスもあります。本障害について同様の症状の確認情報や対策等の情報がありましたらご提供いただけると助かります。以上、よろしくお願いいたします。