こんにちは。NoMaYです。32ビットマイコンの新ファミリ、Arm Cortex-M搭載「RAファミリ」を発表、次世代IoT機器に求められる性能、セキュリティ、周辺機能の最適解を追求~フレキシブル・ソフトウェア・パッケージとArmエコシステムが、開発スピードを加速~www.renesas.com/jp/ja/about/press-center/news/2019/news20191008.html
こんにちは。NoMaYです。最近何度かGNUARMを触ったのですが、e2 studio上でダウンロード/インストールしていたので気付かなかったのですけれども、今はArm社がGNUARMを配布しているのですね。(メンテナンスは、どこが、しているのかな?サポートはコミュニティだけど、メンテナンスはArm社なのかな?)DownloadsArm GNU Toolchain is a community supported pre-built GNU compiler toolchain for Arm based CPUs.developer.arm.com/downloads/-/arm-gnu-toolchain-downloads「Arm GNU Toolchain releases consists of cross toolchains for the following host operating systems:● GNU/Linux ○ Available for x86_64 and AArch64 host architectures ○ Available for bare-metal and Linux targets● Windows ○ Available for x86 host architecture only (compatible with x86_64) ○ Available for bare-metal and Linux targets● macOS ○ Available for x86_64 host architecture only ○ Available for bare-metal targets onlySome releases are for specific toolchain variants and might not provide all the toolchain variants.Please download the correct toolchain variant that suits your development needs.」
> 今はArm社がGNUARMを配布しているのですね。launchpad.netで配布していたのはGCC7ぐらいまでなので、もう大分になりますね。