こんにちは。NoMaYです。32ビットマイコンの新ファミリ、Arm Cortex-M搭載「RAファミリ」を発表、次世代IoT機器に求められる性能、セキュリティ、周辺機能の最適解を追求~フレキシブル・ソフトウェア・パッケージとArmエコシステムが、開発スピードを加速~www.renesas.com/jp/ja/about/press-center/news/2019/news20191008.html
こんにちは。NoMaYです。こんなアプリケーションノートが出ていますね。Guidelines for Using the S Cache on the System BusPDFwww.renesas.com/jp/ja/document/apn/ra-family-guidelines-using-s-cache-system-bus「At the time of the release of this application project, the RA Family MCU groups that support the S Cache are RA6M5, RA6M4, RA6E1, RA6T2, and RA4M3.」「For other RA6 Series MCUs which do not have S Cache, they are provided with SRAMHS. Access to the SRAMHS is always no wait state.」ZIPwww.renesas.com/jp/ja/document/scd/ra-family-guidelines-using-s-cache-system-bus-sample-code[追記]探してみたら、こんなアプリケーションノートも出ていました。Getting Started with CoreMark BenchmarkingPDFwww.renesas.com/jp/ja/document/apn/getting-started-coremark-benchmarkingZIPwww.renesas.com/jp/ja/document/scd/getting-started-coremark-benchmarkingなお、対応コンパイラは以下の2つのようですので、他のコンパイラに関してはソース修正が必要かも知れません。● Arm Compiler 6.15● IAR Embedded Workbench v9.32.1