こんにちは。NoMaYです。「あなたの製品に0.5ドルの追加費用でBluetooth low energy機能を追加出来ますよ(量産規模が大きい場合)」という謳い文句が気になったので調べてみることにしました。ボチボチとやっていきます。他の皆さんからの情報提供も歓迎です。SmartBond DA14530 and DA14531The world’s smallest and lowest power Bluetooth 5.1 System-on-Chipwww.dialog-semiconductor.com/products/bluetooth-low-energy/da14530-and-da14531「The SmartBond TINYTM DA14530 and DA14531 are the Bluetooth® low energy solution to power the next 1 billion IoT devicesSmartBond TINYTM the world’s smallest and lowest power Bluetooth 5.1 System-on-Chip, brings down the cost of adding Bluetooth low energy in any system to $0.50 in high volumes.This awesome combination takes mobile connectivity to places previously out of reach, triggering a wave of a billion IoT devices, all with SmartBond TINY at the heart.」[追記]あれれっ、上の引用はウェブページを先月見た時のものですが、今見ると文言が変わっていますね。0.5ドルという文言が無くなっていますね、、、「The SmartBond TINYTM DA14530 and DA14531 are the Bluetooth® low energy solution to power the next 1 billion IoT devicesSmartBond TINYTM, the world’s smallest and lowest power Bluetooth 5.1 System-on-Chip, brings down the cost of adding Bluetooth low energy in any system and takes mobile connectivity to places previously out of reach, triggering a wave of a billion IoT devices, all with SmartBond TINY at the heart.」[余談]柴田CEOのDialog社についてのインタビュー記事Dialog買収でアナログの土壌整う「半導体は清々しい」、ルネサス柴田社長インタビューeetimes.itmedia.co.jp/ee/articles/2109/24/news045.html
こんにちは。NoMaYです。別製品ですけれども、こういうパンフレットが出ていますね。(すみません、スレッドが放置状態、ですけれども、、、)Ultra Low Power Wi-Fi® Solutionswww.renesas.com/jp/ja/document/gde/ultra-low-power-wi-fi-solutions「DA16200 SoCHighly Integrated Ultra Low Power Wi-Fi System on Chip (SoC)DA16200 ModulesFull Offload Highly Integrated Ultra Low Power Wi-Fi ModulesDA16600 Combo Wi-Fi + BLE ModulesFull Offload Highly Integrated Ultra Low Power ModulesWINNING COMBINATIONSAnalog + Power + Embedded Processing」
DAxx については英語のフォーラムで盛んにやり取りされているので質問がある時もそちらにされると良いと思いますよ。