Hello,
Since it is not possible to create posts in English community, I'm writing there.
I have project with Renesas RA4M2 processor that supports crypto hardware acceleration. Program needs to proceed some cryptographic functionality. For this reason I use MBED TLS library provided in sample files from Renesas site. Sample project uses MBED TLS version 2.25.0 while current version is 3.1.0.
I need to proceed some manipulations with certificate file parsing and I found that MBED TLS version 2.25.0 from Renesas site is different than in official MBET TLS git repository. Some files are just missing while other ones are changed.
For example MBED TLS 2.25.0 from Renesas does not have mbedtls_x509_crt_parse_file() function.
How to parse certificate files in MBED TLS 2.25.0 from Renesas?
Hello gedas,
Before you create a post, you have to join this group.
Some groups require join and some do not. RA group is a group that requires Join.
Please join RA group of Rulz-English as follows.
(1) Click "More" button on the right side of RA page.
(2) Select "Join", so you can join group.
Regards,