こんにちは。NoMaYです。いま2つ気になっています。(1) ICCRL78とLLVM-RL78(とGNURL78)でワーニングレベルを上げるとワーニングがとてもたくさん出る(2) RL78スマートコンフィグレータGUI上でオンチップデバッグトレースを使用する設定にしても予約RAM領域を空けていない
こんにちは。NoMaYです。e2 studio 2021-07でLLVM-RL78&C++&RL78スマートコンフィグレータという組み合わせのプロジェクトを試していて気付いたのですけれど、C++側のソースのインクルードパス設定に以下の画面コピーのようにr_bspとr_configのパスが無いですね。しかも、手作業で追加してもコード再生成するとe2 studioが強制的に削除してしまいますね。これには困惑してしまいます。問題点:(1) C++側のソースのインクルードパス設定にr_bspとr_configのパスが無い(2) 手作業で追加してもコード再生成するとe2 studioが強制的に削除してしまう以下、e2 studioの画面コピーです。C側のソースのインクルードパス設定にはr_bspとr_configのパスが有るC++側のソースのインクルードパス設定にはr_bspとr_configのパスが無い