IKUZOと申します、RX631のメモリプロテクションユニットの使用方法がわかりません、サンプルコードも探したのですが該当が無いようです、アドバイスをいただけませんでしょうか?
IKUZOさん、こんにちは。NoMaYです。昨日の時点では気付いてなかったのですが、先程、あっ、と気付いたことがあります。こちらで試そうとしていることには『アクセス例外が発生したことの確認』が含まれますよね。今のところ、発生していなければ絶対おかしいというレベルの『浮動小数点例外が発生したことの確認』さえ出来ないような事態となっています。ですので、浮動小数点例外の件が解決するまで、IKUZOさんの先程の件(14:09の件)は良いとしても、少なくとも浮動小数点例外の件と話が共通する部分については手を進めないよう、作業をより分けるように気を付けた方が良いと思われます。