こんにちは。NoMaYです。RXスマートコンフィグレータ(V2.0.0)でブロック転送を行うDMAソースを生成させようとして気付いたのですが、以下のGUIの画面コピーの通り設定した「転送回数」と「ブロック/リピートサイズ」の値がソースでは逆になっていると思います。プロジェクトのファイル一式issue_20190318_1.zipRXスマートコンフィグレータのGUIの画面生成されたソースConfig_DMAC0.c (抜粋)
void R_Config_DMAC0_Create(void){ /* Cancel DMAC/DTC module stop state in LPC */ MSTP(DMAC) = 0U; /* Disable DMAC interrupts */ IEN(DMAC,DMAC0I) = 0U; /* Disable DMAC0 transfer */ DMAC0.DMCNT.BIT.DTE = 0U;略 /* Set DMAC0 block size */ DMAC0.DMCRA = _00010001_DMAC0_DMCRA_COUNT; /* Set DMAC0 block transfer count */ DMAC0.DMCRB = _0003_DMAC0_DMCRB_BLK_RPT_COUNT;略 /* Enable DMAC activation */ DMAC.DMAST.BIT.DMST = 1U; R_Config_DMAC0_Create_UserInit();}
Config_DMAC0.h (抜粋)
#define _00000000_DMAC0_SRC_ADDR (0x00000000UL) /* Source address */#define _00000000_DMAC0_DST_ADDR (0x00000000UL) /* Destination address */#define _00010001_DMAC0_DMCRA_COUNT (0x00010001UL) /* Repeat or Block size */#define _0003_DMAC0_DMCRB_BLK_RPT_COUNT (0x0003U) /* Block transfer count */#define _0000_DMAC0_SRC_EXT_RPT_AREA (0x0000U) /* Source address extended repeat area */#define _0000_DMAC0_DST_EXT_RPT_AREA (0x0000U) /* Destination address extended repeat area */#define _00000000_DMAC0_OFFSET_VALUE (0x00000000UL) /* Offset register value */
こんにちは。NoMaYです。以下はバグではなくて、私が気付いた、RXスマートコンフィグレータのV2.5.0とV2.6.0の生成コードの相違に関する、他のユーザさんへのレポート(というより単に相違点の提示に過ぎないですが)です。src/smc_gen/general/r_smc_cgc.hV2.5.0 (CC-RX/GNURX/ICCRX)
/******************************************************************************Global functions******************************************************************************/void R_CGC_Create(void);void R_CGC_Create_UserInit();
V2.6.0 (CC-RX/GNURX/ICCRX)
/******************************************************************************Global functions******************************************************************************/void R_CGC_Create(void);void R_CGC_Create_UserInit(void);
src/smc_gen/general/r_smc_interrupt.cV2.5.0 (CC-RX/GNURX/ICCRX)
/******************************************************************************Includes******************************************************************************/#include "r_smc_interrupt.h"#include "platform.h"/******************************************************************************略******************************************************************************/void R_Interrupt_Create(void){ /* No fast interrupt and group settings have been configured in the Interrupts tab. */}
/******************************************************************************Pragma directive******************************************************************************//* Start user code for pragma. Do not edit comment generated here *//* End user code. Do not edit comment generated here *//******************************************************************************Includes******************************************************************************/#include "r_cg_macrodriver.h"#include "r_smc_interrupt.h"/* Start user code for include. Do not edit comment generated here *//* End user code. Do not edit comment generated here */#include "r_cg_userdefine.h"/******************************************************************************Global variables and functions******************************************************************************//* Start user code for global. Do not edit comment generated here *//* End user code. Do not edit comment generated here *//******************************************************************************略******************************************************************************/void R_Interrupt_Create(void){ /* No fast interrupt and group settings have been configured in the Interrupts tab. */}/* Start user code for adding. Do not edit comment generated here *//* End user code. Do not edit comment generated here */
src/smc_gen/general/r_smc_interrupt.h (SCFG側の設定は変えていません。リリースノートに関連しそうな記載がありました。)V2.5.0 (CC-RX/GNURX/ICCRX)
#define ICU_ICU_SWINT2_PRIORITY (_0F_ICU_PRIORITY_LEVEL15)#define ICU_ICU_SWINT_PRIORITY (_0F_ICU_PRIORITY_LEVEL15)
#define ICU_ICU_SWINT2_PRIORITY (_01_ICU_PRIORITY_LEVEL1)#define ICU_ICU_SWINT_PRIORITY (_01_ICU_PRIORITY_LEVEL1)
[関連リンク]ツールニュース【リビジョンアップ】 e² studio Smart Configuratorプラグイン V2.6.0, RXスマート・コンフィグレータ V2.6.0www.renesas.com/jp/ja/doc/toolnews/jpn/2020/r20ts0596jj0100-sctn.pdfリリースノートSmart Configurator for RX V2.6.0 リリースノートR20UT4487JS0260 Rev.2.60 2020.07.20www.renesas.com/jp/ja/doc/products/tool/doc/016/r20ut4487js0260-smartconfigurator.pdf製品ページスマート・コンフィグレータwww.renesas.com/jp/ja/products/software-tools/tools/solution-toolkit/smart-configurator.html[追記]実は以前から何となく思い始めていたのですが、RXスマートコンフィグレータ使用時でも、デバイス変更が(自分が思い込んでいたよりもずっと)簡単に出来るようになっているような気がします、、、Smart Configurator for RX V2.6.0 リリースノート「2.3.4 デバイス変更後の変更レポートに、端子および割り込み情報を追加デバイス変更後の変更レポートに端子および割り込みの変更情報が追加されました。」「2.3.8 ボードページのデバイス選択が、e2 studio のデバイス変更に移行デバイス変更は、スマートコンフィグレータのボードページから、e2 studio のデバイス変更ウィザードに移行されました。ボードページの“…”ボタンを押下すると、e2 studio のデバイス変更ウィザードが自動的に起動されます。」