こんにちは。NoMaYです。今、以下のスレッドに投稿しているのですけれども、派生ネタが思い浮かびましたので、またひとつ立ててみました。RXv3コアのレジスタ一括退避機能の使い方(Register Bank Save Function Usage)を調べてみるスレッドcommunity-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/9572/rxv3-register-bank-save-function-usage派生ネタ・ 以下のスレッドのやり方にてライブラリを作る・ 単にSETPSW Iする方式ではなく、IPLを操作した後にSETPSW Iする方式とする・ RXv3コアだけでなく、RXv1コアやRXv2コアでも動作するようにする・ 実用になるかどうかは未知数ですスレッドスマートコンフィグレータの自動生成をカスタマイズしたいcommunity-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/8248/thread/42690#42690MISPOさんのNORTiをRX SmartConfiguratorと一緒に使いたい場合の課題と対策を考察してみるスレッドcommunity-ja.renesas.com/cafe_rene/forums-groups/tools/f/forum21/8266/mispo-norti-rx-smartconfigurator/42873#42873
こんにちは。NoMaYです。まず、CC-RX版をひとつ作ってみました。以下、肝心な部分のソースとe2 studioでシミュレータデバッグ中の画面コピーです。(肝心な部分は他にはありません。)NestedIntLib.c
/* * NestedIntLib.c * * Created on: Dec 06, 2022 * Author: NoMaY * License: MIT */ #include "r_smc_entry.h" #include "NestedIntLib.h" static void (* const Int_Hook_Vectors[])(void); void NESTEDINTLIB_INT_HOOK_init(void) { set_intb((void *)Int_Hook_Vectors); } static void dummy_NESTEDINTLIB_INT_HOOK_init(void) { // To prevent developers from being misled regarding the following inline assemble errors. // E0552111:Symbol is undefined // E0552113:Symbol definition is not appropriate // E0552052:Addressing mode specifier is not appropriate // or various inline assemble errors for(;;); } // Convert `0xX` format --> `DD` format for CC-RX inline assembler. #if BSP_CFG_FIT_IPL_MAX >= 16 #error "BSP_CFG_FIT_IPL_MAX should be 0x0 - 0xF." #elif BSP_CFG_FIT_IPL_MAX == 15 #define _BSP_CFG_FIT_IPL_MAX 15 #elif BSP_CFG_FIT_IPL_MAX == 14 #define _BSP_CFG_FIT_IPL_MAX 14 #elif BSP_CFG_FIT_IPL_MAX == 13 #define _BSP_CFG_FIT_IPL_MAX 13 #elif BSP_CFG_FIT_IPL_MAX == 12 #define _BSP_CFG_FIT_IPL_MAX 12 #elif BSP_CFG_FIT_IPL_MAX == 11 #define _BSP_CFG_FIT_IPL_MAX 11 #elif BSP_CFG_FIT_IPL_MAX == 10 #define _BSP_CFG_FIT_IPL_MAX 10 #elif BSP_CFG_FIT_IPL_MAX == 9 #define _BSP_CFG_FIT_IPL_MAX 9 #elif BSP_CFG_FIT_IPL_MAX == 8 #define _BSP_CFG_FIT_IPL_MAX 8 #elif BSP_CFG_FIT_IPL_MAX == 7 #define _BSP_CFG_FIT_IPL_MAX 7 #elif BSP_CFG_FIT_IPL_MAX == 6 #define _BSP_CFG_FIT_IPL_MAX 6 #elif BSP_CFG_FIT_IPL_MAX == 5 #define _BSP_CFG_FIT_IPL_MAX 5 #elif BSP_CFG_FIT_IPL_MAX == 4 #define _BSP_CFG_FIT_IPL_MAX 4 #elif BSP_CFG_FIT_IPL_MAX == 3 #define _BSP_CFG_FIT_IPL_MAX 3 #elif BSP_CFG_FIT_IPL_MAX == 2 #define _BSP_CFG_FIT_IPL_MAX 2 #elif BSP_CFG_FIT_IPL_MAX == 1 #define _BSP_CFG_FIT_IPL_MAX 1 #elif BSP_CFG_FIT_IPL_MAX == 0 #define _BSP_CFG_FIT_IPL_MAX 0 #else #error "BSP_CFG_FIT_IPL_MAX should be 0x0 - 0xF." #endif #pragma inline_asm INT_COMMON_NESTEDINT_PERMIT static void INT_COMMON_NESTEDINT_PERMIT(void) { PUSH.L R15 MVFC PSW, R15 #ifdef __RXV3 BFMOVZ #24, #0, #4, R15, R15 #else SHLR #24, R5 AND #15, R5 #endif CMP #_BSP_CFG_FIT_IPL_MAX, R15 BGEU ?+ MVTIPL #_BSP_CFG_FIT_IPL_MAX ?: SETPSW I MOV.L 4[SP], R15 // address of hook_entry_XXX + 3 --> R15 ADD #(- (__$hook_entry___0 + 3) + TOPOF C$VECT), R15 // 3 = size of BSR.W MOV.L [R15], 4[SP] RTSD #4, R15-R15 // i.e. POP R15, JMP [SP+] } #pragma inline_asm INT_COMMON_NESTEDINT_NOT_PERMIT static void INT_COMMON_NESTEDINT_NOT_PERMIT(void) { XCHG [SP], R15 // address of hook_entry_XXX + 3 --> R15 ADD #(- (__$hook_entry___0 + 3) + TOPOF C$VECT), R15 // 3 = size of BSR.W MOV.L [R15], R15 XCHG [SP], R15 RTS // i.e. JMP [SP+] } #pragma inline_asm INT_ENTRY_NESTEDINT_PERMIT static void INT_ENTRY_NESTEDINT_PERMIT(void) { BSR.W __$INT_COMMON_NESTEDINT_PERMIT } #pragma inline_asm INT_ENTRY_NESTEDINT_NOT_PERMIT static void INT_ENTRY_NESTEDINT_NOT_PERMIT(void) { BSR.W __$INT_COMMON_NESTEDINT_NOT_PERMIT } // Documents // https://www.renesas.com/us/en/document/mas/rx-family-rxv1-instruction-set-architecture-users-manual-software-rev130 // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv2-instruction-set-architecture-users-manual-software // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv3-instruction-set-architecture-users-manual-software-rev100 // To prevent the symbol from being optimized out. void * const dummy_INT_COMMON_NESTEDINT_NOT_PERMIT = (void *)INT_COMMON_NESTEDINT_NOT_PERMIT; void * const dummy_INT_COMMON_NESTEDINT_PERMIT = (void *)INT_COMMON_NESTEDINT_PERMIT; // To prevent the section name symbol `C$VECT` from being optimized out. void * const dummy_VECTTBL = (void *)__sectop("C$VECT"); // To prevent a compile warning. void * const dummy2_NESTEDINTLIB_INT_HOOK_init = (void *)dummy_NESTEDINTLIB_INT_HOOK_init; // The code size of the following functions is just 4 bytes. // For NOT_PERMIT // 00000000 39rrrr W BSR.W __$INT_COMMON_NESTEDINT_NOT_PERMIT // 00000003 02 RTS // Not used. // For PERMIT // 00000000 39rrrr W BSR.W __$INT_COMMON_NESTEDINT_PERMIT // 00000003 02 RTS // Not used. #define _INT_ENTRY(sel) INT_ENTRY_NESTEDINT_##sel() #define INT_ENTRY(sel) _INT_ENTRY(sel) static void hook_entry___0(void) { INT_ENTRY(INTERRUPT___0); } static void hook_entry___1(void) { INT_ENTRY(INTERRUPT___1); } static void hook_entry___2(void) { INT_ENTRY(INTERRUPT___2); } static void hook_entry___3(void) { INT_ENTRY(INTERRUPT___3); } static void hook_entry___4(void) { INT_ENTRY(INTERRUPT___4); } static void hook_entry___5(void) { INT_ENTRY(INTERRUPT___5); } static void hook_entry___6(void) { INT_ENTRY(INTERRUPT___6); } static void hook_entry___7(void) { INT_ENTRY(INTERRUPT___7); } static void hook_entry___8(void) { INT_ENTRY(INTERRUPT___8); } static void hook_entry___9(void) { INT_ENTRY(INTERRUPT___9); } static void hook_entry__10(void) { INT_ENTRY(INTERRUPT__10); } static void hook_entry__11(void) { INT_ENTRY(INTERRUPT__11); } static void hook_entry__12(void) { INT_ENTRY(INTERRUPT__12); } static void hook_entry__13(void) { INT_ENTRY(INTERRUPT__13); } static void hook_entry__14(void) { INT_ENTRY(INTERRUPT__14); } static void hook_entry__15(void) { INT_ENTRY(INTERRUPT__15); } static void hook_entry__16(void) { INT_ENTRY(INTERRUPT__16); } static void hook_entry__17(void) { INT_ENTRY(INTERRUPT__17); } static void hook_entry__18(void) { INT_ENTRY(INTERRUPT__18); } static void hook_entry__19(void) { INT_ENTRY(INTERRUPT__19); } static void hook_entry__20(void) { INT_ENTRY(INTERRUPT__20); } static void hook_entry__21(void) { INT_ENTRY(INTERRUPT__21); } static void hook_entry__22(void) { INT_ENTRY(INTERRUPT__22); } static void hook_entry__23(void) { INT_ENTRY(INTERRUPT__23); } static void hook_entry__24(void) { INT_ENTRY(INTERRUPT__24); } static void hook_entry__25(void) { INT_ENTRY(INTERRUPT__25); } static void hook_entry__26(void) { INT_ENTRY(INTERRUPT__26); } static void hook_entry__27(void) { INT_ENTRY(INTERRUPT__27); } static void hook_entry__28(void) { INT_ENTRY(INTERRUPT__28); } static void hook_entry__29(void) { INT_ENTRY(INTERRUPT__29); } static void hook_entry__30(void) { INT_ENTRY(INTERRUPT__30); } static void hook_entry__31(void) { INT_ENTRY(INTERRUPT__31); } static void hook_entry__32(void) { INT_ENTRY(INTERRUPT__32); } static void hook_entry__33(void) { INT_ENTRY(INTERRUPT__33); } static void hook_entry__34(void) { INT_ENTRY(INTERRUPT__34); } static void hook_entry__35(void) { INT_ENTRY(INTERRUPT__35); } static void hook_entry__36(void) { INT_ENTRY(INTERRUPT__36); } static void hook_entry__37(void) { INT_ENTRY(INTERRUPT__37); } static void hook_entry__38(void) { INT_ENTRY(INTERRUPT__38); } static void hook_entry__39(void) { INT_ENTRY(INTERRUPT__39); } static void hook_entry__40(void) { INT_ENTRY(INTERRUPT__40); } static void hook_entry__41(void) { INT_ENTRY(INTERRUPT__41); } static void hook_entry__42(void) { INT_ENTRY(INTERRUPT__42); } static void hook_entry__43(void) { INT_ENTRY(INTERRUPT__43); } static void hook_entry__44(void) { INT_ENTRY(INTERRUPT__44); } static void hook_entry__45(void) { INT_ENTRY(INTERRUPT__45); } static void hook_entry__46(void) { INT_ENTRY(INTERRUPT__46); } static void hook_entry__47(void) { INT_ENTRY(INTERRUPT__47); } static void hook_entry__48(void) { INT_ENTRY(INTERRUPT__48); } static void hook_entry__49(void) { INT_ENTRY(INTERRUPT__49); } static void hook_entry__50(void) { INT_ENTRY(INTERRUPT__50); } static void hook_entry__51(void) { INT_ENTRY(INTERRUPT__51); } static void hook_entry__52(void) { INT_ENTRY(INTERRUPT__52); } static void hook_entry__53(void) { INT_ENTRY(INTERRUPT__53); } static void hook_entry__54(void) { INT_ENTRY(INTERRUPT__54); } static void hook_entry__55(void) { INT_ENTRY(INTERRUPT__55); } static void hook_entry__56(void) { INT_ENTRY(INTERRUPT__56); } static void hook_entry__57(void) { INT_ENTRY(INTERRUPT__57); } static void hook_entry__58(void) { INT_ENTRY(INTERRUPT__58); } static void hook_entry__59(void) { INT_ENTRY(INTERRUPT__59); } static void hook_entry__60(void) { INT_ENTRY(INTERRUPT__60); } static void hook_entry__61(void) { INT_ENTRY(INTERRUPT__61); } static void hook_entry__62(void) { INT_ENTRY(INTERRUPT__62); } static void hook_entry__63(void) { INT_ENTRY(INTERRUPT__63); } static void hook_entry__64(void) { INT_ENTRY(INTERRUPT__64); } static void hook_entry__65(void) { INT_ENTRY(INTERRUPT__65); } static void hook_entry__66(void) { INT_ENTRY(INTERRUPT__66); } static void hook_entry__67(void) { INT_ENTRY(INTERRUPT__67); } static void hook_entry__68(void) { INT_ENTRY(INTERRUPT__68); } static void hook_entry__69(void) { INT_ENTRY(INTERRUPT__69); } static void hook_entry__70(void) { INT_ENTRY(INTERRUPT__70); } static void hook_entry__71(void) { INT_ENTRY(INTERRUPT__71); } static void hook_entry__72(void) { INT_ENTRY(INTERRUPT__72); } static void hook_entry__73(void) { INT_ENTRY(INTERRUPT__73); } static void hook_entry__74(void) { INT_ENTRY(INTERRUPT__74); } static void hook_entry__75(void) { INT_ENTRY(INTERRUPT__75); } static void hook_entry__76(void) { INT_ENTRY(INTERRUPT__76); } static void hook_entry__77(void) { INT_ENTRY(INTERRUPT__77); } static void hook_entry__78(void) { INT_ENTRY(INTERRUPT__78); } static void hook_entry__79(void) { INT_ENTRY(INTERRUPT__79); } static void hook_entry__80(void) { INT_ENTRY(INTERRUPT__80); } static void hook_entry__81(void) { INT_ENTRY(INTERRUPT__81); } static void hook_entry__82(void) { INT_ENTRY(INTERRUPT__82); } static void hook_entry__83(void) { INT_ENTRY(INTERRUPT__83); } static void hook_entry__84(void) { INT_ENTRY(INTERRUPT__84); } static void hook_entry__85(void) { INT_ENTRY(INTERRUPT__85); } static void hook_entry__86(void) { INT_ENTRY(INTERRUPT__86); } static void hook_entry__87(void) { INT_ENTRY(INTERRUPT__87); } static void hook_entry__88(void) { INT_ENTRY(INTERRUPT__88); } static void hook_entry__89(void) { INT_ENTRY(INTERRUPT__89); } static void hook_entry__90(void) { INT_ENTRY(INTERRUPT__90); } static void hook_entry__91(void) { INT_ENTRY(INTERRUPT__91); } static void hook_entry__92(void) { INT_ENTRY(INTERRUPT__92); } static void hook_entry__93(void) { INT_ENTRY(INTERRUPT__93); } static void hook_entry__94(void) { INT_ENTRY(INTERRUPT__94); } static void hook_entry__95(void) { INT_ENTRY(INTERRUPT__95); } static void hook_entry__96(void) { INT_ENTRY(INTERRUPT__96); } static void hook_entry__97(void) { INT_ENTRY(INTERRUPT__97); } static void hook_entry__98(void) { INT_ENTRY(INTERRUPT__98); } static void hook_entry__99(void) { INT_ENTRY(INTERRUPT__99); } static void hook_entry_100(void) { INT_ENTRY(INTERRUPT_100); } static void hook_entry_101(void) { INT_ENTRY(INTERRUPT_101); } static void hook_entry_102(void) { INT_ENTRY(INTERRUPT_102); } static void hook_entry_103(void) { INT_ENTRY(INTERRUPT_103); } static void hook_entry_104(void) { INT_ENTRY(INTERRUPT_104); } static void hook_entry_105(void) { INT_ENTRY(INTERRUPT_105); } static void hook_entry_106(void) { INT_ENTRY(INTERRUPT_106); } static void hook_entry_107(void) { INT_ENTRY(INTERRUPT_107); } static void hook_entry_108(void) { INT_ENTRY(INTERRUPT_108); } static void hook_entry_109(void) { INT_ENTRY(INTERRUPT_109); } static void hook_entry_110(void) { INT_ENTRY(INTERRUPT_110); } static void hook_entry_111(void) { INT_ENTRY(INTERRUPT_111); } static void hook_entry_112(void) { INT_ENTRY(INTERRUPT_112); } static void hook_entry_113(void) { INT_ENTRY(INTERRUPT_113); } static void hook_entry_114(void) { INT_ENTRY(INTERRUPT_114); } static void hook_entry_115(void) { INT_ENTRY(INTERRUPT_115); } static void hook_entry_116(void) { INT_ENTRY(INTERRUPT_116); } static void hook_entry_117(void) { INT_ENTRY(INTERRUPT_117); } static void hook_entry_118(void) { INT_ENTRY(INTERRUPT_118); } static void hook_entry_119(void) { INT_ENTRY(INTERRUPT_119); } static void hook_entry_120(void) { INT_ENTRY(INTERRUPT_120); } static void hook_entry_121(void) { INT_ENTRY(INTERRUPT_121); } static void hook_entry_122(void) { INT_ENTRY(INTERRUPT_122); } static void hook_entry_123(void) { INT_ENTRY(INTERRUPT_123); } static void hook_entry_124(void) { INT_ENTRY(INTERRUPT_124); } static void hook_entry_125(void) { INT_ENTRY(INTERRUPT_125); } static void hook_entry_126(void) { INT_ENTRY(INTERRUPT_126); } static void hook_entry_127(void) { INT_ENTRY(INTERRUPT_127); } static void hook_entry_128(void) { INT_ENTRY(INTERRUPT_128); } static void hook_entry_129(void) { INT_ENTRY(INTERRUPT_129); } static void hook_entry_130(void) { INT_ENTRY(INTERRUPT_130); } static void hook_entry_131(void) { INT_ENTRY(INTERRUPT_131); } static void hook_entry_132(void) { INT_ENTRY(INTERRUPT_132); } static void hook_entry_133(void) { INT_ENTRY(INTERRUPT_133); } static void hook_entry_134(void) { INT_ENTRY(INTERRUPT_134); } static void hook_entry_135(void) { INT_ENTRY(INTERRUPT_135); } static void hook_entry_136(void) { INT_ENTRY(INTERRUPT_136); } static void hook_entry_137(void) { INT_ENTRY(INTERRUPT_137); } static void hook_entry_138(void) { INT_ENTRY(INTERRUPT_138); } static void hook_entry_139(void) { INT_ENTRY(INTERRUPT_139); } static void hook_entry_140(void) { INT_ENTRY(INTERRUPT_140); } static void hook_entry_141(void) { INT_ENTRY(INTERRUPT_141); } static void hook_entry_142(void) { INT_ENTRY(INTERRUPT_142); } static void hook_entry_143(void) { INT_ENTRY(INTERRUPT_143); } static void hook_entry_144(void) { INT_ENTRY(INTERRUPT_144); } static void hook_entry_145(void) { INT_ENTRY(INTERRUPT_145); } static void hook_entry_146(void) { INT_ENTRY(INTERRUPT_146); } static void hook_entry_147(void) { INT_ENTRY(INTERRUPT_147); } static void hook_entry_148(void) { INT_ENTRY(INTERRUPT_148); } static void hook_entry_149(void) { INT_ENTRY(INTERRUPT_149); } static void hook_entry_150(void) { INT_ENTRY(INTERRUPT_150); } static void hook_entry_151(void) { INT_ENTRY(INTERRUPT_151); } static void hook_entry_152(void) { INT_ENTRY(INTERRUPT_152); } static void hook_entry_153(void) { INT_ENTRY(INTERRUPT_153); } static void hook_entry_154(void) { INT_ENTRY(INTERRUPT_154); } static void hook_entry_155(void) { INT_ENTRY(INTERRUPT_155); } static void hook_entry_156(void) { INT_ENTRY(INTERRUPT_156); } static void hook_entry_157(void) { INT_ENTRY(INTERRUPT_157); } static void hook_entry_158(void) { INT_ENTRY(INTERRUPT_158); } static void hook_entry_159(void) { INT_ENTRY(INTERRUPT_159); } static void hook_entry_160(void) { INT_ENTRY(INTERRUPT_160); } static void hook_entry_161(void) { INT_ENTRY(INTERRUPT_161); } static void hook_entry_162(void) { INT_ENTRY(INTERRUPT_162); } static void hook_entry_163(void) { INT_ENTRY(INTERRUPT_163); } static void hook_entry_164(void) { INT_ENTRY(INTERRUPT_164); } static void hook_entry_165(void) { INT_ENTRY(INTERRUPT_165); } static void hook_entry_166(void) { INT_ENTRY(INTERRUPT_166); } static void hook_entry_167(void) { INT_ENTRY(INTERRUPT_167); } static void hook_entry_168(void) { INT_ENTRY(INTERRUPT_168); } static void hook_entry_169(void) { INT_ENTRY(INTERRUPT_169); } static void hook_entry_170(void) { INT_ENTRY(INTERRUPT_170); } static void hook_entry_171(void) { INT_ENTRY(INTERRUPT_171); } static void hook_entry_172(void) { INT_ENTRY(INTERRUPT_172); } static void hook_entry_173(void) { INT_ENTRY(INTERRUPT_173); } static void hook_entry_174(void) { INT_ENTRY(INTERRUPT_174); } static void hook_entry_175(void) { INT_ENTRY(INTERRUPT_175); } static void hook_entry_176(void) { INT_ENTRY(INTERRUPT_176); } static void hook_entry_177(void) { INT_ENTRY(INTERRUPT_177); } static void hook_entry_178(void) { INT_ENTRY(INTERRUPT_178); } static void hook_entry_179(void) { INT_ENTRY(INTERRUPT_179); } static void hook_entry_180(void) { INT_ENTRY(INTERRUPT_180); } static void hook_entry_181(void) { INT_ENTRY(INTERRUPT_181); } static void hook_entry_182(void) { INT_ENTRY(INTERRUPT_182); } static void hook_entry_183(void) { INT_ENTRY(INTERRUPT_183); } static void hook_entry_184(void) { INT_ENTRY(INTERRUPT_184); } static void hook_entry_185(void) { INT_ENTRY(INTERRUPT_185); } static void hook_entry_186(void) { INT_ENTRY(INTERRUPT_186); } static void hook_entry_187(void) { INT_ENTRY(INTERRUPT_187); } static void hook_entry_188(void) { INT_ENTRY(INTERRUPT_188); } static void hook_entry_189(void) { INT_ENTRY(INTERRUPT_189); } static void hook_entry_190(void) { INT_ENTRY(INTERRUPT_190); } static void hook_entry_191(void) { INT_ENTRY(INTERRUPT_191); } static void hook_entry_192(void) { INT_ENTRY(INTERRUPT_192); } static void hook_entry_193(void) { INT_ENTRY(INTERRUPT_193); } static void hook_entry_194(void) { INT_ENTRY(INTERRUPT_194); } static void hook_entry_195(void) { INT_ENTRY(INTERRUPT_195); } static void hook_entry_196(void) { INT_ENTRY(INTERRUPT_196); } static void hook_entry_197(void) { INT_ENTRY(INTERRUPT_197); } static void hook_entry_198(void) { INT_ENTRY(INTERRUPT_198); } static void hook_entry_199(void) { INT_ENTRY(INTERRUPT_199); } static void hook_entry_200(void) { INT_ENTRY(INTERRUPT_200); } static void hook_entry_201(void) { INT_ENTRY(INTERRUPT_201); } static void hook_entry_202(void) { INT_ENTRY(INTERRUPT_202); } static void hook_entry_203(void) { INT_ENTRY(INTERRUPT_203); } static void hook_entry_204(void) { INT_ENTRY(INTERRUPT_204); } static void hook_entry_205(void) { INT_ENTRY(INTERRUPT_205); } static void hook_entry_206(void) { INT_ENTRY(INTERRUPT_206); } static void hook_entry_207(void) { INT_ENTRY(INTERRUPT_207); } static void hook_entry_208(void) { INT_ENTRY(INTERRUPT_208); } static void hook_entry_209(void) { INT_ENTRY(INTERRUPT_209); } static void hook_entry_210(void) { INT_ENTRY(INTERRUPT_210); } static void hook_entry_211(void) { INT_ENTRY(INTERRUPT_211); } static void hook_entry_212(void) { INT_ENTRY(INTERRUPT_212); } static void hook_entry_213(void) { INT_ENTRY(INTERRUPT_213); } static void hook_entry_214(void) { INT_ENTRY(INTERRUPT_214); } static void hook_entry_215(void) { INT_ENTRY(INTERRUPT_215); } static void hook_entry_216(void) { INT_ENTRY(INTERRUPT_216); } static void hook_entry_217(void) { INT_ENTRY(INTERRUPT_217); } static void hook_entry_218(void) { INT_ENTRY(INTERRUPT_218); } static void hook_entry_219(void) { INT_ENTRY(INTERRUPT_219); } static void hook_entry_220(void) { INT_ENTRY(INTERRUPT_220); } static void hook_entry_221(void) { INT_ENTRY(INTERRUPT_221); } static void hook_entry_222(void) { INT_ENTRY(INTERRUPT_222); } static void hook_entry_223(void) { INT_ENTRY(INTERRUPT_223); } static void hook_entry_224(void) { INT_ENTRY(INTERRUPT_224); } static void hook_entry_225(void) { INT_ENTRY(INTERRUPT_225); } static void hook_entry_226(void) { INT_ENTRY(INTERRUPT_226); } static void hook_entry_227(void) { INT_ENTRY(INTERRUPT_227); } static void hook_entry_228(void) { INT_ENTRY(INTERRUPT_228); } static void hook_entry_229(void) { INT_ENTRY(INTERRUPT_229); } static void hook_entry_230(void) { INT_ENTRY(INTERRUPT_230); } static void hook_entry_231(void) { INT_ENTRY(INTERRUPT_231); } static void hook_entry_232(void) { INT_ENTRY(INTERRUPT_232); } static void hook_entry_233(void) { INT_ENTRY(INTERRUPT_233); } static void hook_entry_234(void) { INT_ENTRY(INTERRUPT_234); } static void hook_entry_235(void) { INT_ENTRY(INTERRUPT_235); } static void hook_entry_236(void) { INT_ENTRY(INTERRUPT_236); } static void hook_entry_237(void) { INT_ENTRY(INTERRUPT_237); } static void hook_entry_238(void) { INT_ENTRY(INTERRUPT_238); } static void hook_entry_239(void) { INT_ENTRY(INTERRUPT_239); } static void hook_entry_240(void) { INT_ENTRY(INTERRUPT_240); } static void hook_entry_241(void) { INT_ENTRY(INTERRUPT_241); } static void hook_entry_242(void) { INT_ENTRY(INTERRUPT_242); } static void hook_entry_243(void) { INT_ENTRY(INTERRUPT_243); } static void hook_entry_244(void) { INT_ENTRY(INTERRUPT_244); } static void hook_entry_245(void) { INT_ENTRY(INTERRUPT_245); } static void hook_entry_246(void) { INT_ENTRY(INTERRUPT_246); } static void hook_entry_247(void) { INT_ENTRY(INTERRUPT_247); } static void hook_entry_248(void) { INT_ENTRY(INTERRUPT_248); } static void hook_entry_249(void) { INT_ENTRY(INTERRUPT_249); } static void hook_entry_250(void) { INT_ENTRY(INTERRUPT_250); } static void hook_entry_251(void) { INT_ENTRY(INTERRUPT_251); } static void hook_entry_252(void) { INT_ENTRY(INTERRUPT_252); } static void hook_entry_253(void) { INT_ENTRY(INTERRUPT_253); } static void hook_entry_254(void) { INT_ENTRY(INTERRUPT_254); } static void hook_entry_255(void) { INT_ENTRY(INTERRUPT_255); } static void (* const Int_Hook_Vectors[])(void) = { (void (*)(void))hook_entry___0, (void (*)(void))hook_entry___1, (void (*)(void))hook_entry___2, (void (*)(void))hook_entry___3, (void (*)(void))hook_entry___4, (void (*)(void))hook_entry___5, (void (*)(void))hook_entry___6, (void (*)(void))hook_entry___7, (void (*)(void))hook_entry___8, (void (*)(void))hook_entry___9, (void (*)(void))hook_entry__10, (void (*)(void))hook_entry__11, (void (*)(void))hook_entry__12, (void (*)(void))hook_entry__13, (void (*)(void))hook_entry__14, (void (*)(void))hook_entry__15, (void (*)(void))hook_entry__16, (void (*)(void))hook_entry__17, (void (*)(void))hook_entry__18, (void (*)(void))hook_entry__19, (void (*)(void))hook_entry__20, (void (*)(void))hook_entry__21, (void (*)(void))hook_entry__22, (void (*)(void))hook_entry__23, (void (*)(void))hook_entry__24, (void (*)(void))hook_entry__25, (void (*)(void))hook_entry__26, (void (*)(void))hook_entry__27, (void (*)(void))hook_entry__28, (void (*)(void))hook_entry__29, (void (*)(void))hook_entry__30, (void (*)(void))hook_entry__31, (void (*)(void))hook_entry__32, (void (*)(void))hook_entry__33, (void (*)(void))hook_entry__34, (void (*)(void))hook_entry__35, (void (*)(void))hook_entry__36, (void (*)(void))hook_entry__37, (void (*)(void))hook_entry__38, (void (*)(void))hook_entry__39, (void (*)(void))hook_entry__40, (void (*)(void))hook_entry__41, (void (*)(void))hook_entry__42, (void (*)(void))hook_entry__43, (void (*)(void))hook_entry__44, (void (*)(void))hook_entry__45, (void (*)(void))hook_entry__46, (void (*)(void))hook_entry__47, (void (*)(void))hook_entry__48, (void (*)(void))hook_entry__49, (void (*)(void))hook_entry__50, (void (*)(void))hook_entry__51, (void (*)(void))hook_entry__52, (void (*)(void))hook_entry__53, (void (*)(void))hook_entry__54, (void (*)(void))hook_entry__55, (void (*)(void))hook_entry__56, (void (*)(void))hook_entry__57, (void (*)(void))hook_entry__58, (void (*)(void))hook_entry__59, (void (*)(void))hook_entry__60, (void (*)(void))hook_entry__61, (void (*)(void))hook_entry__62, (void (*)(void))hook_entry__63, (void (*)(void))hook_entry__64, (void (*)(void))hook_entry__65, (void (*)(void))hook_entry__66, (void (*)(void))hook_entry__67, (void (*)(void))hook_entry__68, (void (*)(void))hook_entry__69, (void (*)(void))hook_entry__70, (void (*)(void))hook_entry__71, (void (*)(void))hook_entry__72, (void (*)(void))hook_entry__73, (void (*)(void))hook_entry__74, (void (*)(void))hook_entry__75, (void (*)(void))hook_entry__76, (void (*)(void))hook_entry__77, (void (*)(void))hook_entry__78, (void (*)(void))hook_entry__79, (void (*)(void))hook_entry__80, (void (*)(void))hook_entry__81, (void (*)(void))hook_entry__82, (void (*)(void))hook_entry__83, (void (*)(void))hook_entry__84, (void (*)(void))hook_entry__85, (void (*)(void))hook_entry__86, (void (*)(void))hook_entry__87, (void (*)(void))hook_entry__88, (void (*)(void))hook_entry__89, (void (*)(void))hook_entry__90, (void (*)(void))hook_entry__91, (void (*)(void))hook_entry__92, (void (*)(void))hook_entry__93, (void (*)(void))hook_entry__94, (void (*)(void))hook_entry__95, (void (*)(void))hook_entry__96, (void (*)(void))hook_entry__97, (void (*)(void))hook_entry__98, (void (*)(void))hook_entry__99, (void (*)(void))hook_entry_100, (void (*)(void))hook_entry_101, (void (*)(void))hook_entry_102, (void (*)(void))hook_entry_103, (void (*)(void))hook_entry_104, (void (*)(void))hook_entry_105, (void (*)(void))hook_entry_106, (void (*)(void))hook_entry_107, (void (*)(void))hook_entry_108, (void (*)(void))hook_entry_109, (void (*)(void))hook_entry_110, (void (*)(void))hook_entry_111, (void (*)(void))hook_entry_112, (void (*)(void))hook_entry_113, (void (*)(void))hook_entry_114, (void (*)(void))hook_entry_115, (void (*)(void))hook_entry_116, (void (*)(void))hook_entry_117, (void (*)(void))hook_entry_118, (void (*)(void))hook_entry_119, (void (*)(void))hook_entry_120, (void (*)(void))hook_entry_121, (void (*)(void))hook_entry_122, (void (*)(void))hook_entry_123, (void (*)(void))hook_entry_124, (void (*)(void))hook_entry_125, (void (*)(void))hook_entry_126, (void (*)(void))hook_entry_127, (void (*)(void))hook_entry_128, (void (*)(void))hook_entry_129, (void (*)(void))hook_entry_130, (void (*)(void))hook_entry_131, (void (*)(void))hook_entry_132, (void (*)(void))hook_entry_133, (void (*)(void))hook_entry_134, (void (*)(void))hook_entry_135, (void (*)(void))hook_entry_136, (void (*)(void))hook_entry_137, (void (*)(void))hook_entry_138, (void (*)(void))hook_entry_139, (void (*)(void))hook_entry_140, (void (*)(void))hook_entry_141, (void (*)(void))hook_entry_142, (void (*)(void))hook_entry_143, (void (*)(void))hook_entry_144, (void (*)(void))hook_entry_145, (void (*)(void))hook_entry_146, (void (*)(void))hook_entry_147, (void (*)(void))hook_entry_148, (void (*)(void))hook_entry_149, (void (*)(void))hook_entry_150, (void (*)(void))hook_entry_151, (void (*)(void))hook_entry_152, (void (*)(void))hook_entry_153, (void (*)(void))hook_entry_154, (void (*)(void))hook_entry_155, (void (*)(void))hook_entry_156, (void (*)(void))hook_entry_157, (void (*)(void))hook_entry_158, (void (*)(void))hook_entry_159, (void (*)(void))hook_entry_160, (void (*)(void))hook_entry_161, (void (*)(void))hook_entry_162, (void (*)(void))hook_entry_163, (void (*)(void))hook_entry_164, (void (*)(void))hook_entry_165, (void (*)(void))hook_entry_166, (void (*)(void))hook_entry_167, (void (*)(void))hook_entry_168, (void (*)(void))hook_entry_169, (void (*)(void))hook_entry_170, (void (*)(void))hook_entry_171, (void (*)(void))hook_entry_172, (void (*)(void))hook_entry_173, (void (*)(void))hook_entry_174, (void (*)(void))hook_entry_175, (void (*)(void))hook_entry_176, (void (*)(void))hook_entry_177, (void (*)(void))hook_entry_178, (void (*)(void))hook_entry_179, (void (*)(void))hook_entry_180, (void (*)(void))hook_entry_181, (void (*)(void))hook_entry_182, (void (*)(void))hook_entry_183, (void (*)(void))hook_entry_184, (void (*)(void))hook_entry_185, (void (*)(void))hook_entry_186, (void (*)(void))hook_entry_187, (void (*)(void))hook_entry_188, (void (*)(void))hook_entry_189, (void (*)(void))hook_entry_190, (void (*)(void))hook_entry_191, (void (*)(void))hook_entry_192, (void (*)(void))hook_entry_193, (void (*)(void))hook_entry_194, (void (*)(void))hook_entry_195, (void (*)(void))hook_entry_196, (void (*)(void))hook_entry_197, (void (*)(void))hook_entry_198, (void (*)(void))hook_entry_199, (void (*)(void))hook_entry_200, (void (*)(void))hook_entry_201, (void (*)(void))hook_entry_202, (void (*)(void))hook_entry_203, (void (*)(void))hook_entry_204, (void (*)(void))hook_entry_205, (void (*)(void))hook_entry_206, (void (*)(void))hook_entry_207, (void (*)(void))hook_entry_208, (void (*)(void))hook_entry_209, (void (*)(void))hook_entry_210, (void (*)(void))hook_entry_211, (void (*)(void))hook_entry_212, (void (*)(void))hook_entry_213, (void (*)(void))hook_entry_214, (void (*)(void))hook_entry_215, (void (*)(void))hook_entry_216, (void (*)(void))hook_entry_217, (void (*)(void))hook_entry_218, (void (*)(void))hook_entry_219, (void (*)(void))hook_entry_220, (void (*)(void))hook_entry_221, (void (*)(void))hook_entry_222, (void (*)(void))hook_entry_223, (void (*)(void))hook_entry_224, (void (*)(void))hook_entry_225, (void (*)(void))hook_entry_226, (void (*)(void))hook_entry_227, (void (*)(void))hook_entry_228, (void (*)(void))hook_entry_229, (void (*)(void))hook_entry_230, (void (*)(void))hook_entry_231, (void (*)(void))hook_entry_232, (void (*)(void))hook_entry_233, (void (*)(void))hook_entry_234, (void (*)(void))hook_entry_235, (void (*)(void))hook_entry_236, (void (*)(void))hook_entry_237, (void (*)(void))hook_entry_238, (void (*)(void))hook_entry_239, (void (*)(void))hook_entry_240, (void (*)(void))hook_entry_241, (void (*)(void))hook_entry_242, (void (*)(void))hook_entry_243, (void (*)(void))hook_entry_244, (void (*)(void))hook_entry_245, (void (*)(void))hook_entry_246, (void (*)(void))hook_entry_247, (void (*)(void))hook_entry_248, (void (*)(void))hook_entry_249, (void (*)(void))hook_entry_250, (void (*)(void))hook_entry_251, (void (*)(void))hook_entry_252, (void (*)(void))hook_entry_253, (void (*)(void))hook_entry_254, (void (*)(void))hook_entry_255 };
/* * NestedIntLib.h * * Created on: Dec 06, 2022 * Author: NoMaY * License: MIT */ #ifndef NESTEDINTLIB_H_ #define NESTEDINTLIB_H_ #define INTERRUPT___0 PERMIT #define INTERRUPT___1 PERMIT #define INTERRUPT___2 PERMIT #define INTERRUPT___3 PERMIT #define INTERRUPT___4 PERMIT #define INTERRUPT___5 PERMIT #define INTERRUPT___6 PERMIT #define INTERRUPT___7 PERMIT #define INTERRUPT___8 PERMIT #define INTERRUPT___9 PERMIT #define INTERRUPT__10 PERMIT #define INTERRUPT__11 PERMIT #define INTERRUPT__12 PERMIT #define INTERRUPT__13 PERMIT #define INTERRUPT__14 PERMIT #define INTERRUPT__15 PERMIT #define INTERRUPT__16 NOT_PERMIT // bus_error_isr #define INTERRUPT__17 PERMIT #define INTERRUPT__18 PERMIT #define INTERRUPT__19 PERMIT #define INTERRUPT__20 PERMIT #define INTERRUPT__21 PERMIT #define INTERRUPT__22 PERMIT #define INTERRUPT__23 PERMIT #define INTERRUPT__24 PERMIT #define INTERRUPT__25 PERMIT #define INTERRUPT__26 PERMIT #define INTERRUPT__27 PERMIT #define INTERRUPT__28 PERMIT #define INTERRUPT__29 PERMIT #define INTERRUPT__30 PERMIT #define INTERRUPT__31 PERMIT #define INTERRUPT__32 PERMIT #define INTERRUPT__33 PERMIT #define INTERRUPT__34 PERMIT #define INTERRUPT__35 PERMIT #define INTERRUPT__36 PERMIT #define INTERRUPT__37 PERMIT #define INTERRUPT__38 PERMIT #define INTERRUPT__39 PERMIT #define INTERRUPT__40 PERMIT #define INTERRUPT__41 PERMIT #define INTERRUPT__42 PERMIT #define INTERRUPT__43 PERMIT #define INTERRUPT__44 PERMIT #define INTERRUPT__45 PERMIT #define INTERRUPT__46 PERMIT #define INTERRUPT__47 PERMIT #define INTERRUPT__48 PERMIT #define INTERRUPT__49 PERMIT #define INTERRUPT__50 PERMIT #define INTERRUPT__51 PERMIT #define INTERRUPT__52 PERMIT #define INTERRUPT__53 PERMIT #define INTERRUPT__54 PERMIT #define INTERRUPT__55 PERMIT #define INTERRUPT__56 PERMIT #define INTERRUPT__57 PERMIT #define INTERRUPT__58 PERMIT #define INTERRUPT__59 PERMIT #define INTERRUPT__60 PERMIT #define INTERRUPT__61 PERMIT #define INTERRUPT__62 PERMIT #define INTERRUPT__63 PERMIT #define INTERRUPT__64 PERMIT #define INTERRUPT__65 PERMIT #define INTERRUPT__66 PERMIT #define INTERRUPT__67 PERMIT #define INTERRUPT__68 PERMIT #define INTERRUPT__69 PERMIT #define INTERRUPT__70 PERMIT #define INTERRUPT__71 PERMIT #define INTERRUPT__72 PERMIT #define INTERRUPT__73 PERMIT #define INTERRUPT__74 PERMIT #define INTERRUPT__75 PERMIT #define INTERRUPT__76 PERMIT #define INTERRUPT__77 PERMIT #define INTERRUPT__78 PERMIT #define INTERRUPT__79 PERMIT #define INTERRUPT__80 PERMIT #define INTERRUPT__81 PERMIT #define INTERRUPT__82 PERMIT #define INTERRUPT__83 PERMIT #define INTERRUPT__84 PERMIT #define INTERRUPT__85 PERMIT #define INTERRUPT__86 PERMIT #define INTERRUPT__87 PERMIT #define INTERRUPT__88 PERMIT #define INTERRUPT__89 PERMIT #define INTERRUPT__90 PERMIT #define INTERRUPT__91 PERMIT #define INTERRUPT__92 PERMIT #define INTERRUPT__93 PERMIT #define INTERRUPT__94 PERMIT #define INTERRUPT__95 PERMIT #define INTERRUPT__96 PERMIT #define INTERRUPT__97 PERMIT #define INTERRUPT__98 PERMIT #define INTERRUPT__99 PERMIT #define INTERRUPT_100 PERMIT #define INTERRUPT_101 PERMIT #define INTERRUPT_102 PERMIT #define INTERRUPT_103 PERMIT #define INTERRUPT_104 PERMIT #define INTERRUPT_105 PERMIT #define INTERRUPT_106 PERMIT #define INTERRUPT_107 PERMIT #define INTERRUPT_108 PERMIT #define INTERRUPT_109 PERMIT #define INTERRUPT_110 PERMIT #define INTERRUPT_111 PERMIT #define INTERRUPT_112 PERMIT #define INTERRUPT_113 PERMIT #define INTERRUPT_114 PERMIT #define INTERRUPT_115 PERMIT #define INTERRUPT_116 PERMIT #define INTERRUPT_117 PERMIT #define INTERRUPT_118 PERMIT #define INTERRUPT_119 PERMIT #define INTERRUPT_120 PERMIT #define INTERRUPT_121 PERMIT #define INTERRUPT_122 PERMIT #define INTERRUPT_123 PERMIT #define INTERRUPT_124 PERMIT #define INTERRUPT_125 PERMIT #define INTERRUPT_126 PERMIT #define INTERRUPT_127 PERMIT #define INTERRUPT_128 PERMIT #define INTERRUPT_129 PERMIT #define INTERRUPT_130 PERMIT #define INTERRUPT_131 PERMIT #define INTERRUPT_132 PERMIT #define INTERRUPT_133 PERMIT #define INTERRUPT_134 PERMIT #define INTERRUPT_135 PERMIT #define INTERRUPT_136 PERMIT #define INTERRUPT_137 PERMIT #define INTERRUPT_138 PERMIT #define INTERRUPT_139 PERMIT #define INTERRUPT_140 PERMIT #define INTERRUPT_141 PERMIT #define INTERRUPT_142 PERMIT #define INTERRUPT_143 PERMIT #define INTERRUPT_144 PERMIT #define INTERRUPT_145 PERMIT #define INTERRUPT_146 PERMIT #define INTERRUPT_147 PERMIT #define INTERRUPT_148 PERMIT #define INTERRUPT_149 PERMIT #define INTERRUPT_150 PERMIT #define INTERRUPT_151 PERMIT #define INTERRUPT_152 PERMIT #define INTERRUPT_153 PERMIT #define INTERRUPT_154 PERMIT #define INTERRUPT_155 PERMIT #define INTERRUPT_156 PERMIT #define INTERRUPT_157 PERMIT #define INTERRUPT_158 PERMIT #define INTERRUPT_159 PERMIT #define INTERRUPT_160 PERMIT #define INTERRUPT_161 PERMIT #define INTERRUPT_162 PERMIT #define INTERRUPT_163 PERMIT #define INTERRUPT_164 PERMIT #define INTERRUPT_165 PERMIT #define INTERRUPT_166 PERMIT #define INTERRUPT_167 PERMIT #define INTERRUPT_168 PERMIT #define INTERRUPT_169 PERMIT #define INTERRUPT_170 PERMIT #define INTERRUPT_171 PERMIT #define INTERRUPT_172 PERMIT #define INTERRUPT_173 PERMIT #define INTERRUPT_174 PERMIT #define INTERRUPT_175 PERMIT #define INTERRUPT_176 PERMIT #define INTERRUPT_177 PERMIT #define INTERRUPT_178 PERMIT #define INTERRUPT_179 PERMIT #define INTERRUPT_180 PERMIT #define INTERRUPT_181 PERMIT #define INTERRUPT_182 PERMIT #define INTERRUPT_183 PERMIT #define INTERRUPT_184 PERMIT #define INTERRUPT_185 PERMIT #define INTERRUPT_186 PERMIT #define INTERRUPT_187 PERMIT #define INTERRUPT_188 PERMIT #define INTERRUPT_189 PERMIT #define INTERRUPT_190 PERMIT #define INTERRUPT_191 PERMIT #define INTERRUPT_192 PERMIT #define INTERRUPT_193 PERMIT #define INTERRUPT_194 PERMIT #define INTERRUPT_195 PERMIT #define INTERRUPT_196 PERMIT #define INTERRUPT_197 PERMIT #define INTERRUPT_198 PERMIT #define INTERRUPT_199 PERMIT #define INTERRUPT_200 PERMIT #define INTERRUPT_201 PERMIT #define INTERRUPT_202 PERMIT #define INTERRUPT_203 PERMIT #define INTERRUPT_204 PERMIT #define INTERRUPT_205 PERMIT #define INTERRUPT_206 PERMIT #define INTERRUPT_207 PERMIT #define INTERRUPT_208 PERMIT #define INTERRUPT_209 PERMIT #define INTERRUPT_210 PERMIT #define INTERRUPT_211 PERMIT #define INTERRUPT_212 PERMIT #define INTERRUPT_213 PERMIT #define INTERRUPT_214 PERMIT #define INTERRUPT_215 PERMIT #define INTERRUPT_216 PERMIT #define INTERRUPT_217 PERMIT #define INTERRUPT_218 PERMIT #define INTERRUPT_219 PERMIT #define INTERRUPT_220 PERMIT #define INTERRUPT_221 PERMIT #define INTERRUPT_222 PERMIT #define INTERRUPT_223 PERMIT #define INTERRUPT_224 PERMIT #define INTERRUPT_225 PERMIT #define INTERRUPT_226 PERMIT #define INTERRUPT_227 PERMIT #define INTERRUPT_228 PERMIT #define INTERRUPT_229 PERMIT #define INTERRUPT_230 PERMIT #define INTERRUPT_231 PERMIT #define INTERRUPT_232 PERMIT #define INTERRUPT_233 PERMIT #define INTERRUPT_234 PERMIT #define INTERRUPT_235 PERMIT #define INTERRUPT_236 PERMIT #define INTERRUPT_237 PERMIT #define INTERRUPT_238 PERMIT #define INTERRUPT_239 PERMIT #define INTERRUPT_240 PERMIT #define INTERRUPT_241 PERMIT #define INTERRUPT_242 PERMIT #define INTERRUPT_243 PERMIT #define INTERRUPT_244 PERMIT #define INTERRUPT_245 PERMIT #define INTERRUPT_246 PERMIT #define INTERRUPT_247 PERMIT #define INTERRUPT_248 PERMIT #define INTERRUPT_249 PERMIT #define INTERRUPT_250 PERMIT #define INTERRUPT_251 PERMIT #define INTERRUPT_252 PERMIT #define INTERRUPT_253 PERMIT #define INTERRUPT_254 PERMIT #define INTERRUPT_255 PERMIT void NESTEDINTLIB_INT_HOOK_init(void); #endif /* NESTEDINTLIB_H_ */
/*********************************************************************** * * FILE : NestedIntLib_CCRX.c * DATE : 2022-12-06 * DESCRIPTION : Main Program * * NOTE:THIS IS A TYPICAL EXAMPLE. * ***********************************************************************/ #include "r_smc_entry.h" #include "NestedIntLib.h" void main(void); void main(void) { NESTEDINTLIB_INT_HOOK_init(); int_exception(16); // bus_error_isr set_ipl(BSP_CFG_FIT_IPL_MAX - 1); int_exception(0); // trap_isr set_ipl(BSP_CFG_FIT_IPL_MAX); int_exception(0); // trap_isr set_ipl(BSP_CFG_FIT_IPL_MAX + 1); int_exception(0); // trap_isr for(;;); } #pragma interrupt trap_isr(vect=0) void trap_isr(void) { nop(); }