Hi
I am facing issue in RZN1D while running ptp i am getting the following errors, i am getting tx time out related and also noticed in get system clock functionality in eth driver is getting 0 and also rz timetamp as 0, and also when i see the output in phc it is not running it is always stays at 0 i have attached the screenshot please let me know about this issue, can ping me also at yashas.dg@utthunga.com from India
Errorptp4l[11030.964]: selected /dev/ptp0 as PTP clockptp4l[11031.080]: port 1: INITIALIZING to SLAVE on INIT_COMPLETEptp4l[11031.082]: port 0: INITIALIZING to LISTENING on INIT_COMPLETEptp4l[11032.082]: timed out while polling for tx timestampptp4l[11032.084]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bugptp4l[11032.086]: port 1: send peer delay request failedptp4l[11032.088]: port 1: SLAVE to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)ptp4l[11032.180]: selected local clock 749050.fffe.0200fd as best masterptp4l[11048.261]: port 1: FAULTY to SLAVE on INIT_COMPLETE
Error 1ptp4l[11678.311]: port 1: INITIALIZING to LISTENING on INIT_COMPLETEptp4l[11678.316]: port 0: INITIALIZING to LISTENING on INIT_COMPLETEptp4l[11679.317]: timed out while polling for tx timestampptp4l[11679.319]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bugptp4l[11679.321]: port 1: send peer delay request failedptp4l[11679.321]: port 1: LISTENING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
Error 2ptp4l[11979.894]: selected /dev/ptp0 as PTP clockptp4l[11979.981]: port 1: INITIALIZING to LISTENING on INIT_COMPLETEptp4l[11979.985]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE^[[28~ptp4l[11987.650]: selected local clock 749050.fffe.0200fd as best masterptp4l[11993.851]: selected local clock 749050.fffe.0200fd as best masterptp4l[12000.590]: selected local clock 749050.fffe.0200fd as best masterptp4l[12007.890]: selected local clock 749050.fffe.0200fd as best master
Error 3ptp4l[12038.699]: selected /dev/ptp0 as PTP clockptp4l[12038.791]: port 1: INITIALIZING to LISTENING on INIT_COMPLETEptp4l[12038.795]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE^[[28~ptp4l[12045.986]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRESptp4l[12045.987]: selected local clock 749050.fffe.0200fd as best masterptp4l[12045.987]: assuming the grand master roleptp4l[12046.988]: timed out while polling for tx timestampptp4l[12046.989]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bugptp4l[12046.989]: port 1: send sync failedptp4l[12046.989]: port 1: MASTER to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)