初めまして。
RZ/V2L Linux Package Version 1.0.1をダウンロードし、Start-up Guideに基づいてLinuxブートをトライしていますが、添付のように途中でKernel panicが起きております。
確認すべき場所などアドバイスを頂けますと幸いです。
+++
NOTICE: BL2: v2.5(release):v2.5/rzg2l-1.00-23-gd4c55f30c-dirtyNOTICE: BL2: Built : 05:27:10, Nov 5 2021NOTICE: BL2: Booting BL31NOTICE: BL31: v2.5(release):v2.5/rzg2l-1.00-23-gd4c55f30c-dirtyNOTICE: BL31: Built : 05:27:10, Nov 5 2021
U-Boot 2020.10 (Nov 18 2021 - 03:32:16 +0000)
CPU: Renesas Electronics E rev 16.15Model: smarc-rzv2lDRAM: 1.9 GiBMMC: sh-sdhi: 0, sh-sdhi: 1Loading Environment from MMC... OKIn: serial@1004b800Out: serial@1004b800Err: serial@1004b800Net:Error: ethernet@11c20000 address not set.No ethernet found.
Hit any key to stop autoboot: 0switch to partitions #0, OKmmc1 is current device13660672 bytes read in 881 ms (14.8 MiB/s)28360 bytes read in 7 ms (3.9 MiB/s)## Flattened Device Tree blob at 48000000 Booting using the fdt blob at 0x48000000ERROR: reserving fdt memory region failed (addr=b9000000 size=4000000)ERROR: reserving fdt memory region failed (addr=bd000000 size=3000000) Loading Device Tree to 0000000057ff6000, end 0000000057fffec7 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050][ 0.000000] Linux version 4.19.165-cip41-yocto-standard (oe-user@oe-host) (gcc version 8.3.0 (GCC)) #1 SMP PREEMPT Sat Feb 27 02:21:18 UTC 2021[ 0.000000] Machine model: RZV2L Evaluation Board Kit (Discrete Power)(Dual Cortex-A55)[ 0.000000] efi: Getting EFI parameters from FDT:[ 0.000000] efi: UEFI not found.[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000058000000, size 256 MiB[ 0.000000] OF: reserved mem: initialized node linux,cma@58000000, compatible id shared-dma-pool[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000068000000, size 128 MiB[ 0.000000] OF: reserved mem: initialized node linux,multimedia, compatible id shared-dma-pool[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b9000000, size *** MiB[ 0.000000] OF: reserved mem: initialized node image_buf@0, compatible id shared-dma-pool[ 0.000000] psci: probing for conduit method from DT.[ 0.000000] psci: PSCIv1.1 detected in firmware.[ 0.000000] psci: Using standard PSCI v0.2 function IDs[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.[ 0.000000] psci: SMC Calling Convention v1.0[ 0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f0 with crng_init=0[ 0.000000] percpu: Embedded 22 pages/cpu s52376 r8192 d29544 u90112[ 0.000000] Detected VIPT I-cache on CPU0[ 0.000000] CPU features: detected: Hardware dirty bit management[ 0.000000] CPU features: detected: Speculative Store Bypassing Safe (SSBS)[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 483840[ 0.000000] Kernel command line: noinitrd root=/dev/mmcblk1p2 rootwait[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)[ 0.000000] Memory: 883728K/1966080K available (8828K kernel code, 604K rwdata, 3268K rodata, 576K init, 357K bss, 623600K reserved, 458752K cma-reserved)[ 0.000000] SLUB: HWalign=***, Order=0-3, MinObjects=0, CPUs=2, Nodes=1[ 0.000000] rcu: Preemptible hierarchical RCU implementation.[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2.[ 0.000000] Tasks RCU enabled.[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2[ 0.000000] NR_IRQS: ***, nr_irqs: ***, preallocated irqs: 0[ 0.000000] GICv3: Distributor has no Range Selector support[ 0.000000] GICv3: no VLPI support, no direct LPI support[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000011940000[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt).[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns[ 0.000004] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns[ 0.000114] Console: colour dummy device 80x25[ 0.000435] console [tty0] enabled[ 0.000463] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)[ 0.000484] pid_max: default: 32768 minimum: 301[ 0.000591] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)[ 0.000614] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)[ 0.001774] ASID allocator initialised with 32768 entries[ 0.001871] rcu: Hierarchical SRCU implementation.[ 0.002403] Detected Renesas RZ/V2L r9a07g054l2[ 0.002677] EFI services will not be available.[ 0.002874] smp: Bringing up secondary CPUs ...[ 0.003263] Detected VIPT I-cache on CPU1[ 0.003298] GICv3: CPU1: found redistributor 100 region 0:0x0000000011960000[ 0.003336] CPU1: Booted secondary processor 0x0000000100 [0x412fd050][ 0.003435] smp: Brought up 1 node, 2 CPUs[ 0.003477] SMP: Total of 2 processors activated.[ 0.003489] CPU features: detected: GIC system register CPU interface[ 0.003500] CPU features: detected: Privileged Access Never[ 0.003511] CPU features: detected: User Access Override[ 0.003520] CPU features: detected: 32-bit EL0 Support[ 0.003886] CPU: All CPU(s) started at EL1[ 0.003908] alternatives: patching kernel code[ 0.005704] devtmpfs: initialized[ 0.009972] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns[ 0.010017] futex hash table entries: 512 (order: 3, 32768 bytes)[ 0.020524] pinctrl core: initialized pinctrl subsystem[ 0.021155] DMI not present or invalid.[ 0.021435] NET: Registered protocol family 16[ 0.021751] audit: initializing netlink subsys (disabled)[ 0.021953] audit: type=2000 audit(0.020:1): state=initialized audit_enabled=0 res=1[ 0.022517] cpuidle: using governor menu[ 0.022671] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.[ 0.023599] DMA: preallocated 256 KiB pool for atomic allocations[ 0.037853] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages[ 0.038291] cryptd: max_cpu_qlen set to 1000[ 0.047373] vgaarb: loaded[ 0.047593] SCSI subsystem initialized[ 0.048068] usbcore: registered new interface driver usbfs[ 0.048123] usbcore: registered new interface driver hub[ 0.048190] usbcore: registered new device driver usb[ 0.048860] media: Linux media interface: v0.10[ 0.048943] videodev: Linux video capture interface: v2.00[ 0.049005] pps_core: LinuxPPS API ver. 1 registered[ 0.049017] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>[ 0.049039] PTP clock support registered[ 0.049064] EDAC MC: Ver: 3.0.0[ 0.049850] rzg2l_mtu3 10001200.timer: ch0: used as clock source[ 0.049873] clocksource: 10001200.timer: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 18711154 ns[ 0.049914] rzg2l_mtu3 10001200.timer: ch1: used for clock events[ 0.050441] Advanced Linux Sound Architecture Driver Initialized.[ 0.054732] GPIO line 458 (canfd0_en) hogged as output/high[ 0.054772] GPIO line 459 (canfd1_en) hogged as output/high[ 0.054800] GPIO line 153 (sd0_pwr_en) hogged as output/high[ 0.054823] GPIO line 434 (sd1_pwr_en) hogged as output/high[ 0.055719] rzg2l-pinctrl 11030000.pin-controller: rzg2l-pinctrl support registered[ 0.056352] clocksource: Switched to clocksource arch_sys_counter[ 0.056534] VFS: Disk quotas dquot_6.6.0[ 0.056600] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)[ 0.061658] NET: Registered protocol family 2[ 0.062280] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes)[ 0.062327] TCP established hash table entries: 16384 (order: 5, 131072 bytes)[ 0.062435] TCP bind hash table entries: 16384 (order: 6, 262144 bytes)[ 0.062721] TCP: Hash tables configured (established 16384 bind 16384)[ 0.062868] UDP hash table entries: 1024 (order: 3, 32768 bytes)[ 0.062913] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)[ 0.063068] NET: Registered protocol family 1[ 0.063484] RPC: Registered named UNIX socket transport module.[ 0.063504] RPC: Registered udp transport module.[ 0.063514] RPC: Registered tcp transport module.[ 0.063524] RPC: Registered tcp NFSv4.1 backchannel transport module.[ 0.064160] kvm [1]: HYP mode not available[ 0.065740] workingset: timestamp_bits=46 max_order=19 bucket_order=0[ 0.070607] squashfs: version 4.0 (2009/01/31) Phillip Lougher[ 0.071240] NFS: Registering the id_resolver key type[ 0.071284] Key type id_resolver registered[ 0.071294] Key type id_legacy registered[ 0.071311] nfs4filelayout_init: NFSv4 File Layout Driver Registering...[ 0.071340] jffs2: version 2.2. (NAND) c 2001-2006 Red Hat, Inc.[ 0.074438] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)[ 0.074473] io scheduler noop registered[ 0.074485] io scheduler deadline registered[ 0.074653] io scheduler cfq registered (default)[ 0.074669] io scheduler mq-deadline registered[ 0.074680] io scheduler kyber registered[ 0.076106] phy_rcar_gen3_usb2 11c50200.usb-phy: Linked as a consumer to regulator.3[ 0.078184] gpt-rzg2l 10048500.gpt: RZ/G2L GPT Driver probed[ 0.108426] SuperH (H)SCI(F) driver initialized[ 0.108815] 1004b800.serial: ttySC0 at MMIO 0x1004b800 (irq = 42, base_baud = 0) is a scif[ 0.851412] console [ttySC0] enabled[ 0.855495] 1004c000.serial: ttySC2 at MMIO 0x1004c000 (irq = 47, base_baud = 0) is a scif[ 0.864907] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).[ 0.871532] [drm] No driver support for vblank timestamp query.[ 0.885739] loop: module loaded[ 0.890412] renesas_spi 1004b000.spi: DMA available[ 0.895650] renesas_spi 1004b000.spi: probed[ 0.903650] m25p80 spi3.0: n25q512a (65536 Kbytes)[ 0.908754] 5 fixed-partitions partitions found on MTD device spi3.0[ 0.915104] Creating 5 MTD partitions on "spi3.0":[ 0.919914] 0x000000000000-0x000000080000 : "u-boot"[ 0.925570] 0x000000080000-0x0000000c0000 : "env"[ 0.930875] 0x0000000c0000-0x000000100000 : "dtb"[ 0.936184] 0x000000800000-0x000001800000 : "rootfs"[ 0.941729] 0x000002000000-0x000002100000 : "test-area"[ 0.948072] libphy: Fixed MDIO Bus: probed[ 0.952514] tun: Universal TUN/TAP device driver, 1.6[ 0.957734] CAN device driver interface[ 0.964421] rcar_canfd 10050000.can: can_clk rate is 49875000[ 0.970513] rcar_canfd 10050000.can: device registered (channel 0)[ 0.976801] rcar_canfd 10050000.can: can_clk rate is 49875000[ 0.982822] rcar_canfd 10050000.can: device registered (channel 1)[ 0.989075] rcar_canfd 10050000.can: global operational state (clk 0, fdmode 1)[ 0.996580] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k[ 1.002395] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.[ 1.009097] ravb 11c20000.ethernet: no valid MAC address supplied, using a random one[ 1.017053] libphy: ravb_mii: probed[ 1.021817] ravb 11c20000.ethernet eth0: Base address at 0x11c20000, 2a:f0:53:60:29:1b, IRQ 105.[ 1.031285] ravb 11c30000.ethernet: no valid MAC address supplied, using a random one[ 1.039271] libphy: ravb_mii: probed[ 1.043998] ravb 11c30000.ethernet eth1: Base address at 0x11c30000, 52:a9:89:b8:ba:0e, IRQ 108.[ 1.053248] VFIO - User Level meta-driver version: 0.3[ 1.058590] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver[ 1.065110] ehci-pci: EHCI PCI platform driver[ 1.069603] ehci-platform: EHCI generic platform driver[ 1.100441] ehci-platform 11c50100.usb: EHCI Host Controller[ 1.106112] ehci-platform 11c50100.usb: new USB bus registered, assigned bus number 1[ 1.114254] ehci-platform 11c50100.usb: irq 112, io mem 0x11c50100[ 1.136356] ehci-platform 11c50100.usb: USB 2.0 started, EHCI 1.10[ 1.143101] hub 1-0:1.0: USB hub found[ 1.146877] hub 1-0:1.0: 1 port detected[ 1.151316] ehci-platform 11c70100.usb: EHCI Host Controller[ 1.156997] ehci-platform 11c70100.usb: new USB bus registered, assigned bus number 2[ 1.165132] ehci-platform 11c70100.usb: irq 114, io mem 0x11c70100[ 1.184358] ehci-platform 11c70100.usb: USB 2.0 started, EHCI 1.10[ 1.191087] hub 2-0:1.0: USB hub found[ 1.194862] hub 2-0:1.0: 1 port detected[ 1.199205] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver[ 1.205404] ohci-pci: OHCI PCI platform driver[ 1.209902] ohci-platform: OHCI generic platform driver[ 1.215391] ohci-platform 11c50000.usb: Generic Platform OHCI controller[ 1.222091] ohci-platform 11c50000.usb: new USB bus registered, assigned bus number 3[ 1.230177] ohci-platform 11c50000.usb: irq 111, io mem 0x11c50000[ 1.326911] hub 3-0:1.0: USB hub found[ 1.330691] hub 3-0:1.0: 1 port detected[ 1.335047] ohci-platform 11c70000.usb: Generic Platform OHCI controller[ 1.341760] ohci-platform 11c70000.usb: new USB bus registered, assigned bus number 4[ 1.349879] ohci-platform 11c70000.usb: irq 113, io mem 0x11c70000[ 1.442892] hub 4-0:1.0: USB hub found[ 1.446674] hub 4-0:1.0: 1 port detected[ 1.451437] usbcore: registered new interface driver usb-storage[ 1.457875] renesas_usbhs 11c60000.usb: host probed[ 1.462769] renesas_usbhs 11c60000.usb: no transceiver found[ 1.468532] renesas_usbhs 11c60000.usb: gadget probed[ 1.473790] renesas_usbhs 11c60000.usb: probed[ 1.478892] usbcore: registered new interface driver usbtouchscreen[ 1.485177] i2c /dev entries driver[ 1.489439] i2c-riic 10058000.i2c: registered with 100000Hz bus speed[ 1.496763] adv7511 1-003d: Linked as a consumer to regulator.1[ 1.502841] adv7511 1-003d: Linked as a consumer to regulator.2[ 1.516236] i2c-riic 10058400.i2c: registered with 100000Hz bus speed[ 1.525789] random: fast init done[ 1.529773] i2c-riic 10058c00.i2c: registered with 400000Hz bus speed[ 1.536941] ov5645 0-003c: Linked as a consumer to regulator.4[ 1.542814] ov5645 0-003c: Linked as a consumer to regulator.6[ 1.548669] ov5645 0-003c: Linked as a consumer to regulator.5[ 1.592484] ov5645 0-003c: ov5645_write_reg: write reg error -6: reg=3103, val=11[ 1.599949] ov5645 0-003c: could not set init registers[ 1.605166] ov5645 0-003c: could not power up OV5645[ 1.610180] ov5645 0-003c: Dropping the link to regulator.5[ 1.615799] ov5645 0-003c: Dropping the link to regulator.6[ 1.621421] ov5645 0-003c: Dropping the link to regulator.4[ 1.629938] rzg2l-csi2 10830400.csi2: 2 lanes found[ 1.643303] renesas_sdhi_internal_dmac 11c00000.sd: Linked as a consumer to regulator.2[ 1.651371] renesas_sdhi_internal_dmac 11c00000.sd: Linked as a consumer to regulator.1[ 1.724537] renesas_sdhi_internal_dmac 11c00000.sd: mmc0 base at 0x11c00000 max clock rate 133 MHz[ 1.734670] renesas_sdhi_internal_dmac 11c10000.sd: Linked as a consumer to regulator.2[ 1.742957] renesas_sdhi_internal_dmac 11c10000.sd: Dropping the link to regulator.2[ 1.751260] ledtrig-cpu: registered to indicate activity on CPUs[ 1.757718] clocksource: ostm: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19160505731 ns[ 1.766997] sched_clock: 32 bits at 99MHz, resolution 10ns, wraps every 21528657914ns[ 1.774819] ostm: used for clocksource[ 1.778835] ostm: used for clock events[ 1.783247] usbcore: registered new interface driver usbhid[ 1.788869] usbhid: USB HID core driver[ 1.799883] optee: probing for conduit method from DT.[ 1.805084] optee: api uid mismatch[ 1.809037] u-dma-buf udmabuf@0: assigned reserved memory node image_buf@0[ 1.842865] u-dma-buf udmabuf0: driver version = 3.2.4[ 1.848030] u-dma-buf udmabuf0: major number = 242[ 1.853023] u-dma-buf udmabuf0: minor number = 0[ 1.857840] u-dma-buf udmabuf0: phys address = 0x00000000b9000000[ 1.864126] u-dma-buf udmabuf0: buffer size = 67108864[ 1.869547] u-dma-buf udmabuf@0: driver installed.[ 1.876865] ssi-pcm-audio 10049c00.ssi: DMA enalbed[ 1.882207] ssi-pcm-audio 1004a000.ssi: DMA enalbed[ 1.887537] NET: Registered protocol family 17[ 1.892047] can: controller area network core (rev 20170425 abi 9)[ 1.898441] NET: Registered protocol family 29[ 1.902961] can: raw protocol (rev 20170425)[ 1.907269] can: broadcast manager protocol (rev 20170425 t)[ 1.912958] can: netlink gateway (rev 20170425) max_hops=1[ 1.918664] Key type dns_resolver registered[ 1.923802] registered taskstats version 1[ 1.934917] thermal emergency: not set value[ 1.940403] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).[ 1.947116] [drm] No driver support for vblank timestamp query.[ 1.955191] renesas_sdhi_internal_dmac 11c10000.sd: Linked as a consumer to regulator.2[ 1.963383] renesas_sdhi_internal_dmac 11c10000.sd: Linked as a consumer to regulator.8[ 1.980405] mmc0: new HS200 MMC card at address 0001[ 1.986111] mmcblk0: mmc0:0001 G1M15M 59.3 GiB[ 1.991034] mmcblk0boot0: mmc0:0001 G1M15M partition 1 31.5 MiB[ 1.997566] mmcblk0boot1: mmc0:0001 G1M15M partition 2 31.5 MiB[ 2.003777] mmcblk0rpmb: mmc0:0001 G1M15M partition 3 4.00 MiB, chardev (243:0)[ 2.012283] mmcblk0: p1 p2[ 2.028305] renesas_sdhi_internal_dmac 11c10000.sd: mmc1 base at 0x11c10000 max clock rate 133 MHz[ 2.039517] asoc-simple-card sound: wm8978-hifi <-> 10049c00.ssi mapping ok[ 2.046583] asoc-simple-card sound: ASoC: no DMI vendor name![ 2.100905] mmc1: new high speed SDHC card at address 1234[ 2.107086] mmcblk1: mmc1:1234 SA04G 3.*** GiB[ 2.113549] mmcblk1: p1 p2 p3[ 2.155125] asoc-audio-graph-card sound_card: i2s-hifi <-> 1004a000.ssi mapping ok[ 2.162790] asoc-audio-graph-card sound_card: ASoC: no DMI vendor name![ 2.170380] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).[ 2.177064] [drm] No driver support for vblank timestamp query.[ 2.183879] [drm] Initialized rcar-du 1.0.0 20130110 for 10890000.display on minor 0[ 2.191643] [drm] Device 10890000.display probed[ 2.197071] [drm] Cannot find any crtc or sizes[ 2.202133] hctosys: unable to open rtc device (rtc0)[ 2.207543] ALSA device list:[ 2.207549] [drm] Cannot find any crtc or sizes[ 2.210555] #0: ssi-dai-wm8978-hifi[ 2.218720] #1: sound_card[ 2.224467] EXT4-fs (mmcblk1p2): mounting ext3 file system using the ext4 subsystem[ 2.275769] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)[ 2.283961] VFS: Mounted root (ext3 filesystem) readonly on device 179:26.[ 2.292566] devtmpfs: error mounting -2[ 2.296854] Freeing unused kernel memory: 576K[ 2.301443] Run /sbin/init as init process[ 2.305631] Run /etc/init as init process[ 2.309749] Run /bin/init as init process[ 2.313780] Run /bin/sh as init process[ 2.317615] Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.[ 2.331765] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 4.19.165-cip41-yocto-standard #1[ 2.339667] Hardware name: RZV2L Evaluation Board Kit (Discrete Power)(Dual Cortex-A55) (DT)[ 2.348089] Call trace:[ 2.350541] dump_backtrace+0x0/0x198[ 2.354197] show_stack+0x14/0x20[ 2.357508] dump_stack+0xa8/0xd0[ 2.360819] panic+0x140/0x29c[ 2.363869] kernel_init+0xec/0x104[ 2.367349] ret_from_fork+0x10/0x18[ 2.370921] SMP: stopping secondary CPUs[ 2.374837] Kernel Offset: disabled[ 2.378318] CPU features: 0x4,20002218[ 2.382056] Memory Limit: none[ 2.385108] ---[ end Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance. ]---