{standard input}: Assembler messages:{standard input}:36: 错误: unexpected character `n' in type specifier{standard input}:36: 错误: bad instruction `b.ne 1b'scripts/Makefile.build:265: recipe for target 'arch/arm/cpu/armv8/cpu.o' failedmake[1]: *** [arch/arm/cpu/armv8/cpu.o] Error 1Makefile:1783: recipe for target 'arch/arm/cpu/armv8' failedmake: *** [arch/arm/cpu/armv8] Error 2
MAKEFILE 添加:ARCH?=armCROSS_COMPILE?=arm-linux-gnueabihf-
Hello 坐看云起,You are writing in the Japanese forum. Please write again in the Chinese forum at the following URL. The Japanese forum and the Chinese forum have different settings, so this post cannot be moved to the Chinese forum.
community-ja.renesas.com/.../rz-g2
Forum admin----------------------------------------------------------
你好你在日文版块写,请在中文版块再写,地址如下。日文版块和中文版块设置不一样,所以这个帖子不能移到中文版块。
论坛管理员