こんにちは。NoMaYです。今首を傾げているのですが、以下のドキュメントによると、e2 studio v7.5.0ではAmazon FreeRTOSプロジェクトに於いてスマートコンフィグレータでRTOS Objectコンポーネントというものが使用出来る/存在するらしいのですが、これは単なるFreeRTOSプロジェクトでは使用出来ない/存在しないものなのでしょうか?(スマートコンフィグレータウィンドウの、コンポーネントタブ上に表示されない&コンポーネント追加ダイアロにも表示されない、ので、そうなのかな、とは思っているのですが、Amazon FreeRTOSプロジェクトとFreeRTOSプロジェクトで、このような部分で違っているのが意外でしたので、、、)e2 studio 7.5.0 Release Notewww.renesas.com/jp/ja/doc/products/tool/doc/016/r20ut4556ee0101-e2studio.pdfPage 17 of 72「New Amazon FreeRTOS Configuration user interface provide within e2 studio 7.5 featuring:● Imported FreeRTOS project with pre-loaded FreeRTOS Components (Object, Kernel and Amazon Libraries).略o FreeRTOS Object configuration: allow user to be able to create, configure multiple FreeRTOS objects using GUI (Tasks, Semaphores, Queues, Software Timers, Event Groups, Message Buffers, Stream Buffers)o Create/Remove FreeRTOS Objects with user friendly UI.略」ちなみに、プロジェクトの生成では、コンパイラはCC-RX V3.01、デバイスはR5F565NEDxFP、に設定して試しました。
こんにちは。NoMaYです。作ったRTOSDemoプログラムは海外のe2 studioに詳しくない方々に渡すことになるのですが、その方々がスマートコンフィグレータを使おうとしなければ問題無いのですが、もし使おうとしてscfgファイルをクリックしたら以下の画面コピーのような状態になってしまって、どう対処したら良いかを説明するのは厄介そうな気がしてきました、、、彼らのこの後の手順としては、どうするのが彼らにとって一番楽なやり方になりますでしょうかね?、、、#今月リリースされる予定らしいe2 studioの次版は、もう64bit版しか提供されないようなので、自分も64bit版をインストールしてみたのですが、(32bit版の設定を弄っていたせいもあるのかも知れませんが)しばし試行錯誤する羽目になってしまって、どうするのが良かったのかと思う今日この頃なのでもありました、、、