こんにちは。NoMaYです。まだQiitaに掲題の投稿は見当たらなかったので考えてみようと思いました。RXv3コア搭載の品種の中でも、RX72M, RX72N, RX66Nには倍精度浮動小数点演算命令がありますが、命令の操作対象となるレジスタは、通常の汎用レジスタが使用される単精度浮動小数点演算の場合とは異なり、倍精度浮動小数点演算専用のレジスタが用意されています。また、命令の演算結果のフラグなどが格納されるレジスタも専用のものが用意されていますし、例外の発生制御を行ったり発生状況が格納されたりするレジスタにも専用のものが用意されています。ですが、既存のRXv2コア向けのFreeRTOSポートレイヤは、当然ながら、これらの倍精度浮動小数点演算専用のレジスタのことは考慮されておらず、タスク切り替え時にこれらのレジスタの内容の退避/復帰を行っていない為、タスク間で倍精度浮動小数点レジスタの値がぐちゃぐちゃに入り乱れることになってしまうので、倍精度浮動小数点演算命令の使用を諦めざるを得ないことになります。これに対処する箇所は以下の4箇所(赤字箇所)かと思います。(まだ今は概念コードのレベルですが。)port.c
#pragma inline_asm prvYieldHandlerstatic void prvYieldHandler( void ){ /* Re-enable interrupts. */ SETPSW I /* Move the data that was automatically pushed onto the interrupt stack when the interrupt occurred from the interrupt stack to the user stack. R15 is saved before it is clobbered. */ PUSH.L R15 /* Read the user stack pointer. */ MVFC USP, R15 /* Move the address down to the data being moved. */ SUB #12, R15 MVTC R15, USP /* Copy the data across. */ MOV.L [ R0 ], [ R15 ] ; R15 MOV.L 4[ R0 ], 4[ R15 ] ; PC MOV.L 8[ R0 ], 8[ R15 ] ; PSW /* Move the interrupt stack pointer to its new correct position. */ ADD #12, R0 /* All the rest of the registers are saved directly to the user stack. */ SETPSW U /* Save the rest of the general registers (R15 has been saved already). */ PUSHM R1-R14
/* Save the FPSW and accumulators. */ MVFC FPSW, R15 PUSH.L R15 MVFACGU #0, A1, R15 PUSH.L R15 MVFACHI #0, A1, R15 PUSH.L R15 MVFACLO #0, A1, R15 ; Low order word. PUSH.L R15 MVFACGU #0, A0, R15 PUSH.L R15 MVFACHI #0, A0, R15 PUSH.L R15 MVFACLO #0, A0, R15 ; Low order word. PUSH.L R15
ここでタスク切り替え前の倍精度浮動小数点演算専用レジスタの値をスタックへ退避する
/* Save the stack pointer to the TCB. */ MOV.L #_pxCurrentTCB, R15 MOV.L [ R15 ], R15 MOV.L R0, [ R15 ] /* Ensure the interrupt mask is set to the syscall priority while the kernel structures are being accessed. */ MVTIPL #configMAX_SYSCALL_INTERRUPT_PRIORITY /* Select the next task to run. */ BSR.A _vTaskSwitchContext /* Reset the interrupt mask as no more data structure access is required. */ MVTIPL #configKERNEL_INTERRUPT_PRIORITY /* Load the stack pointer of the task that is now selected as the Running state task from its TCB. */ MOV.L #_pxCurrentTCB,R15 MOV.L [ R15 ], R15 MOV.L [ R15 ], R0
ここでタスク切り替え後の倍精度浮動小数点演算専用レジスタの値をスタックから復帰する
/* Restore the context of the new task. The PSW (Program Status Word) and PC will be popped by the RTE instruction. */ POP R15 MVTACLO R15, A0 /* Accumulator low 32 bits. */ POP R15 MVTACHI R15, A0 /* Accumulator high 32 bits. */ POP R15 MVTACGU R15, A0 /* Accumulator guard. */ POP R15 MVTACLO R15, A1 /* Accumulator low 32 bits. */ POP R15 MVTACHI R15, A1 /* Accumulator high 32 bits. */ POP R15 MVTACGU R15, A1 /* Accumulator guard. */ POP R15 MVTC R15,FPSW POPM R1-R15 RTE NOP NOP}
#pragma inline_asm prvStartFirstTaskstatic void prvStartFirstTask( void ){ /* When starting the scheduler there is nothing that needs moving to the interrupt stack because the function is not called from an interrupt. Just ensure the current stack is the user stack. */ SETPSW U /* Obtain the location of the stack associated with which ever task pxCurrentTCB is currently pointing to. */ MOV.L #_pxCurrentTCB, R15 MOV.L [R15], R15 MOV.L [R15], R0
ここでタスクのスタート時の倍精度浮動小数点演算専用レジスタの値をスタックから復帰する
/* Restore the registers from the stack of the task pointed to by pxCurrentTCB. */ POP R15 MVTACLO R15, A0 /* Accumulator low 32 bits. */ POP R15 MVTACHI R15, A0 /* Accumulator high 32 bits. */ POP R15 MVTACGU R15, A0 /* Accumulator guard. */ POP R15 MVTACLO R15, A1 /* Accumulator low 32 bits. */ POP R15 MVTACHI R15, A1 /* Accumulator high 32 bits. */ POP R15 MVTACGU R15, A1 /* Accumulator guard. */ POP R15 MVTC R15,FPSW /* Floating point status word. */ POPM R1-R15 /* R1 to R15 - R0 is not included as it is the SP. */ RTE /* This pops the remaining registers. */ NOP NOP}
StackType_t *pxPortInitialiseStack( StackType_t *pxTopOfStack, TaskFunction_t pxCode, void *pvParameters ){ /* R0 is not included as it is the stack pointer. */ *pxTopOfStack = 0x00; pxTopOfStack--; *pxTopOfStack = portINITIAL_PSW; pxTopOfStack--; *pxTopOfStack = ( StackType_t ) pxCode;
/* When debugging it can be useful if every register is set to a known value. Otherwise code space can be saved by just setting the registers that need to be set. */ #ifdef USE_FULL_REGISTER_INITIALISATION { pxTopOfStack--; *pxTopOfStack = 0xffffffff; /* r15. */ pxTopOfStack--; *pxTopOfStack = 0xeeeeeeee; pxTopOfStack--; *pxTopOfStack = 0xdddddddd; pxTopOfStack--; *pxTopOfStack = 0xcccccccc; pxTopOfStack--; *pxTopOfStack = 0xbbbbbbbb; pxTopOfStack--; *pxTopOfStack = 0xaaaaaaaa; pxTopOfStack--; *pxTopOfStack = 0x99999999; pxTopOfStack--; *pxTopOfStack = 0x88888888; pxTopOfStack--; *pxTopOfStack = 0x77777777; pxTopOfStack--; *pxTopOfStack = 0x66666666; pxTopOfStack--; *pxTopOfStack = 0x55555555; pxTopOfStack--; *pxTopOfStack = 0x44444444; pxTopOfStack--; *pxTopOfStack = 0x33333333; pxTopOfStack--; *pxTopOfStack = 0x22222222; pxTopOfStack--; } #else { pxTopOfStack -= 15; } #endif
ここでタスクのスタート時の倍精度浮動小数点演算専用レジスタの値をスタックに書き込む
*pxTopOfStack = ( StackType_t ) pvParameters; /* R1 */ pxTopOfStack--; *pxTopOfStack = portINITIAL_FPSW; pxTopOfStack--; *pxTopOfStack = 0x11111111; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x22222222; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x33333333; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x44444444; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x55555555; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x66666666; /* Accumulator 1. */ return pxTopOfStack;}
続く
こんにちは。NoMaYです。RXv3命令セットを調べてみたところDPUSHMとDPOPMという便利な命令がありましたので、ユーザーズマニュアルの該当頁の画面コピーを取ってみました。(あと、倍精度浮動小数点演算専用レジスタの図の画面コピーも。) また、RX72Nの上記命令実行サイクル数の表の画面コピーも取ってみました。これらの命令を使うとスタックとの間の退避/復帰は以下の記述で済みそうです。命令実行サイクル数は退避と復帰のそれぞれで20クロック程度ですね。(ただ、64ビット幅のレジスタを単純に1つと数えて良いものか(ひょっとして2つとして数えるべきなのか)ちょっと気になりますけれど、、、)スタックへの退避
DPUSHM.D DR0-DR15DPUSHM.L DPSW-DEPC
スタックからの復帰
DPOPM.L DPSW-DEPCDPOPM.D DR0-DR15
RXファミリ RXv3命令セットアーキテクチャ ユーザーズマニュアル ソフトウェア編www.renesas.com/jp/ja/search/keyword-search.html#genre=document&q=r01us0316r01us0316jj0100-rxv3sm.pdfRX72Nグループ ユーザーズマニュアル ハードウェア編www.renesas.com/jp/ja/search/keyword-search.html#genre=document&q=r01uh0824r01uh0824jj0100-rx72n.pdf続く
こんにちは。NoMaYです。Cortex-A9、Cortex-M4F、SH2A-FPU、などのポートレイヤを見ていて気付いたのですが、タスク毎にFPUを使うかどうかをAPI関数で申告して(申告しなければFPUを使わないものとして)、FPUを使わないタスクではFPUレジスタの退避/復帰を省略して、スタック使用量(RXv3なら8×16+4×4=144byte)と実行サイクル(RXv3なら20クロック程度×2)を節約出来る機構があるようです。申告する場合のソース例として、FreeRTOS kernelのFreeRTOS Demoプロジェクトに以下のものがありました。赤文字箇所が申告する場合のおまじないのAPI関数です。ちゃんとやる時は、ここまで実装しておきたいですね。Demo/Common/Minimal/flop.c
static portTASK_FUNCTION( vCompetingMathTask1, pvParameters ){volatile portDOUBLE d1, d2, d3, d4;volatile uint16_t *pusTaskCheckVariable;volatile portDOUBLE dAnswer;short sError = pdFALSE; /* Some ports require that tasks that use a hardware floating point unit tell the kernel that they require a floating point context before any floating point instructions are executed. */ portTASK_USES_FLOATING_POINT(); d1 = 123.4567; d2 = 2345.6789; d3 = -918.222; dAnswer = ( d1 + d2 ) * d3; /* The variable this task increments to show it is still running is passed in as the parameter. */ pusTaskCheckVariable = ( volatile uint16_t * ) pvParameters; /* Keep performing a calculation and checking the result against a constant. */ for(;;) { d1 = 123.4567; d2 = 2345.6789; d3 = -918.222; d4 = ( d1 + d2 ) * d3; #if configUSE_PREEMPTION == 0 taskYIELD(); #endif /* If the calculation does not match the expected constant, stop the increment of the check variable. */ if( fabs( d4 - dAnswer ) > 0.001 ) { sError = pdTRUE; } if( sError == pdFALSE ) { /* If the calculation has always been correct then set set the check variable. The check variable will get set to pdFALSE each time xAreMathsTaskStillRunning() is executed. */ ( *pusTaskCheckVariable ) = pdTRUE; } #if configUSE_PREEMPTION == 0 taskYIELD(); #endif }}
こんにちは。NoMaYです。> タスク毎にFPUを使うかどうかをAPI関数で申告して(申告しなければFPUを使わないものとして)、FPUを使わないタスクではFPUレジスタの退避/復帰を省略して、スタック使用量(RXv3なら8×16+4×4=144byte)と実行サイクル(RXv3なら20クロック程度×2)を節約出来る機構があるようです。…略… ちゃんとやる時は、ここまで実装しておきたいですね。この機構も実装出来ました。なお、デバッグしていて気付いたのですが、倍精度浮動小数点演算専用レジスタの内のDEPCは、以下のソフトウェアマニュアルの画面コピーの通り、リードオンリレジスタでしたので、退避/復帰をしないようにしました。(というか出来ません。) GNURX版(開発環境で一番トラブルが多い) > ICCRX版 > CC-RX版(開発環境で一番トラブルが少ない) という優先順位で作業をしていますが、今日時点のGNURX版のポートレイヤを添付しておきます。RXファミリ RXv3命令セットアーキテクチャ ユーザーズマニュアル ソフトウェア編 画面コピーwww.renesas.com/jp/ja/search/keyword-search.html#genre=document&q=r01us0316r01us0316jj0100-rxv3sm.pdfFreeRTOS/Source/portable/GCC/RX700v3_DPFPU/port.c
/* * FreeRTOS Kernel V10.3.1 * Copyright (C) 2020 Amazon.com, Inc. or its affiliates. All Rights Reserved. * * Permission is hereby granted, free of charge, to any person obtaining a copy of * this software and associated documentation files (the "Software"), to deal in * the Software without restriction, including without limitation the rights to * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of * the Software, and to permit persons to whom the Software is furnished to do so, * subject to the following conditions: * * The above copyright notice and this permission notice shall be included in all * copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE. * * http://www.FreeRTOS.org * http://aws.amazon.com/freertos * * 1 tab == 4 spaces! */ /*----------------------------------------------------------- * Implementation of functions defined in portable.h for the RX700 DPFPU port. *----------------------------------------------------------*/ /* Scheduler includes. */ #include "FreeRTOS.h" #include "task.h" /* Library includes. */ #include "string.h" /* Hardware specifics. */ #if( configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H == 1 ) #include "platform.h" #else #include "iodefine.h" #endif /*-----------------------------------------------------------*/ /* Tasks should start with interrupts enabled and in Supervisor mode, therefore PSW is set with U and I set, and PM and IPL clear. */ #define portINITIAL_PSW ( ( StackType_t ) 0x00030000 ) #define portINITIAL_FPSW ( ( StackType_t ) 0x00000100 ) #define portINITIAL_DPSW ( ( StackType_t ) 0x00000100 ) #define portINITIAL_DCMR ( ( StackType_t ) 0x00000000 ) #define portINITIAL_DECNT ( ( StackType_t ) 0x00000001 ) /* Tasks are not created with a DPFPU context, but can be given a DPFPU context after they have been created. A variable is stored as part of the tasks context that holds portNO_DPFPU_CONTEXT if the task does not have an DPFPU context, or any other value if the task does have an DPFPU context. */ #define portNO_DPFPU_CONTEXT ( ( StackType_t ) 0 ) /* These macros allow a critical section to be added around the call to xTaskIncrementTick(), which is only ever called from interrupts at the kernel priority - ie a known priority. Therefore these local macros are a slight optimisation compared to calling the global SET/CLEAR_INTERRUPT_MASK macros, which would require the old IPL to be read first and stored in a local variable. */ #define portMASK_INTERRUPTS_FROM_KERNEL_ISR() __asm volatile ( "MVTIPL %0" ::"i"(configMAX_SYSCALL_INTERRUPT_PRIORITY) ) #define portUNMASK_INTERRUPTS_FROM_KERNEL_ISR() __asm volatile ( "MVTIPL %0" ::"i"(configKERNEL_INTERRUPT_PRIORITY) ) /*-----------------------------------------------------------*/ /* * Function to start the first task executing - written in asm code as direct * access to registers is required. */ static void prvStartFirstTask( void ) __attribute__((naked)); /* * Software interrupt handler. Performs the actual context switch (saving and * restoring of registers). Written in asm code as direct register access is * required. */ #if( configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H == 1 ) void vSoftwareInterruptISR( void ) __attribute__((naked, vector( R_BSP_SECNAME_INTVECTTBL, VECT_ICU_SWINT ))); #else void vSoftwareInterruptISR( void ) __attribute__((naked)); #endif /* * The tick interrupt handler. */ #if( configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H == 1 ) void vTickISR( void ) __attribute__((interrupt( R_BSP_SECNAME_INTVECTTBL, _VECT( configTICK_VECTOR ) ))); #else void vTickISR( void ) __attribute__((interrupt)); #endif /*-----------------------------------------------------------*/ extern void *pxCurrentTCB; StackType_t ulPortTaskHasDPFPUContext; /*-----------------------------------------------------------*/ /* * See header file for description. */ StackType_t *pxPortInitialiseStack( StackType_t *pxTopOfStack, TaskFunction_t pxCode, void *pvParameters ) { /* R0 is not included as it is the stack pointer. */ *pxTopOfStack = 0x00; pxTopOfStack--; *pxTopOfStack = portINITIAL_PSW; pxTopOfStack--; *pxTopOfStack = ( StackType_t ) pxCode; /* When debugging it can be useful if every register is set to a known value. Otherwise code space can be saved by just setting the registers that need to be set. */ #ifdef USE_FULL_REGISTER_INITIALISATION { pxTopOfStack--; *pxTopOfStack = 0xffffffff; /* r15. */ pxTopOfStack--; *pxTopOfStack = 0xeeeeeeee; pxTopOfStack--; *pxTopOfStack = 0xdddddddd; pxTopOfStack--; *pxTopOfStack = 0xcccccccc; pxTopOfStack--; *pxTopOfStack = 0xbbbbbbbb; pxTopOfStack--; *pxTopOfStack = 0xaaaaaaaa; pxTopOfStack--; *pxTopOfStack = 0x99999999; pxTopOfStack--; *pxTopOfStack = 0x88888888; pxTopOfStack--; *pxTopOfStack = 0x77777777; pxTopOfStack--; *pxTopOfStack = 0x66666666; pxTopOfStack--; *pxTopOfStack = 0x55555555; pxTopOfStack--; *pxTopOfStack = 0x44444444; pxTopOfStack--; *pxTopOfStack = 0x33333333; pxTopOfStack--; *pxTopOfStack = 0x22222222; pxTopOfStack--; } #else { pxTopOfStack -= 15; } #endif *pxTopOfStack = ( StackType_t ) pvParameters; /* R1 */ pxTopOfStack--; *pxTopOfStack = portINITIAL_FPSW; pxTopOfStack--; *pxTopOfStack = 0x11111111; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x22222222; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x33333333; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x44444444; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x55555555; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x66666666; /* Accumulator 0. */ #if( configUSE_TASK_DPFPU_SUPPORT == 1 ) { /* The task will start without a DPFPU context. A task that uses the DPFPU hardware must call vPortTaskUsesDPFPU() before executing any floating point instructions. */ pxTopOfStack--; *pxTopOfStack = portNO_DPFPU_CONTEXT; } #elif( configUSE_TASK_DPFPU_SUPPORT == 2 ) { /* The task will start with a DPFPU context. Leave enough space for the registers - and ensure they are initialised if desired. */ #ifdef USE_FULL_REGISTER_INITIALISATION { pxTopOfStack -= 2; *(double *)pxTopOfStack = 1515.1515; /* DR15. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1414.1414; /* DR14. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1313.1313; /* DR13. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1212.1212; /* DR12. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1111.1111; /* DR11. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1010.1010; /* DR10. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 909.0909; /* DR9. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 808.0808; /* DR8. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 707.0707; /* DR7. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 606.0606; /* DR6. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 505.0505; /* DR5. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 404.0404; /* DR4. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 303.0303; /* DR3. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 202.0202; /* DR2. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 101.0101; /* DR1. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 9876.54321;/* DR0. */ } #else { pxTopOfStack -= 32; } #endif pxTopOfStack--; *pxTopOfStack = portINITIAL_DECNT; /* DECNT. */ pxTopOfStack--; *pxTopOfStack = portINITIAL_DCMR; /* DCMR. */ pxTopOfStack--; *pxTopOfStack = portINITIAL_DPSW; /* DPSW. */ pxTopOfStack--; *pxTopOfStack = pdTRUE; ////????////ulPortTaskHasDPFPUContext = pdTRUE; } #elif( configUSE_TASK_DPFPU_SUPPORT == 0 ) { /* Omit DPFPU support. */ } #else { #error Invalid configUSE_TASK_DPFPU_SUPPORT setting - configUSE_TASK_DPFPU_SUPPORT must be set to 0, 1, 2, or left undefined. } #endif return pxTopOfStack; } /*-----------------------------------------------------------*/ BaseType_t xPortStartScheduler( void ) { extern void vApplicationSetupTimerInterrupt( void ); /* Use pxCurrentTCB just so it does not get optimised away. */ if( pxCurrentTCB != NULL ) { /* Call an application function to set up the timer that will generate the tick interrupt. This way the application can decide which peripheral to use. A demo application is provided to show a suitable example. */ vApplicationSetupTimerInterrupt(); /* Enable the software interrupt. */ _IEN( _ICU_SWINT ) = 1; /* Ensure the software interrupt is clear. */ _IR( _ICU_SWINT ) = 0; /* Ensure the software interrupt is set to the kernel priority. */ _IPR( _ICU_SWINT ) = configKERNEL_INTERRUPT_PRIORITY; /* Start the first task. */ prvStartFirstTask(); } /* Should not get here. */ return pdFAIL; } /*-----------------------------------------------------------*/ void vPortEndScheduler( void ) { /* Not implemented in ports where there is nothing to return to. Artificially force an assert. */ configASSERT( pxCurrentTCB == NULL ); } /*-----------------------------------------------------------*/ static void prvStartFirstTask( void ) { __asm volatile ( /* When starting the scheduler there is nothing that needs moving to the interrupt stack because the function is not called from an interrupt. Just ensure the current stack is the user stack. */ "SETPSW U \n" \ /* Obtain the location of the stack associated with which ever task pxCurrentTCB is currently pointing to. */ "MOV.L #_pxCurrentTCB, R15 \n" \ "MOV.L [R15], R15 \n" \ "MOV.L [R15], R0 \n" \ /* Restore the registers from the stack of the task pointed to by pxCurrentTCB. */ ////////////////////////////////////////////////////////////////////////////////////////////////////////////// #if( configUSE_TASK_DPFPU_SUPPORT != 0 ) /* Is there a DPFPU context to restore? If the restored ulPortTaskHasDPFPUContext is zero then no. */ "POP R15 \n" \ "MOV.L #_ulPortTaskHasDPFPUContext, R14 \n" \ "MOV.L R15, [R14] \n" \ "CMP #0, R15 \n" \ /* Restore the DPFPU context, if any. */ "BEQ.B ?+ \n" \ "DPOPM.L DPSW-DECNT \n" \ "DPOPM.D DR0-DR15 \n" \ "?: \n" \ #endif /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A0 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A0 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A0 \n" \ /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A1 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A1 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A1 \n" \ /* Floating point status word. */ "POP R15 \n" \ "MVTC R15, FPSW \n" \ /* R1 to R15 - R0 is not included as it is the SP. */ "POPM R1-R15 \n" \ /* This pops the remaining registers. */ "RTE \n" \ "NOP \n" \ "NOP \n" ); } /*-----------------------------------------------------------*/ void vSoftwareInterruptISR( void ) { __asm volatile ( /* Re-enable interrupts. */ "SETPSW I \n" \ /* Move the data that was automatically pushed onto the interrupt stack when the interrupt occurred from the interrupt stack to the user stack. R15 is saved before it is clobbered. */ "PUSH.L R15 \n" \ /* Read the user stack pointer. */ "MVFC USP, R15 \n" \ /* Move the address down to the data being moved. */ "SUB #12, R15 \n" \ "MVTC R15, USP \n" \ /* Copy the data across, R15, then PC, then PSW. */ "MOV.L [ R0 ], [ R15 ] \n" \ "MOV.L 4[ R0 ], 4[ R15 ] \n" \ "MOV.L 8[ R0 ], 8[ R15 ] \n" \ /* Move the interrupt stack pointer to its new correct position. */ "ADD #12, R0 \n" \ /* All the rest of the registers are saved directly to the user stack. */ "SETPSW U \n" \ /* Save the rest of the general registers (R15 has been saved already). */ "PUSHM R1-R14 \n" \ /* Floating point status word. */ "MVFC FPSW, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator guard. */ "MVFACGU #0, A1, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator high 32 bits. */ "MVFACHI #0, A1, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator low 32 bits. */ "MVFACLO #0, A1, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator guard. */ "MVFACGU #0, A0, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator high 32 bits. */ "MVFACHI #0, A0, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator low 32 bits. */ "MVFACLO #0, A0, R15 \n" \ "PUSH.L R15 \n" \ ////////////////////////////////////////////////////////////////////////////////////////////////////////////// #if( configUSE_TASK_DPFPU_SUPPORT != 0 ) /* Does the task have a DPFPU context that needs saving? If ulPortTaskHasDPFPUContext is 0 then no. */ "MOV.L #_ulPortTaskHasDPFPUContext, R15 \n" \ "MOV.L [R15], R15 \n" \ "CMP #0, R15 \n" \ /* Save the DPFPU context, if any. */ "BEQ.B ?+ \n" \ "DPUSHM.D DR0-DR15 \n" \ "DPUSHM.L DPSW-DECNT \n" \ "?: \n" \ /* Save ulPortTaskHasDPFPUContext itself. */ "PUSH R15 \n" \ #endif /* Save the stack pointer to the TCB. */ "MOV.L #_pxCurrentTCB, R15 \n" \ "MOV.L [ R15 ], R15 \n" \ "MOV.L R0, [ R15 ] \n" \ /* Ensure the interrupt mask is set to the syscall priority while the kernel structures are being accessed. */ "MVTIPL %0 \n" \ /* Select the next task to run. */ "BSR.A _vTaskSwitchContext \n" \ /* Reset the interrupt mask as no more data structure access is required. */ "MVTIPL %1 \n" \ /* Load the stack pointer of the task that is now selected as the Running state task from its TCB. */ "MOV.L #_pxCurrentTCB,R15 \n" \ "MOV.L [ R15 ], R15 \n" \ "MOV.L [ R15 ], R0 \n" \ /* Restore the context of the new task. The PSW (Program Status Word) and PC will be popped by the RTE instruction. */ ////////////////////////////////////////////////////////////////////////////////////////////////////////////// #if( configUSE_TASK_DPFPU_SUPPORT != 0 ) /* Is there a DPFPU context to restore? If the restored ulPortTaskHasDPFPUContext is zero then no. */ "POP R15 \n" \ "MOV.L #_ulPortTaskHasDPFPUContext, R14 \n" \ "MOV.L R15, [R14] \n" \ "CMP #0, R15 \n" \ /* Restore the DPFPU context, if any. */ "BEQ.B ?+ \n" \ "DPOPM.L DPSW-DECNT \n" \ "DPOPM.D DR0-DR15 \n" \ "?: \n" \ #endif /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A0 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A0 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A0 \n" \ /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A1 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A1 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A1 \n" \ /* Floating point status word. */ "POP R15 \n" \ "MVTC R15, FPSW \n" \ /* R1 to R15 - R0 is not included as it is the SP. */ "POPM R1-R15 \n" \ /* This pops the remaining registers. */ "RTE \n" \ "NOP \n" \ "NOP " :: "i"(configMAX_SYSCALL_INTERRUPT_PRIORITY), "i"(configKERNEL_INTERRUPT_PRIORITY) ); } /*-----------------------------------------------------------*/ void vTickISR( void ) { /* Re-enabled interrupts. */ __asm volatile( "SETPSW I" ); /* Increment the tick, and perform any processing the new tick value necessitates. Ensure IPL is at the max syscall value first. */ portMASK_INTERRUPTS_FROM_KERNEL_ISR(); { if( xTaskIncrementTick() != pdFALSE ) { taskYIELD(); } } portUNMASK_INTERRUPTS_FROM_KERNEL_ISR(); } /*-----------------------------------------------------------*/ uint32_t ulPortGetIPL( void ) { __asm volatile ( "MVFC PSW, R1 \n" \ "SHLR #24, R1 \n" \ "RTS " ); /* This will never get executed, but keeps the compiler from complaining. */ return 0; } /*-----------------------------------------------------------*/ void vPortSetIPL( uint32_t ulNewIPL ) { /* Avoid compiler warning about unreferenced parameter. */ ( void ) ulNewIPL; __asm volatile ( "PUSH R5 \n" \ "MVFC PSW, R5 \n" \ "SHLL #24, R1 \n" \ "AND #-0F000001H, R5 \n" \ "OR R1, R5 \n" \ "MVTC R5, PSW \n" \ "POP R5 \n" \ "RTS " ); } /*-----------------------------------------------------------*/ #if( configUSE_TASK_DPFPU_SUPPORT == 1 ) void vPortTaskUsesDPFPU( void ) { /* A task is registering the fact that it needs a DPFPU context. Set the DPFPU flag (which is saved as part of the task context). */ ulPortTaskHasDPFPUContext = pdTRUE; } #endif /* configUSE_TASK_DPFPU_SUPPORT */ /*-----------------------------------------------------------*/
/* * FreeRTOS Kernel V10.3.1 * Copyright (C) 2020 Amazon.com, Inc. or its affiliates. All Rights Reserved. * * Permission is hereby granted, free of charge, to any person obtaining a copy of * this software and associated documentation files (the "Software"), to deal in * the Software without restriction, including without limitation the rights to * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of * the Software, and to permit persons to whom the Software is furnished to do so, * subject to the following conditions: * * The above copyright notice and this permission notice shall be included in all * copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE. * * http://www.FreeRTOS.org * http://aws.amazon.com/freertos * * 1 tab == 4 spaces! */ #ifndef PORTMACRO_H #define PORTMACRO_H #ifdef __cplusplus extern "C" { #endif /*----------------------------------------------------------- * Port specific definitions. * * The settings in this file configure FreeRTOS correctly for the * given hardware and compiler. * * These settings should not be altered. *----------------------------------------------------------- */ /* Set configUSE_TASK_DPFPU_SUPPORT to 0 to omit DPFPU support even if DPFPU hardware is otherwise supported by the FreeRTOS port in use. This constant is supported by only FreeRTOS Renesas RX ports that include DPFPU support. */ /* If configUSE_TASK_DPFPU_SUPPORT is set to 1 (or undefined) then each task will be created without a DPFPU context, and a task must call vTaskUsesDPFPU() before making use of any DPFPU registers. If configUSE_TASK_DPFPU_SUPPORT is set to 2 then tasks are created with a DPFPU context by default, and calling vTaskUsesDPFPU() has no effect. If configUSE_TASK_DPFPU_SUPPORT is set to 0 then tasks never take care of any DPFPU context (even if registers DPFPU are used). */ #ifndef configUSE_TASK_DPFPU_SUPPORT #define configUSE_TASK_DPFPU_SUPPORT 1 #endif /* When the FIT configurator or the Smart Configurator is used, platform.h has to be used. */ #ifndef configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H #define configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H 0 #endif /*-----------------------------------------------------------*/ /* Type definitions - these are a bit legacy and not really used now, other than portSTACK_TYPE and portBASE_TYPE. */ #define portCHAR char #define portFLOAT float #define portDOUBLE double #define portLONG long #define portSHORT short #define portSTACK_TYPE uint32_t #define portBASE_TYPE long typedef portSTACK_TYPE StackType_t; typedef long BaseType_t; typedef unsigned long UBaseType_t; #if( configUSE_16_BIT_TICKS == 1 ) typedef uint16_t TickType_t; #define portMAX_DELAY ( TickType_t ) 0xffff #else typedef uint32_t TickType_t; #define portMAX_DELAY ( TickType_t ) 0xffffffffUL /* 32-bit tick type on a 32-bit architecture, so reads of the tick count do not need to be guarded with a critical section. */ #define portTICK_TYPE_IS_ATOMIC 1 #endif /*-----------------------------------------------------------*/ /* Hardware specifics. */ #define portBYTE_ALIGNMENT 8 /* Could make four, according to manual. */ #define portSTACK_GROWTH -1 #define portTICK_PERIOD_MS ( ( TickType_t ) 1000 / configTICK_RATE_HZ ) #define portNOP() __asm volatile( "NOP" ) /* Yield equivalent to "*portITU_SWINTR = 0x01; ( void ) *portITU_SWINTR;" where portITU_SWINTR is the location of the software interrupt register (0x000872E0). Don't rely on the assembler to select a register, so instead save and restore clobbered registers manually. */ #define portYIELD() \ __asm volatile \ ( \ "PUSH.L R10 \n" \ "MOV.L #0x872E0, R10 \n" \ "MOV.B #0x1, [R10] \n" \ "CMP [R10].UB, R10 \n" \ "POP R10 \n" \ ) #define portYIELD_FROM_ISR( x ) if( ( x ) != pdFALSE ) portYIELD() /* These macros should not be called directly, but through the taskENTER_CRITICAL() and taskEXIT_CRITICAL() macros. An extra check is performed if configASSERT() is defined to ensure an assertion handler does not inadvertently attempt to lower the IPL when the call to assert was triggered because the IPL value was found to be above configMAX_SYSCALL_INTERRUPT_PRIORITY when an ISR safe FreeRTOS API function was executed. ISR safe FreeRTOS API functions are those that end in FromISR. FreeRTOS maintains a separate interrupt API to ensure API function and interrupt entry is as fast and as simple as possible. */ #define portENABLE_INTERRUPTS() __asm volatile ( "MVTIPL #0" ) #ifdef configASSERT #define portASSERT_IF_INTERRUPT_PRIORITY_INVALID() configASSERT( ( ulPortGetIPL() <= configMAX_SYSCALL_INTERRUPT_PRIORITY ) ) #define portDISABLE_INTERRUPTS() if( ulPortGetIPL() < configMAX_SYSCALL_INTERRUPT_PRIORITY ) __asm volatile ( "MVTIPL %0" ::"i"(configMAX_SYSCALL_INTERRUPT_PRIORITY) ) #else #define portDISABLE_INTERRUPTS() __asm volatile ( "MVTIPL %0" ::"i"(configMAX_SYSCALL_INTERRUPT_PRIORITY) ) #endif /* Critical nesting counts are stored in the TCB. */ #define portCRITICAL_NESTING_IN_TCB ( 1 ) /* The critical nesting functions defined within tasks.c. */ extern void vTaskEnterCritical( void ); extern void vTaskExitCritical( void ); #define portENTER_CRITICAL() vTaskEnterCritical() #define portEXIT_CRITICAL() vTaskExitCritical() /* As this port allows interrupt nesting... */ uint32_t ulPortGetIPL( void ) __attribute__((naked)); void vPortSetIPL( uint32_t ulNewIPL ) __attribute__((naked)); #define portSET_INTERRUPT_MASK_FROM_ISR() ulPortGetIPL(); portDISABLE_INTERRUPTS() #define portCLEAR_INTERRUPT_MASK_FROM_ISR( uxSavedInterruptStatus ) vPortSetIPL( uxSavedInterruptStatus ) /*-----------------------------------------------------------*/ /* Task function macros as described on the FreeRTOS.org WEB site. */ #define portTASK_FUNCTION_PROTO( vFunction, pvParameters ) void vFunction( void *pvParameters ) #define portTASK_FUNCTION( vFunction, pvParameters ) void vFunction( void *pvParameters ) /* If configUSE_TASK_DPFPU_SUPPORT is set to 1 (or left undefined) then tasks are created without a DPFPU context and must call vPortTaskUsesDPFPU() to give themselves a DPFPU context before using any DPFPU instructions. If configUSE_TASK_DPFPU_SUPPORT is set to 2 then all tasks will have an DPFPU context by default. */ #if( configUSE_TASK_DPFPU_SUPPORT == 1 ) void vPortTaskUsesDPFPU( void ); #else /* Each task has a DPFPU context already, so define this function away to nothing to prevent it being called accidentally. */ #define vPortTaskUsesDPFPU() #endif #define portTASK_USES_DPFPU() vPortTaskUsesDPFPU() /* Definition to allow compatibility with existing FreeRTOS Demo using flop.c. */ #define portTASK_USES_FLOATING_POINT() vPortTaskUsesDPFPU() #ifdef __cplusplus } #endif #endif /* PORTMACRO_H */
こんにちは。NoMaYです。こんな感じになりました。zipファイルには、作成したRXv3-DPFPUポートレイヤと、比較用に移植元のRXv2ポートレイヤを、一緒に固めました。(なお、RTOSDemoプログラムの方は微調整作業の最中です。)RX700v3-DPFPU-portlayer-rc1-20200701.zip
├─org-FreeRTOS-Kernel-10.3.1 (比較用の移植元のRXv2ポートレイヤ)│ └─portable│ ├─GCC│ │ └─RX600v2│ │ ├─portmacro.h│ │ └─port.c│ ├─IAR│ │ └─RXv2 (なぜかフォルダ名が他と違います)│ │ ├─portmacro.h│ │ ├─port.c│ │ └─port_asm.s│ └─Renesas│ └─RX600v2│ ├─portmacro.h│ ├─port.c│ └─port_asm.src└─rc1-20200701 (作成したRXv3-DPFPUポートレイヤ) └─portable ├─GCC │ └─RX700v3_DPFPU │ ├─portmacro.h │ └─port.c ├─IAR │ └─RX700v3_DPFPU │ ├─portmacro.h │ └─port.c └─Renesas └─RX700v3_DPFPU ├─portmacro.h ├─port.c └─port_asm.src (変更無し)
こんにちは。NoMaYです。RX72N搭載の三角関数演算器(RXv3アーキテクチャ構成要素では無いですけれども)ですが、レジスタの仕様が公開されておらず自分が最初から諦めていたので問題意識として脇へ追いやっていたのですが、CC-RXで組み込み関数から普通に使えますし、コンパイルオプションを指定すれば数学ライブラリ内で使われるようにもなりますので、タスク切り替え時に退避/復帰することが出来るようにする何らかの実装があった方が良いとは思っているのですが、仕様が公開されていないので何も出来ていないです。RX72Nグループ ユーザーズマニュアル ハードウェア編www.renesas.com/jp/ja/search/keyword-search.html#genre=document&q=r01uh0824r01uh0824jj0100-rx72n.pdf三角関数演算器についての記載はこれだけです、、、
NoMaYさん シェルティです。こんにちは。 本件、とても気になります。 hirakuni45さんもご自身のブログ記事でこの点言及されてました。 FreeRTOSのタスク切り替え時にどう処理すべきかを軸に少し調査してみます。 また何かわかりましたらこの場で相談させてください。 以上です
こんにちは。NoMaYです。あっ、RXマイコンのポートレイヤは、うっかりタスクからreturnしてしまった場合のフールプルーフ処置が無い、ですね、、、RL78ですと、以下のように無限ループするprvTaskExitErrorという関数へリターンするようになっているのですが、、、
static void prvTaskExitError( void ){ /* A function that implements a task must not exit or attempt to return to its caller as there is nothing to return to. If a task wants to exit it should instead call vTaskDelete( NULL ). Artificially force an assert() to be triggered if configASSERT() is defined, then stop here so application writers can catch the error. */ configASSERT( usCriticalNesting == ~0U ); portDISABLE_INTERRUPTS(); for( ;; );}
StackType_t *pxPortInitialiseStack( StackType_t *pxTopOfStack, TaskFunction_t pxCode, void *pvParameters ){uint32_t *pulLocal; /* With large code sizeof( TaskFunction_t ) == 4. With small code sizeof( TaskFunction_t ) == 2. Always sizeof( StackType_t ) == 2 and sizeof( StackType_t * ) == 2. */ /* The return address, leaving space for the first two bytes of the 32-bit value. See the comments above the prvTaskExitError() prototype at the top of this file. */ pxTopOfStack--; pulLocal = ( uint32_t * ) pxTopOfStack;#ifdef __RL78_SMALL__ /* Cast from 16bits pointer to 32bits value is potentially not safe. */ *pulLocal = ( uint32_t ) ( uint16_t ) prvTaskExitError;#else /* __RL78_MEDIUM__ */ /* Cast from 32bits (actually 24bits) pointer to 32bits value is safe. */ *pulLocal = ( uint32_t ) prvTaskExitError;#endif pxTopOfStack--; /* Task function. Again as it is written as a 32-bit value a space is left on the stack for the second two bytes. */ pxTopOfStack--; /* Task function start address combined with the PSW. */ pulLocal = ( uint32_t * ) pxTopOfStack;#ifdef __RL78_SMALL__ /* Cast from 16bits pointer to 32bits value is potentially not safe. */ *pulLocal = ( ( ( uint32_t ) ( uint16_t ) pxCode ) | ( portPSW << 24UL ) );#else /* __RL78_MEDIUM__ */ /* Cast from 32bits (actually 24bits) pointer to 32bits value is safe. */ *pulLocal = ( ( ( uint32_t ) pxCode ) | ( portPSW << 24UL ) );#endif
RXですと、そのような関数への戻り番地は何も詰まれていませんので、タスクからreturnすると暴走しますね、、、
StackType_t *pxPortInitialiseStack( StackType_t *pxTopOfStack, TaskFunction_t pxCode, void *pvParameters )
{
/* R0 is not included as it is the stack pointer. */
*pxTopOfStack = 0x00;
pxTopOfStack--;
*pxTopOfStack = portINITIAL_PSW;
*pxTopOfStack = ( StackType_t ) pxCode;
NoMaYさん
シェルティです、こんにちは。
チケット作っておきました。https://github.com/renesas/FreeRTOS-Kernel/issues/7
プルリクエストして本家のコードを直すところまで持っていきます。
ご連絡感謝いたします。
以上です
みなさんこんにちは。
このような重要なトピックがあるのに気がつきませんでした・・
---
RTOS下での、TFUの扱いですが、TFUは純粋なハードウェアー(だと思う)なので、計算途中を退避するのは難しいと思います。
なので、当面は、排他制御で、誰かがTFUにアクセスしたら、それが終了するまで、他を待たせるしか出来ないと思います。
hirakuni45さん、NoMaYさん
こんにちはシェルティです。hirakuni45さんのブログ記事いつも更新を楽しみに待っております。
TFUについてはhirakuni45さんの仰る通りの対処が正しいと思います。
現在組み込み機器のIoT化の流れにともない、クラウド側の雄であるAWSとMicrosoftが提供するリアルタイムOSであるところのFreeRTOS(AWS)とAzure RTOS(Microsoft)のユーザ実製品での活用検討がいよいよ盛んになってきたと考えております。これに伴い、これまでほぼシェルティ+1名くらいの体制で開発していたオープンソースなRTOS周りの開発体制を強化しつつあります。強化完了した暁には頂いたフィードバックはAWSなりMicrosoftなりにGitHub上で素早くプルリクエストを出して正式にカーネルに取り込んでもらうよう働きかけていきたいと考えています。現状まだなかなか歩みが遅い感じになっていますが、改善を進めておりますので、引き続きご支援いただけますと幸いです。