こんにちは。NoMaYです。最近、以下のスレッドに関わって知ったのですが、ルネサスさんのTCP/IPスタックT4のバイナリライブラリ(元ソースもRXスマートコンフィグレータにて提供される)が以下の画面コピーのT4のドキュメント記載の事情によりビルド出来ないことを知りました。そこで対処法を試行錯誤してみました。続く。FreeRTOSとr_t4_rxを使用した際のビルドエラーについて(RX72N)japan.renesasrulz.com/cafe_rene/forums-groups/beginners/f/002-2095199602/8335/freertos-r_t4_rx-rx72n/42982#42982「ところで脱線しますけれども、T4のドキュメントの以下の制限事項ですが、エラーは発生するのでしょうか?」RX SmartConfiguratorで気になった点とか改善する案とか報告してみるスレッドjapan.renesasrulz.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/7536/rx-smartconfigurator/43222#43222「ビルドエラーが発生するのはT4のライブラリ(r_t4_rx/make_lib/make_lib.zip の中にライブラリソースと作成用プロジェクトが入っています)を自前で作成する時です。」以下、T4のドキュメントの画面コピーです。
こんにちは。NoMaYです。細かい話の前にパッチを上げておきます。ベースはr_t4_rx v2.10です。T4_Library_patch_20220818.zip ⇒ 不要です。コンパイルオプションの-std=gnu99→c99の変更で事足ります。
make_lib/T4_src/t4define.hmake_lib/T4_src/dhcp.cmake_lib/T4_src/ether.cmake_lib/T4_src/tcp_api.c
続く。以下、変更箇所の画面コピーです。左側が変更前、右側が変更後、です。(4枚)
こんにちは。NoMaYです。2重定義になっているin_addr_tという型は以下になります。なお、Google検索すると業界標準は、構造体/共用体による定義ではなく、プレーンな32ビット整数型による定義の方のようです。T4側
typedef struct _in_addr{ union { struct { uint8_t s_b1; uint8_t s_b2; uint8_t s_b3; uint8_t s_b4; } S_un_b; struct { uint16_t s_w1; uint16_t s_w2; } S_un_w; uint32_t S_addr; } S_un;} in_addr_t;
GCC側
#if __BSD_VISIBLE#include <machine/endian.h>#include <sys/select.h># define physadr physadr_t# define quad quad_t#ifndef _IN_ADDR_T_DECLAREDtypedef __uint32_t in_addr_t; /* base type for internet address */#define _IN_ADDR_T_DECLARED#endif#ifndef _IN_PORT_T_DECLAREDtypedef __uint16_t in_port_t;#define _IN_PORT_T_DECLARED#endiftypedef __uintptr_t u_register_t;#endif /* __BSD_VISIBLE */
Google検索: in_addr_twww.google.com/search?q=in_addr_t続く。
こんにちは。NoMaYです。#とても気まずいことに気付いてしまいました、、、今回はT4側のin_addr_tを業界標準に適合させることを目的にしませんでしたので、GCC側のin_addr_tを無効化することにしました。T4がサポートしている他のコンパイラのCC-RXとICCRXではBSD由来のもろもろをサポートしていない(と思われる)ことを考えると、__BSD_VISIBLEを無効化することを考えるのが妥当では無いかと私は考えました。そして、以下の画面コピーのとおり#defineの連鎖を追ってみた結果、_ISOC99_SOURCEを#defineするのが良さそうだと考えるに至りました。(ところがどっこい、今頃気付いたのですが、以下の画面コピーの3枚目の内容を見ていてハタとコンパイルオプションを-std=gnu99では無くて-std=c99とすれば良いのだろうか?と思って試してみたら、それだけで出来てしまいました、、、あぁっ、とても気まずいです、、、)続く。以下、画面コピーです。
/* * Feature test macros control which symbols are exposed by the system * headers. Any of these must be defined before including any headers. * * __STRICT_ANSI__ (defined by gcc -ansi, -std=c90, -std=c99, or -std=c11) * ISO C * * _POSIX_SOURCE (deprecated by _POSIX_C_SOURCE=1) * _POSIX_C_SOURCE >= 1 * POSIX.1-1990 * * _POSIX_C_SOURCE >= 2 * POSIX.2-1992 * * _POSIX_C_SOURCE >= 199309L * POSIX.1b-1993 Real-time extensions * * _POSIX_C_SOURCE >= 199506L * POSIX.1c-1995 Threads extensions * * _POSIX_C_SOURCE >= 200112L * POSIX.1-2001 and C99 * * _POSIX_C_SOURCE >= 200809L * POSIX.1-2008 * * _XOPEN_SOURCE * POSIX.1-1990 and XPG4 * * _XOPEN_SOURCE_EXTENDED * SUSv1 (POSIX.2-1992 plus XPG4v2) * * _XOPEN_SOURCE >= 500 * SUSv2 (POSIX.1c-1995 plus XSI) * * _XOPEN_SOURCE >= 600 * SUSv3 (POSIX.1-2001 plus XSI) and C99 * * _XOPEN_SOURCE >= 700 * SUSv4 (POSIX.1-2008 plus XSI) * * _ISOC99_SOURCE or gcc -std=c99 or g++ * ISO C99 * * _ISOC11_SOURCE or gcc -std=c11 or g++ -std=c++11 * ISO C11 * * _ATFILE_SOURCE (implied by _POSIX_C_SOURCE >= 200809L) * "at" functions * * _LARGEFILE_SOURCE (deprecated by _XOPEN_SOURCE >= 500) * fseeko, ftello * * _GNU_SOURCE * All of the above plus GNU extensions * * _BSD_SOURCE (deprecated by _DEFAULT_SOURCE) * _SVID_SOURCE (deprecated by _DEFAULT_SOURCE) * _DEFAULT_SOURCE (or none of the above) * POSIX-1.2008 with BSD and SVr4 extensions * * _FORTIFY_SOURCE = 1 or 2 * Object Size Checking function wrappers */
こんにちは。NoMaYです。気付いてしまえば、ソースファイル自体は何も変える必要は無く、以下の画面コピーの通り、コンパイルオプションを-std=gnu99→c99へと変更するだけで事足りました。(GCC for Renesas 8.3.0.202202-GNURXを使いました。)了以下、e2 studioの画面コピーです。