/*********************************************************************** * * FILE : NestedIntLib_CCRX.c * DATE : 2022-12-06 * DESCRIPTION : Main Program * * NOTE:THIS IS A TYPICAL EXAMPLE. * ***********************************************************************/ #include "r_smc_entry.h" #include "NestedIntLib.h" void main(void); void main(void) { NESTEDINTLIB_INT_HOOK_init(); int_exception(16); // bus_error_isr set_ipl(BSP_CFG_FIT_IPL_MAX - 1); int_exception(0); // trap_isr set_ipl(BSP_CFG_FIT_IPL_MAX); int_exception(0); // trap_isr set_ipl(BSP_CFG_FIT_IPL_MAX + 1); int_exception(0); // trap_isr for(;;); } #pragma interrupt trap_isr(vect=0) void trap_isr(void) { nop(); }