generic_rx110\resetprg.c(396): /* Sub-clock oscillator is chosen. Start it operating. */ generic_rx110\resetprg.c(398): /* Set the sub-clock to operating. */ generic_rx110\resetprg.c(405): /* There is not an oscillation stabilization flag for the sub-clock so a software delay is used. generic_rx110\resetprg.c(406): The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX111's generic_rx110\resetprg.c(416): /* Set the sub-clock to stopped. */ generic_rx110\resetprg.c(553): /* Sub-clock oscillator is chosen. Start it operating. */ generic_rx110\resetprg.c(557): /* Set the sub-clock to stopped. */ generic_rx110\r_bsp_config_reference.h(208): 3 = Sub-Clock Oscillator generic_rx111\resetprg.c(412): /* Sub-clock oscillator is chosen. Start it operating. */ generic_rx111\resetprg.c(414): /* Set the sub-clock to operating. */ generic_rx111\resetprg.c(421): /* There is not an oscillation stabilization flag for the sub-clock so a software delay is used. generic_rx111\resetprg.c(422): The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX111's generic_rx111\resetprg.c(432): /* Set the sub-clock to stopped. */ generic_rx111\resetprg.c(607): /* Sub-clock oscillator is chosen. Start it operating. */ generic_rx111\resetprg.c(611): /* Set the sub-clock to stopped. */ generic_rx111\r_bsp_config_reference.h(228): 3 = Sub-Clock Oscillator generic_rx113\resetprg.c(405): /* Sub-clock oscillator is chosen. Start it operating. */ generic_rx113\resetprg.c(407): /* Set the sub-clock to operating. */ generic_rx113\resetprg.c(414): /* There is not an oscillation stabilization flag for the sub-clock so a software delay is used. generic_rx113\resetprg.c(415): The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX111's generic_rx113\resetprg.c(425): /* Set the sub-clock to stopped. */ generic_rx113\resetprg.c(696): /* Sub-clock oscillator is chosen. Start it operating. */ generic_rx113\resetprg.c(700): /* Set the sub-clock to stopped. */ generic_rx113\r_bsp_config_reference.h(204): 3 = Sub-Clock Oscillator generic_rx113\r_bsp_config_reference.h(219): 3 = Sub-Clock Oscillator ★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ generic_rx130\resetprg.c(32): * Changed the method of Wait for at least five cycles (about 153 μs) of the sub-clock. generic_rx130\resetprg.c(69): /* When the system clock is the sub-clock, warning will occur but there is no problem. generic_rx130\resetprg.c(434): SYSTEM.SOSCCR.BYTE = 0x01; /* Make sure sub-clock is initially stopped */ generic_rx130\resetprg.c(441): RTC.RCR3.BIT.RTCEN = 0; /* Also set the RTC Sub-Clock disable */ generic_rx130\resetprg.c(448): /* wait for 5 sub-clock cycles (153us): measurement result is approx. 176us */ generic_rx130\resetprg.c(451): RTC.RCR3.BIT.RTCDV = 0x01; /* Init the Sub-Clock Oscillator Drive Capacity = Low CL */ generic_rx130\resetprg.c(458): SYSTEM.SOSCCR.BYTE = 0x00; /* Start sub-clock */ generic_rx130\resetprg.c(466): /* Wait for the oscillation stabilization time of the sub-clock. (1.3 seconds.)*/ generic_rx130\resetprg.c(470): RTC.RCR3.BIT.RTCEN = 0x01; /* Also set the RTC Sub-Clock enable */ generic_rx130\resetprg.c(478): /* Wait for the oscillation stabilization time of the sub-clock. (1.3 seconds.)*/ generic_rx130\resetprg.c(481): /* Set the sub-clock to stopped. */ generic_rx130\resetprg.c(489): /* Set the sub-clock to stopped. */ generic_rx130\resetprg.c(594): /* Sub-clock or None is chosen. */ generic_rx130\resetprg.c(595): /* sub-clock oscillator already initialized in clock_source_select() */ generic_rx130\r_bsp_config_reference.h(197): 3 = Sub-Clock Oscillator generic_rx130\r_bsp_config_reference.h(209): 0 = Sub-clock ★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ generic_rx230\resetprg.c(64): /* When the system clock is the sub-clock, warning will occur but there is no problem. generic_rx230\resetprg.c(508): SYSTEM.SOSCCR.BYTE = 0x01; // Make sure sub-clock is initially stopped generic_rx230\resetprg.c(515): RTC.RCR3.BIT.RTCEN = 0; // Also set the RTC Sub-Clock disable generic_rx230\resetprg.c(528): RTC.RCR3.BIT.RTCDV = 0x01; // Init the Sub-Clock Oscillator Drive Capacity = Low CL generic_rx230\resetprg.c(535): SYSTEM.SOSCCR.BYTE = 0x00; // Start sub-clock generic_rx230\resetprg.c(544): RTC.RCR3.BIT.RTCEN = 0x01; // Also set the RTC Sub-Clock enable generic_rx230\resetprg.c(551): /* Set the sub-clock to stopped. */ generic_rx230\resetprg.c(611): /* Sub-clock is chosen. */ generic_rx230\resetprg.c(612): /* sub-clock oscillator already initialized in clock_source_select() or cgc_clock_config() */ generic_rx230\r_bsp_config_reference.h(202): 3 = Sub-Clock Oscillator generic_rx230\r_bsp_config_reference.h(208): 0 = Sub-clock ★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ generic_rx231\resetprg.c(65): /* When the system clock is the sub-clock, warning will occur but there is no problem. generic_rx231\resetprg.c(510): SYSTEM.SOSCCR.BYTE = 0x01; // Make sure sub-clock is initially stopped generic_rx231\resetprg.c(517): RTC.RCR3.BIT.RTCEN = 0; // Also set the RTC Sub-Clock disable generic_rx231\resetprg.c(530): RTC.RCR3.BIT.RTCDV = 0x01; // Init the Sub-Clock Oscillator Drive Capacity = Low CL generic_rx231\resetprg.c(537): SYSTEM.SOSCCR.BYTE = 0x00; // Start sub-clock generic_rx231\resetprg.c(546): RTC.RCR3.BIT.RTCEN = 0x01; // Also set the RTC Sub-Clock enable generic_rx231\resetprg.c(553): /* Set the sub-clock to stopped. */ generic_rx231\resetprg.c(650): /* Sub-clock is chosen. */ generic_rx231\resetprg.c(651): /* sub-clock oscillator already initialized in clock_source_select() or cgc_clock_config() */ generic_rx231\r_bsp_config_reference.h(221): 3 = Sub-Clock Oscillator generic_rx231\r_bsp_config_reference.h(233): 0 = Sub-clock ★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ generic_rx23t\r_bsp_config_reference.h(199): 3 = Sub-Clock Oscillator (N/A for RX23T) generic_rx24t\r_bsp_config_reference.h(200): 3 = Sub-Clock Oscillator (N/A for RX24T) generic_rx24u\r_bsp_config_reference.h(187): 3 = Sub-Clock Oscillator (N/A for RX24U) generic_rx64m\resetprg.c(34): * - Sub-Clock Oscillator Wait Control Register (SOSCWTCR) generic_rx64m\resetprg.c(37): * Changed the sub-clock oscillator settings. generic_rx64m\resetprg.c(616): /* Sub-clock setting. */ generic_rx64m\resetprg.c(621): /* Stop the sub-clock oscillator */ generic_rx64m\resetprg.c(624): b0 RCKSEL - Count Source Select - Sub-clock oscillator is selected. */ generic_rx64m\resetprg.c(642): b3:b1 RTCDV - Sub-clock oscillator Drive Ability Control. generic_rx64m\resetprg.c(643): b0 RTCEN - Sub-clock oscillator is stopped. */ generic_rx64m\resetprg.c(659): /* SOSCCR - Sub-Clock Oscillator Control Register generic_rx64m\resetprg.c(661): b0 SOSTP - Sub-clock oscillator Stop - Sub-clock oscillator is stopped. */ generic_rx64m\resetprg.c(675): /* The delay period needed is to make sure that the sub-clock has stopped. */ generic_rx64m\resetprg.c(679): /* Set the drive capacity of the sub-clock oscillator */ generic_rx64m\resetprg.c(703): /* Set wait time until the sub-clock oscillator stabilizes */ generic_rx64m\resetprg.c(704): /* SOSCWTCR - Sub-Clock Oscillator Wait Control Register generic_rx64m\resetprg.c(706): b4:b0 SSTS - Sub-Clock Oscillator Waiting Time - Waiting time is 2.044ms(the maximum value of fLOCO). */ generic_rx64m\resetprg.c(709): /* Operate the Sub-clock oscillator */ generic_rx64m\resetprg.c(723): /* The delay period needed is to make sure that the sub-clock has stabilized. */ generic_rx64m\resetprg.c(728): /* ---- Set wait time until the sub-clock oscillator stabilizes ---- */ generic_rx64m\resetprg.c(731): /* ---- Operate the sub-clock oscillator ---- */ generic_rx64m\resetprg.c(749): /* Wait for six the sub-clock cycles */ generic_rx64m\resetprg.c(750): /* 6 count of sub-clock : (1000000/32768)*6=183.10546875us generic_rx64m\resetprg.c(794): /* Wait for one the sub-clock cycles */ generic_rx64m\resetprg.c(795): /* 1 count of sub-clock : (1000000/32768)=30.517578125us generic_rx64m\resetprg.c(811): /* SOSCCR - Sub-Clock Oscillator Control Register generic_rx64m\resetprg.c(813): b0 SOSTP - Sub-clock oscillator Stop - Sub-clock oscillator is stopped. */ generic_rx64m\resetprg.c(832): /* Set wait time until the sub-clock oscillator stabilizes */ generic_rx64m\resetprg.c(833): /* SOSCWTCR - Sub-Clock Oscillator Wait Control Register generic_rx64m\resetprg.c(835): b4:b0 SSTS - Sub-Clock Oscillator Waiting Time - Waiting time is 2.044ms(the maximum value of fLOCO). */ generic_rx64m\resetprg.c(838): /* Operate the Sub-clock oscillator */ generic_rx64m\resetprg.c(854): /* The delay period needed is to make sure that the sub-clock has stabilized. */ generic_rx64m\resetprg.c(859): /* ---- Set wait time until the sub-clock oscillator stabilizes ---- */ generic_rx64m\r_bsp_config_reference.h(247): 3 = Sub-Clock Oscillator generic_rx64m\r_bsp_config_reference.h(252): /* The sub-clock oscillation control for using the RTC. generic_rx64m\r_bsp_config_reference.h(253): When '1' is selected, the registers related to RTC are initialized and the sub-clock oscillator is operated. generic_rx64m\r_bsp_config_reference.h(259): /* Sub-Clock Oscillator Drive Capacity Control (RTCDV). generic_rx64m\r_bsp_config_reference.h(391): /* Sub-Clock Oscillator Wait Time (SOSCWTCR). generic_rx64m\r_bsp_config_reference.h(393): by the sub-clock oscillator is obtained by using the maximum frequency for fLOCO in the formula below. generic_rx64m\r_bsp_config_reference.h(396): (tSUBOSC: sub-clock oscillation stabilization time; fLOCO_max: maximum frequency for fLOCO) generic_rx65n\resetprg.c(32): * Changed the sub-clock oscillator settings. generic_rx65n\resetprg.c(633): /* Sub-clock setting. */ generic_rx65n\resetprg.c(638): /* Stop the sub-clock oscillator */ generic_rx65n\resetprg.c(641): b0 RCKSEL - Count Source Select - Sub-clock oscillator is selected. */ generic_rx65n\resetprg.c(659): b3:b1 RTCDV - Sub-clock oscillator Drive Ability Control. generic_rx65n\resetprg.c(660): b0 RTCEN - Sub-clock oscillator is stopped. */ generic_rx65n\resetprg.c(676): /* SOSCCR - Sub-Clock Oscillator Control Register generic_rx65n\resetprg.c(678): b0 SOSTP - Sub-clock oscillator Stop - Sub-clock oscillator is stopped. */ generic_rx65n\resetprg.c(692): /* The delay period needed is to make sure that the sub-clock has stopped. */ generic_rx65n\resetprg.c(696): /* Set the drive capacity of the sub-clock oscillator */ generic_rx65n\resetprg.c(720): /* Set wait time until the sub-clock oscillator stabilizes */ generic_rx65n\resetprg.c(721): /* SOSCWTCR - Sub-Clock Oscillator Wait Control Register generic_rx65n\resetprg.c(723): b4:b0 SSTS - Sub-Clock Oscillator Waiting Time - Waiting time is 2.044ms(the maximum value of fLOCO). */ generic_rx65n\resetprg.c(726): /* Operate the Sub-clock oscillator */ generic_rx65n\resetprg.c(740): /* The delay period needed is to make sure that the sub-clock has stabilized. */ generic_rx65n\resetprg.c(745): /* ---- Set wait time until the sub-clock oscillator stabilizes ---- */ generic_rx65n\resetprg.c(748): /* ---- Operate the sub-clock oscillator ---- */ generic_rx65n\resetprg.c(766): /* Wait for six the sub-clock cycles */ generic_rx65n\resetprg.c(767): /* 6 count of sub-clock : (1000000/32768)*6=183.10546875us generic_rx65n\resetprg.c(811): /* Wait for one the sub-clock cycles */ generic_rx65n\resetprg.c(812): /* 1 count of sub-clock : (1000000/32768)=30.517578125us generic_rx65n\resetprg.c(828): /* SOSCCR - Sub-Clock Oscillator Control Register generic_rx65n\resetprg.c(830): b0 SOSTP - Sub-clock oscillator Stop - Sub-clock oscillator is stopped. */ generic_rx65n\resetprg.c(849): /* Set wait time until the sub-clock oscillator stabilizes */ generic_rx65n\resetprg.c(850): /* SOSCWTCR - Sub-Clock Oscillator Wait Control Register generic_rx65n\resetprg.c(852): b4:b0 SSTS - Sub-Clock Oscillator Waiting Time - Waiting time is 2.044ms(the maximum value of fLOCO). */ generic_rx65n\resetprg.c(855): /* Operate the Sub-clock oscillator */ generic_rx65n\resetprg.c(871): /* The delay period needed is to make sure that the sub-clock has stabilized. */ generic_rx65n\resetprg.c(876): /* ---- Set wait time until the sub-clock oscillator stabilizes ---- */ generic_rx65n\r_bsp_config_reference.h(217): 3 = Sub-Clock Oscillator generic_rx65n\r_bsp_config_reference.h(228): /* The sub-clock oscillation control for using the RTC. generic_rx65n\r_bsp_config_reference.h(229): When '1' is selected, the registers related to RTC are initialized and the sub-clock oscillator is operated. generic_rx65n\r_bsp_config_reference.h(235): /* Sub-Clock Oscillator Drive Capacity Control (RTCDV). generic_rx65n\r_bsp_config_reference.h(361): /* Sub-Clock Oscillator Wait Time (SOSCWTCR). generic_rx65n\r_bsp_config_reference.h(363): by the sub-clock oscillator is obtained by using the maximum frequency for fLOCO in the formula below. generic_rx65n\r_bsp_config_reference.h(366): (tSUBOSC: sub-clock oscillation stabilization time; fLOCO_max: maximum frequency for fLOCO) generic_rx71m\resetprg.c(34): * - Sub-Clock Oscillator Wait Control Register (SOSCWTCR) generic_rx71m\resetprg.c(37): * Changed the sub-clock oscillator settings. generic_rx71m\resetprg.c(620): /* Sub-clock setting. */ generic_rx71m\resetprg.c(625): /* Stop the sub-clock oscillator */ generic_rx71m\resetprg.c(628): b0 RCKSEL - Count Source Select - Sub-clock oscillator is selected. */ generic_rx71m\resetprg.c(646): b3:b1 RTCDV - Sub-clock oscillator Drive Ability Control. generic_rx71m\resetprg.c(647): b0 RTCEN - Sub-clock oscillator is stopped. */ generic_rx71m\resetprg.c(663): /* SOSCCR - Sub-Clock Oscillator Control Register generic_rx71m\resetprg.c(665): b0 SOSTP - Sub-clock oscillator Stop - Sub-clock oscillator is stopped. */ generic_rx71m\resetprg.c(679): /* The delay period needed is to make sure that the sub-clock has stopped. */ generic_rx71m\resetprg.c(683): /* Set the drive capacity of the sub-clock oscillator */ generic_rx71m\resetprg.c(707): /* Set wait time until the sub-clock oscillator stabilizes */ generic_rx71m\resetprg.c(708): /* SOSCWTCR - Sub-Clock Oscillator Wait Control Register generic_rx71m\resetprg.c(710): b4:b0 SSTS - Sub-Clock Oscillator Waiting Time - Waiting time is 2.044ms(the maximum value of fLOCO). */ generic_rx71m\resetprg.c(713): /* Operate the Sub-clock oscillator */ generic_rx71m\resetprg.c(727): /* The delay period needed is to make sure that the sub-clock has stabilized. */ generic_rx71m\resetprg.c(732): /* ---- Set wait time until the sub-clock oscillator stabilizes ---- */ generic_rx71m\resetprg.c(735): /* ---- Operate the sub-clock oscillator ---- */ generic_rx71m\resetprg.c(753): /* Wait for six the sub-clock cycles */ generic_rx71m\resetprg.c(754): /* 6 count of sub-clock : (1000000/32768)*6=183.10546875us generic_rx71m\resetprg.c(798): /* Wait for one the sub-clock cycles */ generic_rx71m\resetprg.c(799): /* 1 count of sub-clock : (1000000/32768)=30.517578125us generic_rx71m\resetprg.c(815): /* SOSCCR - Sub-Clock Oscillator Control Register generic_rx71m\resetprg.c(817): b0 SOSTP - Sub-clock oscillator Stop - Sub-clock oscillator is stopped. */ generic_rx71m\resetprg.c(836): /* Set wait time until the sub-clock oscillator stabilizes */ generic_rx71m\resetprg.c(837): /* SOSCWTCR - Sub-Clock Oscillator Wait Control Register generic_rx71m\resetprg.c(839): b4:b0 SSTS - Sub-Clock Oscillator Waiting Time - Waiting time is 2.044ms(the maximum value of fLOCO). */ generic_rx71m\resetprg.c(842): /* Operate the Sub-clock oscillator */ generic_rx71m\resetprg.c(858): /* The delay period needed is to make sure that the sub-clock has stabilized. */ generic_rx71m\resetprg.c(863): /* ---- Set wait time until the sub-clock oscillator stabilizes ---- */ generic_rx71m\r_bsp_config_reference.h(236): 3 = Sub-Clock Oscillator generic_rx71m\r_bsp_config_reference.h(241): /* The sub-clock oscillation control for using the RTC. generic_rx71m\r_bsp_config_reference.h(242): When '1' is selected, the registers related to RTC are initialized and the sub-clock oscillator is operated. generic_rx71m\r_bsp_config_reference.h(248): /* Sub-Clock Oscillator Drive Capacity Control (RTCDV). generic_rx71m\r_bsp_config_reference.h(380): /* Sub-Clock Oscillator Wait Time (SOSCWTCR). generic_rx71m\r_bsp_config_reference.h(382): by the sub-clock oscillator is obtained by using the maximum frequency for fLOCO in the formula below. generic_rx71m\r_bsp_config_reference.h(385): (tSUBOSC: sub-clock oscillation stabilization time; fLOCO_max: maximum frequency for fLOCO) hsbrx21ap\resetprg.c(475): /* Sub-clock oscillator is chosen. Start it operating. */ hsbrx21ap\resetprg.c(479): /* Set the sub-clock to operating. */ hsbrx21ap\resetprg.c(482): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's hsbrx21ap\resetprg.c(493): /* Set the sub-clock to stopped. */ hsbrx21ap\r_bsp_config_reference.h(184): 3 = Sub-Clock Oscillator rdkrx631\resetprg.c(501): /* Sub-clock oscillator is chosen. Start it operating. */ rdkrx631\resetprg.c(505): /* Set the sub-clock to operating. */ rdkrx631\resetprg.c(508): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rdkrx631\resetprg.c(519): /* Set the sub-clock to stopped. */ rdkrx631\r_bsp_config_reference.h(270): 3 = Sub-Clock Oscillator rdkrx63n\resetprg.c(503): /* Sub-clock oscillator is chosen. Start it operating. */ rdkrx63n\resetprg.c(507): /* Set the sub-clock to operating. */ rdkrx63n\resetprg.c(510): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rdkrx63n\resetprg.c(521): /* Set the sub-clock to stopped. */ rdkrx63n\r_bsp_config_reference.h(269): 3 = Sub-Clock Oscillator rskrx210\resetprg.c(498): /* Sub-clock oscillator is chosen. Start it operating. */ rskrx210\resetprg.c(500): SYSTEM.SOSCCR.BYTE = 0x01; // Make sure sub-clock is initially stopped rskrx210\resetprg.c(523): /* ---- Wait for five sub-clock cycles ---- */ rskrx210\resetprg.c(524): /* Wait time is 5 sub-clock cycles (approx. 152 us). rskrx210\resetprg.c(531): RTC.RCR3.BYTE = REG_RCR3; // Restore original sub-clock and state rskrx210\resetprg.c(540): /* Set the sub-clock to operating. */ rskrx210\resetprg.c(543): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rskrx210\resetprg.c(554): /* Set the sub-clock to stopped. */ rskrx210\resetprg.c(749): /* Sub-clock oscillator is chosen. Start it operating. */ rskrx210\resetprg.c(753): /* Set the sub-clock to stopped. */ rskrx210\r_bsp_config_reference.h(230): 3 = Sub-Clock Oscillator rskrx220\resetprg.c(403): /* Sub-clock oscillator is chosen. Start it operating. */ rskrx220\resetprg.c(407): /* Set the sub-clock to operating. */ rskrx220\resetprg.c(410): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rskrx220\resetprg.c(421): /* Set the sub-clock to stopped. */ rskrx220\r_bsp_config_reference.h(187): 3 = Sub-Clock Oscillator rskrx23t\r_bsp_config_reference.h(194): 3 = Sub-Clock Oscillator (N/A for RX23T) rskrx24t\r_bsp_config_reference.h(195): 3 = Sub-Clock Oscillator (N/A for RX24T) rskrx24u\r_bsp_config_reference.h(182): 3 = Sub-Clock Oscillator (N/A for RX24U) rskrx630\resetprg.c(471): /* Sub-clock oscillator is chosen. Start it operating. */ rskrx630\resetprg.c(475): /* Set the sub-clock to operating. */ rskrx630\resetprg.c(478): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rskrx630\resetprg.c(489): /* Set the sub-clock to stopped. */ rskrx630\r_bsp_config_reference.h(224): 3 = Sub-Clock Oscillator rskrx631\resetprg.c(501): /* Sub-clock oscillator is chosen. Start it operating. */ rskrx631\resetprg.c(505): /* Set the sub-clock to operating. */ rskrx631\resetprg.c(508): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rskrx631\resetprg.c(519): /* Set the sub-clock to stopped. */ rskrx631\r_bsp_config_reference.h(272): 3 = Sub-Clock Oscillator rskrx63n\resetprg.c(504): /* Sub-clock oscillator is chosen. Start it operating. */ rskrx63n\resetprg.c(508): /* Set the sub-clock to operating. */ rskrx63n\resetprg.c(511): /* The delay period needed is to make sure that the sub-clock has stabilized. According to Rev.1.00 of the RX63N's rskrx63n\resetprg.c(522): /* Set the sub-clock to stopped. */ rskrx63n\r_bsp_config_reference.h(272): 3 = Sub-Clock Oscillator rsskrx23t\r_bsp_config_reference.h(180): 3 = Sub-Clock Oscillator (N/A for RX23T)