/*********************************************************************************************************************** * DISCLAIMER * This software is supplied by Renesas Electronics Corporation and is only intended for use with Renesas products. No * other uses are authorized. This software is owned by Renesas Electronics Corporation and is protected under all * applicable laws, including copyright laws. * THIS SOFTWARE IS PROVIDED "AS IS" AND RENESAS MAKES NO WARRANTIES REGARDING * THIS SOFTWARE, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING BUT NOT LIMITED TO WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. ALL SUCH WARRANTIES ARE EXPRESSLY DISCLAIMED. TO THE MAXIMUM * EXTENT PERMITTED NOT PROHIBITED BY LAW, NEITHER RENESAS ELECTRONICS CORPORATION NOR ANY OF ITS AFFILIATED COMPANIES * SHALL BE LIABLE FOR ANY DIRECT, INDIRECT, SPECIAL, INCIDENTAL OR CONSEQUENTIAL DAMAGES FOR ANY REASON RELATED TO THIS * SOFTWARE, EVEN IF RENESAS OR ITS AFFILIATES HAVE BEEN ADVISED OF THE POSSIBILITY OF SUCH DAMAGES. * Renesas reserves the right, without notice, to make changes to this software and to discontinue the availability of * this software. By using this software, you agree to the additional terms and conditions found by accessing the * following link: * http://www.renesas.com/disclaimer * * Copyright (C) 2015(2016) Renesas Electronics Corporation. All rights reserved. ***********************************************************************************************************************/ /******************************************************************************* * File Name : r_usb_pcdc_echo_apl.c * Description : USB Peripheral Communications Devices Class Sample Code ******************************************************************************* * History : DD.MM.YYYY Version Description * : 30.09.2015 2.20 First Release * : 30.09.2016 2.30 Using new USB API. ******************************************************************************/ /****************************************************************************** Includes , "Project Includes" ******************************************************************************/ #include "r_usb_pcdc_apl.h" #if OPERATION_MODE == USB_ECHO /****************************************************************************** Macro definitions ***************************************************************************#***/ /****************************************************************************** Private global variables and functions ******************************************************************************/ static void usb_pin_setting (void); static uint8_t g_buf[DATA_LEN]; const static usb_descriptor_t usb_descriptor = { g_apl_device, /* Pointer to the device descriptor */ g_apl_configuration, /* Pointer to the configuration descriptor for Full-speed */ USB_NULL, /* Pointer to the configuration descriptor for Hi-speed */ USB_NULL, /* Pointer to the qualifier descriptor */ g_apl_string_table /* Pointer to the string descriptor table */ }; /****************************************************************************** Renesas Peripheral Communications Devices Class Sample Code functions ******************************************************************************/ /****************************************************************************** Function Name : usb_main Description : Peripheral CDC application main process Arguments : none Return value : none ******************************************************************************/ void usb_main (void) { usb_ctrl_t ctrl; usb_cfg_t cfg; usb_pin_setting(); /* USB MCU pin setting */ ctrl.module = USE_USBIP; ctrl.type = USB_PCDC; cfg.usb_speed = USB_SUPPORT_SPEED; /* USB_HS/USB_FS */ cfg.usb_mode = USB_PERI; cfg.p_usb_reg = (usb_descriptor_t *)&usb_descriptor; R_USB_Open(&ctrl, &cfg); /* Initializes the USB module */ /* Loop back between PC(TerminalSoft) and USB MCU */ while (1) { switch (R_USB_GetEvent(&ctrl)) { case USB_STS_CONFIGURED : case USB_STS_WRITE_COMPLETE : ctrl.type = USB_PCDC; R_USB_Read(&ctrl, g_buf, DATA_LEN); break; case USB_STS_READ_COMPLETE : R_USB_Write(&ctrl, g_buf, ctrl.size); break; case USB_STS_SUSPEND : case USB_STS_DETACH : #if defined(USE_LPW) low_power_mcu(); #endif /* defined(USE_LPW) */ break; default : break; } } } /* End of function usb_main() */ /****************************************************************************** Function Name : usb_pin_setting Description : USB Pin Setting Arguments : none Return value : none ******************************************************************************/ /*---CUT---CUT---CUT---CUT---CUT---CUT---CUT---CUT---CUT---CUT---CUT---CUT---*/ #endif /* OPERATION_MODE == USB_ECHO */ /****************************************************************************** End Of File ******************************************************************************/