/*********************************************************************************************************************** * DISCLAIMER * This software is supplied by Renesas Electronics Corporation and is only intended for use with Renesas products. * No other uses are authorized. This software is owned by Renesas Electronics Corporation and is protected under all * applicable laws, including copyright laws. * THIS SOFTWARE IS PROVIDED "AS IS" AND RENESAS MAKES NO WARRANTIES REGARDING THIS SOFTWARE, WHETHER EXPRESS, IMPLIED * OR STATUTORY, INCLUDING BUT NOT LIMITED TO WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND * NON-INFRINGEMENT. ALL SUCH WARRANTIES ARE EXPRESSLY DISCLAIMED.TO THE MAXIMUM EXTENT PERMITTED NOT PROHIBITED BY * LAW, NEITHER RENESAS ELECTRONICS CORPORATION NOR ANY OF ITS AFFILIATED COMPANIES SHALL BE LIABLE FOR ANY DIRECT, * INDIRECT, SPECIAL, INCIDENTAL OR CONSEQUENTIAL DAMAGES FOR ANY REASON RELATED TO THIS SOFTWARE, EVEN IF RENESAS OR * ITS AFFILIATES HAVE BEEN ADVISED OF THE POSSIBILITY OF SUCH DAMAGES. * Renesas reserves the right, without notice, to make changes to this software and to discontinue the availability * of this software. By using this software, you agree to the additional terms and conditions found by accessing the * following link: * http://www.renesas.com/disclaimer * * Copyright (C) 2022 Renesas Electronics Corporation. All rights reserved. ***********************************************************************************************************************/ /*********************************************************************************************************************** * File Name : Config_CMT3_user.c * Component Version: 2.3.0 * Device(s) : R5F566NNHxFP * Description : This file implements device driver for Config_CMT3. ***********************************************************************************************************************/ /*********************************************************************************************************************** Pragma directive ***********************************************************************************************************************/ /* Start user code for pragma. Do not edit comment generated here */ /* End user code. Do not edit comment generated here */ /*********************************************************************************************************************** Includes ***********************************************************************************************************************/ #include "r_cg_macrodriver.h" #include "Config_CMT3.h" /* Start user code for include. Do not edit comment generated here */ #include "MultiSuperLoop.h" /* End user code. Do not edit comment generated here */ #include "r_cg_userdefine.h" /*********************************************************************************************************************** Global variables and functions ***********************************************************************************************************************/ /* Start user code for global. Do not edit comment generated here */ R_BSP_PRAGMA_STATIC_INLINE(MultiSuperLoop_Dispatch) void MultiSuperLoop_Dispatch(void) { R_BSP_ASM_BEGIN /* Re-enable interrupt. */ R_BSP_ASM( setpsw i ) /* Save the current super loop context. Be aware that the USP is used from now. */ /* (As of today, the DPFPU registers are neither saved nor restored.) */ R_BSP_ASM( setpsw u ) R_BSP_ASM( sub U_BSP_ASM_IMM(8), r0 ) R_BSP_ASM( push.l r1 ) R_BSP_ASM( mov.l U_BSP_ASM_IMM(_SuperLoopContextTable), r1 ) R_BSP_ASM( mov.b 16[r1], r1 ) R_BSP_ASM( save r1 ) /* Move PSW, PC from the interrupt stack to the current super loop's user stack. */ R_BSP_ASM( mvfc isp, r2 ) R_BSP_ASM( mov.l 4[r2], 8[r0] ) R_BSP_ASM( mov.l 0[r2], 4[r0] ) R_BSP_ASM( add U_BSP_ASM_IMM(8), r2 ) R_BSP_ASM( mvtc r2, isp ) /* Select the next super loop. */ R_BSP_ASM( mov.l U_BSP_ASM_IMM(_SuperLoopContextTable), r2 ) R_BSP_ASM( add r2, r1 ) R_BSP_ASM( mov.b [r1], r1 ) R_BSP_ASM( mov.b r1, 16[r2] ) /* Restore the next super loop context. Be aware that the USP is used here. */ /* (As of today, the DPFPU registers are neither saved nor restored.) */ R_BSP_ASM( rstr r1 ) R_BSP_ASM( pop r1 ) R_BSP_ASM( rte ) R_BSP_ASM_END } /* End user code. Do not edit comment generated here */ /*********************************************************************************************************************** * Function Name: R_Config_CMT3_Create_UserInit * Description : This function adds user code after initializing the CMT3 channel * Arguments : None * Return Value : None ***********************************************************************************************************************/ void R_Config_CMT3_Create_UserInit(void) { /* Start user code for user init. Do not edit comment generated here */ /* End user code. Do not edit comment generated here */ } /*********************************************************************************************************************** * Function Name: r_Config_CMT3_cmi3_interrupt * Description : This function is CMI3 interrupt service routine * Arguments : None * Return Value : None ***********************************************************************************************************************/ #pragma vector = VECT_PERIB_INTB129 #if FAST_INTERRUPT_VECTOR == VECT_PERIB_INTB129 __fast_interrupt static void r_Config_CMT3_cmi3_interrupt(void) #else __interrupt static void r_Config_CMT3_cmi3_interrupt(void) #endif { /* Start user code for r_Config_CMT3_cmi3_interrupt. Do not edit comment generated here */ MultiSuperLoop_Dispatch(); /* End user code. Do not edit comment generated here */ } /* Start user code for adding. Do not edit comment generated here */ R_BSP_PRAGMA_STATIC_INLINE_ASM(_Initialize_RegisterSaveBank) void _Initialize_RegisterSaveBank(uint32_t pc, uint32_t usp, uint32_t bank) { R_BSP_ASM_INTERNAL_USED(pc) /* r1 */ R_BSP_ASM_INTERNAL_USED(usp) /* r2 */ R_BSP_ASM_INTERNAL_USED(bank) /* r3 */ R_BSP_ASM_BEGIN /* Save PSW, USP to scratch registers and disable interrupt. */ R_BSP_ASM( mvfc psw, r4 ) R_BSP_ASM( clrpsw i ) R_BSP_ASM( mvfc usp, r5 ) /* Initialize the specified register save bank. */ R_BSP_ASM( sub U_BSP_ASM_IMM(12), r2 ) /* Reserve the space for PSW, PC and R1. */ R_BSP_ASM( mvtc r2, usp ) /* usp */ R_BSP_ASM( mov.l r4, 8[r2] ) /* psw */ R_BSP_ASM( mov.l r1, 4[r2] ) /* pc */ R_BSP_ASM( mov.l U_BSP_ASM_IMM(0), 0[r2] ) /* r1 but the value isn't important. */ R_BSP_ASM( save r3 ) /* Only the value of USP and FPSW are important. */ /* Restore PSW, USP from scratch registers. */ R_BSP_ASM( mvtc r5, usp ) R_BSP_ASM( mvtc r4, psw ) R_BSP_ASM_END } static void Initialize_RegisterSaveBank(uint32_t pc, uint32_t usp, uint32_t bank) { (void) pc; /* r1 */ (void) usp; /* r2 */ (void) bank; /* r3 */ _Initialize_RegisterSaveBank(pc, usp, bank); } void MultiSuperLoop_Add_Loop1(void (*pc)(void), uint8_t *usp) { /* Prevent the debugger from messing up unwinding of the stack. */ usp = (uint8_t *)usp - sizeof(uint32_t); *(uint32_t *)usp = 0; Initialize_RegisterSaveBank((uint32_t)pc, (uint32_t)usp, 1); SuperLoopContextTable[16] = 0; SuperLoopContextTable[ 0] = 1; SuperLoopContextTable[ 1] = 0; SuperLoopContextTable[ 2] = 255; SuperLoopContextTable[ 3] = 255; SuperLoopContextTable[ 4] = 255; SuperLoopContextTable[ 5] = 255; SuperLoopContextTable[ 6] = 255; SuperLoopContextTable[ 7] = 255; SuperLoopContextTable[ 8] = 255; SuperLoopContextTable[ 9] = 255; SuperLoopContextTable[10] = 255; SuperLoopContextTable[11] = 255; SuperLoopContextTable[12] = 255; SuperLoopContextTable[13] = 255; SuperLoopContextTable[14] = 255; SuperLoopContextTable[15] = 255; R_Config_CMT3_Start(); } void MultiSuperLoop_Yield(void) { uint8_t ipl = get_ipl(); if (ipl == 0) { set_ipl(1); } /* Switch to the next super loop. Be aware that the value of IPL is */ /* also switched to the value which is used in the next super loop. */ int_exception(VECT(PERIB,INTB129)); if (ipl == 0) { set_ipl(0); } } /* End user code. Do not edit comment generated here */