/* * NORTi_interrupt.c * * Created on: Jun 24, 2022 * Last Modified on: Jun 29, 2022 9:00 * Author: NoMaY * License: MIT */ #include "NORTi_interrupt.h" #include static void (* const Int_Hook_Vectors[])(void); void NORTi_INT_HOOK_init(void) { set_intb((void *)Int_Hook_Vectors); } static void dummy_NORTi_INT_HOOK(void) { // To prevent developers from being misled regarding the following inline assemble error. // E0552111:Symbol is undefined for(;;); } #pragma inline_asm INT_COMMON_nonOS static void INT_COMMON_nonOS(void) { XCHG [SP], R15 // the address of hook_entry_XXX --> R15 ADD #(- (__$hook_entry___0 + 7)), R15 // 7 = 4 * size of NOP + size of BSR.W SHLR #1, R15 ADD #TOPOF C$VECT, R15 // i.e. C$VECT + ((hook_entry_XXX - hook_entry___0) / 8) * 4 --> R15 MOV.L [R15], R15 XCHG [SP], R15 RTS // i.e. JMP [SP+] } #pragma inline_asm INT_COMMON_NORTi static void INT_COMMON_NORTi(void) { POP R15 // the address of hook_entry_XXX --> R15 ADD #(- (__$hook_entry___0 + 7)), R15 // 7 = size of BSR.A + size of BSR.W SHLR #1, R15 ADD #TOPOF C$VECT, R15 // i.e. C$VECT + ((hook_entry_XXX - hook_entry___0) / 8) * 4 --> R15 MOV.L [R15], R15 PUSHC PSW MOV.L #?+, R14 PUSH.L R14 JMP R15 // Program will return to the next label from the interrupt service routine by RTE. ?: BRA.A _v3_ret_int // Call NORTi API (in this case, jump to NORTi). } #pragma inline_asm INT_ENTRY_nonOS static void INT_ENTRY_nonOS(void) { NOP NOP NOP NOP BSR.W __$INT_COMMON_nonOS } #pragma inline_asm INT_ENTRY_NORTi static void INT_ENTRY_NORTi(void) { BSR.A _v3_ent_int // Call NORTi API. BSR.W __$INT_COMMON_NORTi } // Documents // https://www.mispo.co.jp/document/no4guid.pdf // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv3-instruction-set-architecture-users-manual-software-rev100 // Labels and functions extern void v3_ent_int(void); extern void v3_ret_int (void); static void INT_COMMON_nonOS(void); static void INT_COMMON_NORTi(void); // To prevent the symbol from being optimized out. void * const dummy_NORTi_INT_enter = (void *)v3_ent_int; void * const dummy_NORTi_INT_return = (void *)v3_ret_int; void * const dummy_INT_COMMON_nonOS = (void *)INT_COMMON_nonOS; void * const dummy_INT_COMMON_NORTi = (void *)INT_COMMON_NORTi; // To prevent the section name symbol `C$VECT` from being optimized out. void * const dummy_VECTTBL = (void *)__sectop("C$VECT"); // To prevent a compile warning. void * const dummy2_NORTi_INT_HOOK = (void *)dummy_NORTi_INT_HOOK; // The code size of the following functions is just 8 bytes. // For nonOS // 00000000 03 NOP // 00000001 03 NOP // 00000002 03 NOP // 00000003 03 NOP // 00000004 39rrrr W BSR.W __$INT_COMMON_nonOS // 00000007 02 RTS // Not used. // For NORTi // 00000000 05rrrrrr A BSR.A _v3_ret_int // 00000004 39rrrr W BSR.W __$INT_COMMON_NORTi // 00000007 02 RTS // Not used. #define _INT_ENTRY(sel) INT_ENTRY_##sel() #define INT_ENTRY(sel) _INT_ENTRY(sel) static void hook_entry___0(void) { INT_ENTRY(INTERRUPT___0); } static void hook_entry___1(void) { INT_ENTRY(INTERRUPT___1); } static void hook_entry___2(void) { INT_ENTRY(INTERRUPT___2); } static void hook_entry___3(void) { INT_ENTRY(INTERRUPT___3); } static void hook_entry___4(void) { INT_ENTRY(INTERRUPT___4); } static void hook_entry___5(void) { INT_ENTRY(INTERRUPT___5); } static void hook_entry___6(void) { INT_ENTRY(INTERRUPT___6); } static void hook_entry___7(void) { INT_ENTRY(INTERRUPT___7); } static void hook_entry___8(void) { INT_ENTRY(INTERRUPT___8); } static void hook_entry___9(void) { INT_ENTRY(INTERRUPT___9); } static void hook_entry__10(void) { INT_ENTRY(INTERRUPT__10); } static void hook_entry__11(void) { INT_ENTRY(INTERRUPT__11); } static void hook_entry__12(void) { INT_ENTRY(INTERRUPT__12); } static void hook_entry__13(void) { INT_ENTRY(INTERRUPT__13); } static void hook_entry__14(void) { INT_ENTRY(INTERRUPT__14); } static void hook_entry__15(void) { INT_ENTRY(INTERRUPT__15); } static void hook_entry__16(void) { INT_ENTRY(INTERRUPT__16); } static void hook_entry__17(void) { INT_ENTRY(INTERRUPT__17); } static void hook_entry__18(void) { INT_ENTRY(INTERRUPT__18); } static void hook_entry__19(void) { INT_ENTRY(INTERRUPT__19); } static void hook_entry__20(void) { INT_ENTRY(INTERRUPT__20); } static void hook_entry__21(void) { INT_ENTRY(INTERRUPT__21); } static void hook_entry__22(void) { INT_ENTRY(INTERRUPT__22); } static void hook_entry__23(void) { INT_ENTRY(INTERRUPT__23); } static void hook_entry__24(void) { INT_ENTRY(INTERRUPT__24); } static void hook_entry__25(void) { INT_ENTRY(INTERRUPT__25); } static void hook_entry__26(void) { INT_ENTRY(INTERRUPT__26); } static void hook_entry__27(void) { INT_ENTRY(INTERRUPT__27); } static void hook_entry__28(void) { INT_ENTRY(INTERRUPT__28); } static void hook_entry__29(void) { INT_ENTRY(INTERRUPT__29); } static void hook_entry__30(void) { INT_ENTRY(INTERRUPT__30); } static void hook_entry__31(void) { INT_ENTRY(INTERRUPT__31); } static void hook_entry__32(void) { INT_ENTRY(INTERRUPT__32); } static void hook_entry__33(void) { INT_ENTRY(INTERRUPT__33); } static void hook_entry__34(void) { INT_ENTRY(INTERRUPT__34); } static void hook_entry__35(void) { INT_ENTRY(INTERRUPT__35); } static void hook_entry__36(void) { INT_ENTRY(INTERRUPT__36); } static void hook_entry__37(void) { INT_ENTRY(INTERRUPT__37); } static void hook_entry__38(void) { INT_ENTRY(INTERRUPT__38); } static void hook_entry__39(void) { INT_ENTRY(INTERRUPT__39); } static void hook_entry__40(void) { INT_ENTRY(INTERRUPT__40); } static void hook_entry__41(void) { INT_ENTRY(INTERRUPT__41); } static void hook_entry__42(void) { INT_ENTRY(INTERRUPT__42); } static void hook_entry__43(void) { INT_ENTRY(INTERRUPT__43); } static void hook_entry__44(void) { INT_ENTRY(INTERRUPT__44); } static void hook_entry__45(void) { INT_ENTRY(INTERRUPT__45); } static void hook_entry__46(void) { INT_ENTRY(INTERRUPT__46); } static void hook_entry__47(void) { INT_ENTRY(INTERRUPT__47); } static void hook_entry__48(void) { INT_ENTRY(INTERRUPT__48); } static void hook_entry__49(void) { INT_ENTRY(INTERRUPT__49); } static void hook_entry__50(void) { INT_ENTRY(INTERRUPT__50); } static void hook_entry__51(void) { INT_ENTRY(INTERRUPT__51); } static void hook_entry__52(void) { INT_ENTRY(INTERRUPT__52); } static void hook_entry__53(void) { INT_ENTRY(INTERRUPT__53); } static void hook_entry__54(void) { INT_ENTRY(INTERRUPT__54); } static void hook_entry__55(void) { INT_ENTRY(INTERRUPT__55); } static void hook_entry__56(void) { INT_ENTRY(INTERRUPT__56); } static void hook_entry__57(void) { INT_ENTRY(INTERRUPT__57); } static void hook_entry__58(void) { INT_ENTRY(INTERRUPT__58); } static void hook_entry__59(void) { INT_ENTRY(INTERRUPT__59); } static void hook_entry__60(void) { INT_ENTRY(INTERRUPT__60); } static void hook_entry__61(void) { INT_ENTRY(INTERRUPT__61); } static void hook_entry__62(void) { INT_ENTRY(INTERRUPT__62); } static void hook_entry__63(void) { INT_ENTRY(INTERRUPT__63); } static void hook_entry__64(void) { INT_ENTRY(INTERRUPT__64); } static void hook_entry__65(void) { INT_ENTRY(INTERRUPT__65); } static void hook_entry__66(void) { INT_ENTRY(INTERRUPT__66); } static void hook_entry__67(void) { INT_ENTRY(INTERRUPT__67); } static void hook_entry__68(void) { INT_ENTRY(INTERRUPT__68); } static void hook_entry__69(void) { INT_ENTRY(INTERRUPT__69); } static void hook_entry__70(void) { INT_ENTRY(INTERRUPT__70); } static void hook_entry__71(void) { INT_ENTRY(INTERRUPT__71); } static void hook_entry__72(void) { INT_ENTRY(INTERRUPT__72); } static void hook_entry__73(void) { INT_ENTRY(INTERRUPT__73); } static void hook_entry__74(void) { INT_ENTRY(INTERRUPT__74); } static void hook_entry__75(void) { INT_ENTRY(INTERRUPT__75); } static void hook_entry__76(void) { INT_ENTRY(INTERRUPT__76); } static void hook_entry__77(void) { INT_ENTRY(INTERRUPT__77); } static void hook_entry__78(void) { INT_ENTRY(INTERRUPT__78); } static void hook_entry__79(void) { INT_ENTRY(INTERRUPT__79); } static void hook_entry__80(void) { INT_ENTRY(INTERRUPT__80); } static void hook_entry__81(void) { INT_ENTRY(INTERRUPT__81); } static void hook_entry__82(void) { INT_ENTRY(INTERRUPT__82); } static void hook_entry__83(void) { INT_ENTRY(INTERRUPT__83); } static void hook_entry__84(void) { INT_ENTRY(INTERRUPT__84); } static void hook_entry__85(void) { INT_ENTRY(INTERRUPT__85); } static void hook_entry__86(void) { INT_ENTRY(INTERRUPT__86); } static void hook_entry__87(void) { INT_ENTRY(INTERRUPT__87); } static void hook_entry__88(void) { INT_ENTRY(INTERRUPT__88); } static void hook_entry__89(void) { INT_ENTRY(INTERRUPT__89); } static void hook_entry__90(void) { INT_ENTRY(INTERRUPT__90); } static void hook_entry__91(void) { INT_ENTRY(INTERRUPT__91); } static void hook_entry__92(void) { INT_ENTRY(INTERRUPT__92); } static void hook_entry__93(void) { INT_ENTRY(INTERRUPT__93); } static void hook_entry__94(void) { INT_ENTRY(INTERRUPT__94); } static void hook_entry__95(void) { INT_ENTRY(INTERRUPT__95); } static void hook_entry__96(void) { INT_ENTRY(INTERRUPT__96); } static void hook_entry__97(void) { INT_ENTRY(INTERRUPT__97); } static void hook_entry__98(void) { INT_ENTRY(INTERRUPT__98); } static void hook_entry__99(void) { INT_ENTRY(INTERRUPT__99); } static void hook_entry_100(void) { INT_ENTRY(INTERRUPT_100); } static void hook_entry_101(void) { INT_ENTRY(INTERRUPT_101); } static void hook_entry_102(void) { INT_ENTRY(INTERRUPT_102); } static void hook_entry_103(void) { INT_ENTRY(INTERRUPT_103); } static void hook_entry_104(void) { INT_ENTRY(INTERRUPT_104); } static void hook_entry_105(void) { INT_ENTRY(INTERRUPT_105); } static void hook_entry_106(void) { INT_ENTRY(INTERRUPT_106); } static void hook_entry_107(void) { INT_ENTRY(INTERRUPT_107); } static void hook_entry_108(void) { INT_ENTRY(INTERRUPT_108); } static void hook_entry_109(void) { INT_ENTRY(INTERRUPT_109); } static void hook_entry_110(void) { INT_ENTRY(INTERRUPT_110); } static void hook_entry_111(void) { INT_ENTRY(INTERRUPT_111); } static void hook_entry_112(void) { INT_ENTRY(INTERRUPT_112); } static void hook_entry_113(void) { INT_ENTRY(INTERRUPT_113); } static void hook_entry_114(void) { INT_ENTRY(INTERRUPT_114); } static void hook_entry_115(void) { INT_ENTRY(INTERRUPT_115); } static void hook_entry_116(void) { INT_ENTRY(INTERRUPT_116); } static void hook_entry_117(void) { INT_ENTRY(INTERRUPT_117); } static void hook_entry_118(void) { INT_ENTRY(INTERRUPT_118); } static void hook_entry_119(void) { INT_ENTRY(INTERRUPT_119); } static void hook_entry_120(void) { INT_ENTRY(INTERRUPT_120); } static void hook_entry_121(void) { INT_ENTRY(INTERRUPT_121); } static void hook_entry_122(void) { INT_ENTRY(INTERRUPT_122); } static void hook_entry_123(void) { INT_ENTRY(INTERRUPT_123); } static void hook_entry_124(void) { INT_ENTRY(INTERRUPT_124); } static void hook_entry_125(void) { INT_ENTRY(INTERRUPT_125); } static void hook_entry_126(void) { INT_ENTRY(INTERRUPT_126); } static void hook_entry_127(void) { INT_ENTRY(INTERRUPT_127); } static void hook_entry_128(void) { INT_ENTRY(INTERRUPT_128); } static void hook_entry_129(void) { INT_ENTRY(INTERRUPT_129); } static void hook_entry_130(void) { INT_ENTRY(INTERRUPT_130); } static void hook_entry_131(void) { INT_ENTRY(INTERRUPT_131); } static void hook_entry_132(void) { INT_ENTRY(INTERRUPT_132); } static void hook_entry_133(void) { INT_ENTRY(INTERRUPT_133); } static void hook_entry_134(void) { INT_ENTRY(INTERRUPT_134); } static void hook_entry_135(void) { INT_ENTRY(INTERRUPT_135); } static void hook_entry_136(void) { INT_ENTRY(INTERRUPT_136); } static void hook_entry_137(void) { INT_ENTRY(INTERRUPT_137); } static void hook_entry_138(void) { INT_ENTRY(INTERRUPT_138); } static void hook_entry_139(void) { INT_ENTRY(INTERRUPT_139); } static void hook_entry_140(void) { INT_ENTRY(INTERRUPT_140); } static void hook_entry_141(void) { INT_ENTRY(INTERRUPT_141); } static void hook_entry_142(void) { INT_ENTRY(INTERRUPT_142); } static void hook_entry_143(void) { INT_ENTRY(INTERRUPT_143); } static void hook_entry_144(void) { INT_ENTRY(INTERRUPT_144); } static void hook_entry_145(void) { INT_ENTRY(INTERRUPT_145); } static void hook_entry_146(void) { INT_ENTRY(INTERRUPT_146); } static void hook_entry_147(void) { INT_ENTRY(INTERRUPT_147); } static void hook_entry_148(void) { INT_ENTRY(INTERRUPT_148); } static void hook_entry_149(void) { INT_ENTRY(INTERRUPT_149); } static void hook_entry_150(void) { INT_ENTRY(INTERRUPT_150); } static void hook_entry_151(void) { INT_ENTRY(INTERRUPT_151); } static void hook_entry_152(void) { INT_ENTRY(INTERRUPT_152); } static void hook_entry_153(void) { INT_ENTRY(INTERRUPT_153); } static void hook_entry_154(void) { INT_ENTRY(INTERRUPT_154); } static void hook_entry_155(void) { INT_ENTRY(INTERRUPT_155); } static void hook_entry_156(void) { INT_ENTRY(INTERRUPT_156); } static void hook_entry_157(void) { INT_ENTRY(INTERRUPT_157); } static void hook_entry_158(void) { INT_ENTRY(INTERRUPT_158); } static void hook_entry_159(void) { INT_ENTRY(INTERRUPT_159); } static void hook_entry_160(void) { INT_ENTRY(INTERRUPT_160); } static void hook_entry_161(void) { INT_ENTRY(INTERRUPT_161); } static void hook_entry_162(void) { INT_ENTRY(INTERRUPT_162); } static void hook_entry_163(void) { INT_ENTRY(INTERRUPT_163); } static void hook_entry_164(void) { INT_ENTRY(INTERRUPT_164); } static void hook_entry_165(void) { INT_ENTRY(INTERRUPT_165); } static void hook_entry_166(void) { INT_ENTRY(INTERRUPT_166); } static void hook_entry_167(void) { INT_ENTRY(INTERRUPT_167); } static void hook_entry_168(void) { INT_ENTRY(INTERRUPT_168); } static void hook_entry_169(void) { INT_ENTRY(INTERRUPT_169); } static void hook_entry_170(void) { INT_ENTRY(INTERRUPT_170); } static void hook_entry_171(void) { INT_ENTRY(INTERRUPT_171); } static void hook_entry_172(void) { INT_ENTRY(INTERRUPT_172); } static void hook_entry_173(void) { INT_ENTRY(INTERRUPT_173); } static void hook_entry_174(void) { INT_ENTRY(INTERRUPT_174); } static void hook_entry_175(void) { INT_ENTRY(INTERRUPT_175); } static void hook_entry_176(void) { INT_ENTRY(INTERRUPT_176); } static void hook_entry_177(void) { INT_ENTRY(INTERRUPT_177); } static void hook_entry_178(void) { INT_ENTRY(INTERRUPT_178); } static void hook_entry_179(void) { INT_ENTRY(INTERRUPT_179); } static void hook_entry_180(void) { INT_ENTRY(INTERRUPT_180); } static void hook_entry_181(void) { INT_ENTRY(INTERRUPT_181); } static void hook_entry_182(void) { INT_ENTRY(INTERRUPT_182); } static void hook_entry_183(void) { INT_ENTRY(INTERRUPT_183); } static void hook_entry_184(void) { INT_ENTRY(INTERRUPT_184); } static void hook_entry_185(void) { INT_ENTRY(INTERRUPT_185); } static void hook_entry_186(void) { INT_ENTRY(INTERRUPT_186); } static void hook_entry_187(void) { INT_ENTRY(INTERRUPT_187); } static void hook_entry_188(void) { INT_ENTRY(INTERRUPT_188); } static void hook_entry_189(void) { INT_ENTRY(INTERRUPT_189); } static void hook_entry_190(void) { INT_ENTRY(INTERRUPT_190); } static void hook_entry_191(void) { INT_ENTRY(INTERRUPT_191); } static void hook_entry_192(void) { INT_ENTRY(INTERRUPT_192); } static void hook_entry_193(void) { INT_ENTRY(INTERRUPT_193); } static void hook_entry_194(void) { INT_ENTRY(INTERRUPT_194); } static void hook_entry_195(void) { INT_ENTRY(INTERRUPT_195); } static void hook_entry_196(void) { INT_ENTRY(INTERRUPT_196); } static void hook_entry_197(void) { INT_ENTRY(INTERRUPT_197); } static void hook_entry_198(void) { INT_ENTRY(INTERRUPT_198); } static void hook_entry_199(void) { INT_ENTRY(INTERRUPT_199); } static void hook_entry_200(void) { INT_ENTRY(INTERRUPT_200); } static void hook_entry_201(void) { INT_ENTRY(INTERRUPT_201); } static void hook_entry_202(void) { INT_ENTRY(INTERRUPT_202); } static void hook_entry_203(void) { INT_ENTRY(INTERRUPT_203); } static void hook_entry_204(void) { INT_ENTRY(INTERRUPT_204); } static void hook_entry_205(void) { INT_ENTRY(INTERRUPT_205); } static void hook_entry_206(void) { INT_ENTRY(INTERRUPT_206); } static void hook_entry_207(void) { INT_ENTRY(INTERRUPT_207); } static void hook_entry_208(void) { INT_ENTRY(INTERRUPT_208); } static void hook_entry_209(void) { INT_ENTRY(INTERRUPT_209); } static void hook_entry_210(void) { INT_ENTRY(INTERRUPT_210); } static void hook_entry_211(void) { INT_ENTRY(INTERRUPT_211); } static void hook_entry_212(void) { INT_ENTRY(INTERRUPT_212); } static void hook_entry_213(void) { INT_ENTRY(INTERRUPT_213); } static void hook_entry_214(void) { INT_ENTRY(INTERRUPT_214); } static void hook_entry_215(void) { INT_ENTRY(INTERRUPT_215); } static void hook_entry_216(void) { INT_ENTRY(INTERRUPT_216); } static void hook_entry_217(void) { INT_ENTRY(INTERRUPT_217); } static void hook_entry_218(void) { INT_ENTRY(INTERRUPT_218); } static void hook_entry_219(void) { INT_ENTRY(INTERRUPT_219); } static void hook_entry_220(void) { INT_ENTRY(INTERRUPT_220); } static void hook_entry_221(void) { INT_ENTRY(INTERRUPT_221); } static void hook_entry_222(void) { INT_ENTRY(INTERRUPT_222); } static void hook_entry_223(void) { INT_ENTRY(INTERRUPT_223); } static void hook_entry_224(void) { INT_ENTRY(INTERRUPT_224); } static void hook_entry_225(void) { INT_ENTRY(INTERRUPT_225); } static void hook_entry_226(void) { INT_ENTRY(INTERRUPT_226); } static void hook_entry_227(void) { INT_ENTRY(INTERRUPT_227); } static void hook_entry_228(void) { INT_ENTRY(INTERRUPT_228); } static void hook_entry_229(void) { INT_ENTRY(INTERRUPT_229); } static void hook_entry_230(void) { INT_ENTRY(INTERRUPT_230); } static void hook_entry_231(void) { INT_ENTRY(INTERRUPT_231); } static void hook_entry_232(void) { INT_ENTRY(INTERRUPT_232); } static void hook_entry_233(void) { INT_ENTRY(INTERRUPT_233); } static void hook_entry_234(void) { INT_ENTRY(INTERRUPT_234); } static void hook_entry_235(void) { INT_ENTRY(INTERRUPT_235); } static void hook_entry_236(void) { INT_ENTRY(INTERRUPT_236); } static void hook_entry_237(void) { INT_ENTRY(INTERRUPT_237); } static void hook_entry_238(void) { INT_ENTRY(INTERRUPT_238); } static void hook_entry_239(void) { INT_ENTRY(INTERRUPT_239); } static void hook_entry_240(void) { INT_ENTRY(INTERRUPT_240); } static void hook_entry_241(void) { INT_ENTRY(INTERRUPT_241); } static void hook_entry_242(void) { INT_ENTRY(INTERRUPT_242); } static void hook_entry_243(void) { INT_ENTRY(INTERRUPT_243); } static void hook_entry_244(void) { INT_ENTRY(INTERRUPT_244); } static void hook_entry_245(void) { INT_ENTRY(INTERRUPT_245); } static void hook_entry_246(void) { INT_ENTRY(INTERRUPT_246); } static void hook_entry_247(void) { INT_ENTRY(INTERRUPT_247); } static void hook_entry_248(void) { INT_ENTRY(INTERRUPT_248); } static void hook_entry_249(void) { INT_ENTRY(INTERRUPT_249); } static void hook_entry_250(void) { INT_ENTRY(INTERRUPT_250); } static void hook_entry_251(void) { INT_ENTRY(INTERRUPT_251); } static void hook_entry_252(void) { INT_ENTRY(INTERRUPT_252); } static void hook_entry_253(void) { INT_ENTRY(INTERRUPT_253); } static void hook_entry_254(void) { INT_ENTRY(INTERRUPT_254); } static void hook_entry_255(void) { INT_ENTRY(INTERRUPT_255); } static void (* const Int_Hook_Vectors[])(void) = { (void (*)(void))hook_entry___0, (void (*)(void))hook_entry___1, (void (*)(void))hook_entry___2, (void (*)(void))hook_entry___3, (void (*)(void))hook_entry___4, (void (*)(void))hook_entry___5, (void (*)(void))hook_entry___6, (void (*)(void))hook_entry___7, (void (*)(void))hook_entry___8, (void (*)(void))hook_entry___9, (void (*)(void))hook_entry__10, (void (*)(void))hook_entry__11, (void (*)(void))hook_entry__12, (void (*)(void))hook_entry__13, (void (*)(void))hook_entry__14, (void (*)(void))hook_entry__15, (void (*)(void))hook_entry__16, (void (*)(void))hook_entry__17, (void (*)(void))hook_entry__18, (void (*)(void))hook_entry__19, (void (*)(void))hook_entry__20, (void (*)(void))hook_entry__21, (void (*)(void))hook_entry__22, (void (*)(void))hook_entry__23, (void (*)(void))hook_entry__24, (void (*)(void))hook_entry__25, (void (*)(void))hook_entry__26, (void (*)(void))hook_entry__27, (void (*)(void))hook_entry__28, (void (*)(void))hook_entry__29, (void (*)(void))hook_entry__30, (void (*)(void))hook_entry__31, (void (*)(void))hook_entry__32, (void (*)(void))hook_entry__33, (void (*)(void))hook_entry__34, (void (*)(void))hook_entry__35, (void (*)(void))hook_entry__36, (void (*)(void))hook_entry__37, (void (*)(void))hook_entry__38, (void (*)(void))hook_entry__39, (void (*)(void))hook_entry__40, (void (*)(void))hook_entry__41, (void (*)(void))hook_entry__42, (void (*)(void))hook_entry__43, (void (*)(void))hook_entry__44, (void (*)(void))hook_entry__45, (void (*)(void))hook_entry__46, (void (*)(void))hook_entry__47, (void (*)(void))hook_entry__48, (void (*)(void))hook_entry__49, (void (*)(void))hook_entry__50, (void (*)(void))hook_entry__51, (void (*)(void))hook_entry__52, (void (*)(void))hook_entry__53, (void (*)(void))hook_entry__54, (void (*)(void))hook_entry__55, (void (*)(void))hook_entry__56, (void (*)(void))hook_entry__57, (void (*)(void))hook_entry__58, (void (*)(void))hook_entry__59, (void (*)(void))hook_entry__60, (void (*)(void))hook_entry__61, (void (*)(void))hook_entry__62, (void (*)(void))hook_entry__63, (void (*)(void))hook_entry__64, (void (*)(void))hook_entry__65, (void (*)(void))hook_entry__66, (void (*)(void))hook_entry__67, (void (*)(void))hook_entry__68, (void (*)(void))hook_entry__69, (void (*)(void))hook_entry__70, (void (*)(void))hook_entry__71, (void (*)(void))hook_entry__72, (void (*)(void))hook_entry__73, (void (*)(void))hook_entry__74, (void (*)(void))hook_entry__75, (void (*)(void))hook_entry__76, (void (*)(void))hook_entry__77, (void (*)(void))hook_entry__78, (void (*)(void))hook_entry__79, (void (*)(void))hook_entry__80, (void (*)(void))hook_entry__81, (void (*)(void))hook_entry__82, (void (*)(void))hook_entry__83, (void (*)(void))hook_entry__84, (void (*)(void))hook_entry__85, (void (*)(void))hook_entry__86, (void (*)(void))hook_entry__87, (void (*)(void))hook_entry__88, (void (*)(void))hook_entry__89, (void (*)(void))hook_entry__90, (void (*)(void))hook_entry__91, (void (*)(void))hook_entry__92, (void (*)(void))hook_entry__93, (void (*)(void))hook_entry__94, (void (*)(void))hook_entry__95, (void (*)(void))hook_entry__96, (void (*)(void))hook_entry__97, (void (*)(void))hook_entry__98, (void (*)(void))hook_entry__99, (void (*)(void))hook_entry_100, (void (*)(void))hook_entry_101, (void (*)(void))hook_entry_102, (void (*)(void))hook_entry_103, (void (*)(void))hook_entry_104, (void (*)(void))hook_entry_105, (void (*)(void))hook_entry_106, (void (*)(void))hook_entry_107, (void (*)(void))hook_entry_108, (void (*)(void))hook_entry_109, (void (*)(void))hook_entry_110, (void (*)(void))hook_entry_111, (void (*)(void))hook_entry_112, (void (*)(void))hook_entry_113, (void (*)(void))hook_entry_114, (void (*)(void))hook_entry_115, (void (*)(void))hook_entry_116, (void (*)(void))hook_entry_117, (void (*)(void))hook_entry_118, (void (*)(void))hook_entry_119, (void (*)(void))hook_entry_120, (void (*)(void))hook_entry_121, (void (*)(void))hook_entry_122, (void (*)(void))hook_entry_123, (void (*)(void))hook_entry_124, (void (*)(void))hook_entry_125, (void (*)(void))hook_entry_126, (void (*)(void))hook_entry_127, (void (*)(void))hook_entry_128, (void (*)(void))hook_entry_129, (void (*)(void))hook_entry_130, (void (*)(void))hook_entry_131, (void (*)(void))hook_entry_132, (void (*)(void))hook_entry_133, (void (*)(void))hook_entry_134, (void (*)(void))hook_entry_135, (void (*)(void))hook_entry_136, (void (*)(void))hook_entry_137, (void (*)(void))hook_entry_138, (void (*)(void))hook_entry_139, (void (*)(void))hook_entry_140, (void (*)(void))hook_entry_141, (void (*)(void))hook_entry_142, (void (*)(void))hook_entry_143, (void (*)(void))hook_entry_144, (void (*)(void))hook_entry_145, (void (*)(void))hook_entry_146, (void (*)(void))hook_entry_147, (void (*)(void))hook_entry_148, (void (*)(void))hook_entry_149, (void (*)(void))hook_entry_150, (void (*)(void))hook_entry_151, (void (*)(void))hook_entry_152, (void (*)(void))hook_entry_153, (void (*)(void))hook_entry_154, (void (*)(void))hook_entry_155, (void (*)(void))hook_entry_156, (void (*)(void))hook_entry_157, (void (*)(void))hook_entry_158, (void (*)(void))hook_entry_159, (void (*)(void))hook_entry_160, (void (*)(void))hook_entry_161, (void (*)(void))hook_entry_162, (void (*)(void))hook_entry_163, (void (*)(void))hook_entry_164, (void (*)(void))hook_entry_165, (void (*)(void))hook_entry_166, (void (*)(void))hook_entry_167, (void (*)(void))hook_entry_168, (void (*)(void))hook_entry_169, (void (*)(void))hook_entry_170, (void (*)(void))hook_entry_171, (void (*)(void))hook_entry_172, (void (*)(void))hook_entry_173, (void (*)(void))hook_entry_174, (void (*)(void))hook_entry_175, (void (*)(void))hook_entry_176, (void (*)(void))hook_entry_177, (void (*)(void))hook_entry_178, (void (*)(void))hook_entry_179, (void (*)(void))hook_entry_180, (void (*)(void))hook_entry_181, (void (*)(void))hook_entry_182, (void (*)(void))hook_entry_183, (void (*)(void))hook_entry_184, (void (*)(void))hook_entry_185, (void (*)(void))hook_entry_186, (void (*)(void))hook_entry_187, (void (*)(void))hook_entry_188, (void (*)(void))hook_entry_189, (void (*)(void))hook_entry_190, (void (*)(void))hook_entry_191, (void (*)(void))hook_entry_192, (void (*)(void))hook_entry_193, (void (*)(void))hook_entry_194, (void (*)(void))hook_entry_195, (void (*)(void))hook_entry_196, (void (*)(void))hook_entry_197, (void (*)(void))hook_entry_198, (void (*)(void))hook_entry_199, (void (*)(void))hook_entry_200, (void (*)(void))hook_entry_201, (void (*)(void))hook_entry_202, (void (*)(void))hook_entry_203, (void (*)(void))hook_entry_204, (void (*)(void))hook_entry_205, (void (*)(void))hook_entry_206, (void (*)(void))hook_entry_207, (void (*)(void))hook_entry_208, (void (*)(void))hook_entry_209, (void (*)(void))hook_entry_210, (void (*)(void))hook_entry_211, (void (*)(void))hook_entry_212, (void (*)(void))hook_entry_213, (void (*)(void))hook_entry_214, (void (*)(void))hook_entry_215, (void (*)(void))hook_entry_216, (void (*)(void))hook_entry_217, (void (*)(void))hook_entry_218, (void (*)(void))hook_entry_219, (void (*)(void))hook_entry_220, (void (*)(void))hook_entry_221, (void (*)(void))hook_entry_222, (void (*)(void))hook_entry_223, (void (*)(void))hook_entry_224, (void (*)(void))hook_entry_225, (void (*)(void))hook_entry_226, (void (*)(void))hook_entry_227, (void (*)(void))hook_entry_228, (void (*)(void))hook_entry_229, (void (*)(void))hook_entry_230, (void (*)(void))hook_entry_231, (void (*)(void))hook_entry_232, (void (*)(void))hook_entry_233, (void (*)(void))hook_entry_234, (void (*)(void))hook_entry_235, (void (*)(void))hook_entry_236, (void (*)(void))hook_entry_237, (void (*)(void))hook_entry_238, (void (*)(void))hook_entry_239, (void (*)(void))hook_entry_240, (void (*)(void))hook_entry_241, (void (*)(void))hook_entry_242, (void (*)(void))hook_entry_243, (void (*)(void))hook_entry_244, (void (*)(void))hook_entry_245, (void (*)(void))hook_entry_246, (void (*)(void))hook_entry_247, (void (*)(void))hook_entry_248, (void (*)(void))hook_entry_249, (void (*)(void))hook_entry_250, (void (*)(void))hook_entry_251, (void (*)(void))hook_entry_252, (void (*)(void))hook_entry_253, (void (*)(void))hook_entry_254, (void (*)(void))hook_entry_255 };