/* * FreeRTOS Kernel V10.3.1 * Copyright (C) 2020 Amazon.com, Inc. or its affiliates. All Rights Reserved. * * Permission is hereby granted, free of charge, to any person obtaining a copy of * this software and associated documentation files (the "Software"), to deal in * the Software without restriction, including without limitation the rights to * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of * the Software, and to permit persons to whom the Software is furnished to do so, * subject to the following conditions: * * The above copyright notice and this permission notice shall be included in all * copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE. * * http://www.FreeRTOS.org * http://aws.amazon.com/freertos * * 1 tab == 4 spaces! */ /*----------------------------------------------------------- * Implementation of functions defined in portable.h for the RX700 DPFPU port. *----------------------------------------------------------*/ /* Scheduler includes. */ #include "FreeRTOS.h" #include "task.h" /* Library includes. */ #include "string.h" /* Hardware specifics. */ #if( configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H == 1 ) #include "platform.h" #else #include "iodefine.h" #endif /*-----------------------------------------------------------*/ /* Tasks should start with interrupts enabled and in Supervisor mode, therefore PSW is set with U and I set, and PM and IPL clear. */ #define portINITIAL_PSW ( ( StackType_t ) 0x00030000 ) #define portINITIAL_FPSW ( ( StackType_t ) 0x00000100 ) #define portINITIAL_DPSW ( ( StackType_t ) 0x00000100 ) #define portINITIAL_DCMR ( ( StackType_t ) 0x00000000 ) #define portINITIAL_DECNT ( ( StackType_t ) 0x00000001 ) /* Tasks are not created with a DPFPU context, but can be given a DPFPU context after they have been created. A variable is stored as part of the tasks context that holds portNO_DPFPU_CONTEXT if the task does not have an DPFPU context, or any other value if the task does have an DPFPU context. */ #define portNO_DPFPU_CONTEXT ( ( StackType_t ) 0 ) /* These macros allow a critical section to be added around the call to xTaskIncrementTick(), which is only ever called from interrupts at the kernel priority - ie a known priority. Therefore these local macros are a slight optimisation compared to calling the global SET/CLEAR_INTERRUPT_MASK macros, which would require the old IPL to be read first and stored in a local variable. */ #define portMASK_INTERRUPTS_FROM_KERNEL_ISR() __asm volatile ( "MVTIPL %0" ::"i"(configMAX_SYSCALL_INTERRUPT_PRIORITY) ) #define portUNMASK_INTERRUPTS_FROM_KERNEL_ISR() __asm volatile ( "MVTIPL %0" ::"i"(configKERNEL_INTERRUPT_PRIORITY) ) /*-----------------------------------------------------------*/ /* * Function to start the first task executing - written in asm code as direct * access to registers is required. */ static void prvStartFirstTask( void ) __attribute__((naked)); /* * Software interrupt handler. Performs the actual context switch (saving and * restoring of registers). Written in asm code as direct register access is * required. */ #if( configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H == 1 ) void vSoftwareInterruptISR( void ) __attribute__((naked, vector( R_BSP_SECNAME_INTVECTTBL, VECT_ICU_SWINT ))); #else void vSoftwareInterruptISR( void ) __attribute__((naked)); #endif /* * The tick interrupt handler. */ #if( configINCLUDE_PLATFORM_H_INSTEAD_OF_IODEFINE_H == 1 ) void vTickISR( void ) __attribute__((interrupt( R_BSP_SECNAME_INTVECTTBL, _VECT( configTICK_VECTOR ) ))); #else void vTickISR( void ) __attribute__((interrupt)); #endif /*-----------------------------------------------------------*/ extern void *pxCurrentTCB; StackType_t ulPortTaskHasDPFPUContext; /*-----------------------------------------------------------*/ /* * See header file for description. */ StackType_t *pxPortInitialiseStack( StackType_t *pxTopOfStack, TaskFunction_t pxCode, void *pvParameters ) { /* R0 is not included as it is the stack pointer. */ *pxTopOfStack = 0x00; pxTopOfStack--; *pxTopOfStack = portINITIAL_PSW; pxTopOfStack--; *pxTopOfStack = ( StackType_t ) pxCode; /* When debugging it can be useful if every register is set to a known value. Otherwise code space can be saved by just setting the registers that need to be set. */ #ifdef USE_FULL_REGISTER_INITIALISATION { pxTopOfStack--; *pxTopOfStack = 0xffffffff; /* r15. */ pxTopOfStack--; *pxTopOfStack = 0xeeeeeeee; pxTopOfStack--; *pxTopOfStack = 0xdddddddd; pxTopOfStack--; *pxTopOfStack = 0xcccccccc; pxTopOfStack--; *pxTopOfStack = 0xbbbbbbbb; pxTopOfStack--; *pxTopOfStack = 0xaaaaaaaa; pxTopOfStack--; *pxTopOfStack = 0x99999999; pxTopOfStack--; *pxTopOfStack = 0x88888888; pxTopOfStack--; *pxTopOfStack = 0x77777777; pxTopOfStack--; *pxTopOfStack = 0x66666666; pxTopOfStack--; *pxTopOfStack = 0x55555555; pxTopOfStack--; *pxTopOfStack = 0x44444444; pxTopOfStack--; *pxTopOfStack = 0x33333333; pxTopOfStack--; *pxTopOfStack = 0x22222222; pxTopOfStack--; } #else { pxTopOfStack -= 15; } #endif *pxTopOfStack = ( StackType_t ) pvParameters; /* R1 */ pxTopOfStack--; *pxTopOfStack = portINITIAL_FPSW; pxTopOfStack--; *pxTopOfStack = 0x11111111; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x22222222; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x33333333; /* Accumulator 1. */ pxTopOfStack--; *pxTopOfStack = 0x44444444; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x55555555; /* Accumulator 0. */ pxTopOfStack--; *pxTopOfStack = 0x66666666; /* Accumulator 0. */ #if( configUSE_TASK_DPFPU_SUPPORT == 1 ) { /* The task will start without a DPFPU context. A task that uses the DPFPU hardware must call vPortTaskUsesDPFPU() before executing any floating point instructions. */ pxTopOfStack--; *pxTopOfStack = portNO_DPFPU_CONTEXT; } #elif( configUSE_TASK_DPFPU_SUPPORT == 2 ) { /* The task will start with a DPFPU context. Leave enough space for the registers - and ensure they are initialised if desired. */ #ifdef USE_FULL_REGISTER_INITIALISATION { pxTopOfStack -= 2; *(double *)pxTopOfStack = 1515.1515; /* DR15. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1414.1414; /* DR14. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1313.1313; /* DR13. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1212.1212; /* DR12. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1111.1111; /* DR11. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 1010.1010; /* DR10. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 909.0909; /* DR9. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 808.0808; /* DR8. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 707.0707; /* DR7. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 606.0606; /* DR6. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 505.0505; /* DR5. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 404.0404; /* DR4. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 303.0303; /* DR3. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 202.0202; /* DR2. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 101.0101; /* DR1. */ pxTopOfStack -= 2; *(double *)pxTopOfStack = 9876.54321;/* DR0. */ } #else { pxTopOfStack -= 32; } #endif pxTopOfStack--; *pxTopOfStack = portINITIAL_DECNT; /* DECNT. */ pxTopOfStack--; *pxTopOfStack = portINITIAL_DCMR; /* DCMR. */ pxTopOfStack--; *pxTopOfStack = portINITIAL_DPSW; /* DPSW. */ pxTopOfStack--; *pxTopOfStack = pdTRUE; ////????////ulPortTaskHasDPFPUContext = pdTRUE; } #elif( configUSE_TASK_DPFPU_SUPPORT == 0 ) { /* Omit DPFPU support. */ } #else { #error Invalid configUSE_TASK_DPFPU_SUPPORT setting - configUSE_TASK_DPFPU_SUPPORT must be set to 0, 1, 2, or left undefined. } #endif return pxTopOfStack; } /*-----------------------------------------------------------*/ BaseType_t xPortStartScheduler( void ) { extern void vApplicationSetupTimerInterrupt( void ); /* Use pxCurrentTCB just so it does not get optimised away. */ if( pxCurrentTCB != NULL ) { /* Call an application function to set up the timer that will generate the tick interrupt. This way the application can decide which peripheral to use. A demo application is provided to show a suitable example. */ vApplicationSetupTimerInterrupt(); /* Enable the software interrupt. */ _IEN( _ICU_SWINT ) = 1; /* Ensure the software interrupt is clear. */ _IR( _ICU_SWINT ) = 0; /* Ensure the software interrupt is set to the kernel priority. */ _IPR( _ICU_SWINT ) = configKERNEL_INTERRUPT_PRIORITY; /* Start the first task. */ prvStartFirstTask(); } /* Should not get here. */ return pdFAIL; } /*-----------------------------------------------------------*/ void vPortEndScheduler( void ) { /* Not implemented in ports where there is nothing to return to. Artificially force an assert. */ configASSERT( pxCurrentTCB == NULL ); } /*-----------------------------------------------------------*/ static void prvStartFirstTask( void ) { __asm volatile ( /* When starting the scheduler there is nothing that needs moving to the interrupt stack because the function is not called from an interrupt. Just ensure the current stack is the user stack. */ "SETPSW U \n" \ /* Obtain the location of the stack associated with which ever task pxCurrentTCB is currently pointing to. */ "MOV.L #_pxCurrentTCB, R15 \n" \ "MOV.L [R15], R15 \n" \ "MOV.L [R15], R0 \n" \ /* Restore the registers from the stack of the task pointed to by pxCurrentTCB. */ ////////////////////////////////////////////////////////////////////////////////////////////////////////////// #if( configUSE_TASK_DPFPU_SUPPORT != 0 ) /* Is there a DPFPU context to restore? If the restored ulPortTaskHasDPFPUContext is zero then no. */ "POP R15 \n" \ "MOV.L #_ulPortTaskHasDPFPUContext, R14 \n" \ "MOV.L R15, [R14] \n" \ "CMP #0, R15 \n" \ /* Restore the DPFPU context, if any. */ "BEQ.B ?+ \n" \ "DPOPM.L DPSW-DECNT \n" \ "DPOPM.D DR0-DR15 \n" \ "?: \n" \ #endif /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A0 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A0 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A0 \n" \ /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A1 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A1 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A1 \n" \ /* Floating point status word. */ "POP R15 \n" \ "MVTC R15, FPSW \n" \ /* R1 to R15 - R0 is not included as it is the SP. */ "POPM R1-R15 \n" \ /* This pops the remaining registers. */ "RTE \n" \ "NOP \n" \ "NOP \n" ); } /*-----------------------------------------------------------*/ void vSoftwareInterruptISR( void ) { __asm volatile ( /* Re-enable interrupts. */ "SETPSW I \n" \ /* Move the data that was automatically pushed onto the interrupt stack when the interrupt occurred from the interrupt stack to the user stack. R15 is saved before it is clobbered. */ "PUSH.L R15 \n" \ /* Read the user stack pointer. */ "MVFC USP, R15 \n" \ /* Move the address down to the data being moved. */ "SUB #12, R15 \n" \ "MVTC R15, USP \n" \ /* Copy the data across, R15, then PC, then PSW. */ "MOV.L [ R0 ], [ R15 ] \n" \ "MOV.L 4[ R0 ], 4[ R15 ] \n" \ "MOV.L 8[ R0 ], 8[ R15 ] \n" \ /* Move the interrupt stack pointer to its new correct position. */ "ADD #12, R0 \n" \ /* All the rest of the registers are saved directly to the user stack. */ "SETPSW U \n" \ /* Save the rest of the general registers (R15 has been saved already). */ "PUSHM R1-R14 \n" \ /* Floating point status word. */ "MVFC FPSW, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator guard. */ "MVFACGU #0, A1, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator high 32 bits. */ "MVFACHI #0, A1, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator low 32 bits. */ "MVFACLO #0, A1, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator guard. */ "MVFACGU #0, A0, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator high 32 bits. */ "MVFACHI #0, A0, R15 \n" \ "PUSH.L R15 \n" \ /* Accumulator low 32 bits. */ "MVFACLO #0, A0, R15 \n" \ "PUSH.L R15 \n" \ ////////////////////////////////////////////////////////////////////////////////////////////////////////////// #if( configUSE_TASK_DPFPU_SUPPORT != 0 ) /* Does the task have a DPFPU context that needs saving? If ulPortTaskHasDPFPUContext is 0 then no. */ "MOV.L #_ulPortTaskHasDPFPUContext, R15 \n" \ "MOV.L [R15], R15 \n" \ "CMP #0, R15 \n" \ /* Save the DPFPU context, if any. */ "BEQ.B ?+ \n" \ "DPUSHM.D DR0-DR15 \n" \ "DPUSHM.L DPSW-DECNT \n" \ "?: \n" \ /* Save ulPortTaskHasDPFPUContext itself. */ "PUSH R15 \n" \ #endif /* Save the stack pointer to the TCB. */ "MOV.L #_pxCurrentTCB, R15 \n" \ "MOV.L [ R15 ], R15 \n" \ "MOV.L R0, [ R15 ] \n" \ /* Ensure the interrupt mask is set to the syscall priority while the kernel structures are being accessed. */ "MVTIPL %0 \n" \ /* Select the next task to run. */ "BSR.A _vTaskSwitchContext \n" \ /* Reset the interrupt mask as no more data structure access is required. */ "MVTIPL %1 \n" \ /* Load the stack pointer of the task that is now selected as the Running state task from its TCB. */ "MOV.L #_pxCurrentTCB,R15 \n" \ "MOV.L [ R15 ], R15 \n" \ "MOV.L [ R15 ], R0 \n" \ /* Restore the context of the new task. The PSW (Program Status Word) and PC will be popped by the RTE instruction. */ ////////////////////////////////////////////////////////////////////////////////////////////////////////////// #if( configUSE_TASK_DPFPU_SUPPORT != 0 ) /* Is there a DPFPU context to restore? If the restored ulPortTaskHasDPFPUContext is zero then no. */ "POP R15 \n" \ "MOV.L #_ulPortTaskHasDPFPUContext, R14 \n" \ "MOV.L R15, [R14] \n" \ "CMP #0, R15 \n" \ /* Restore the DPFPU context, if any. */ "BEQ.B ?+ \n" \ "DPOPM.L DPSW-DECNT \n" \ "DPOPM.D DR0-DR15 \n" \ "?: \n" \ #endif /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A0 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A0 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A0 \n" \ /* Accumulator low 32 bits. */ "POP R15 \n" \ "MVTACLO R15, A1 \n" \ /* Accumulator high 32 bits. */ "POP R15 \n" \ "MVTACHI R15, A1 \n" \ /* Accumulator guard. */ "POP R15 \n" \ "MVTACGU R15, A1 \n" \ /* Floating point status word. */ "POP R15 \n" \ "MVTC R15, FPSW \n" \ /* R1 to R15 - R0 is not included as it is the SP. */ "POPM R1-R15 \n" \ /* This pops the remaining registers. */ "RTE \n" \ "NOP \n" \ "NOP " :: "i"(configMAX_SYSCALL_INTERRUPT_PRIORITY), "i"(configKERNEL_INTERRUPT_PRIORITY) ); } /*-----------------------------------------------------------*/ void vTickISR( void ) { /* Re-enabled interrupts. */ __asm volatile( "SETPSW I" ); /* Increment the tick, and perform any processing the new tick value necessitates. Ensure IPL is at the max syscall value first. */ portMASK_INTERRUPTS_FROM_KERNEL_ISR(); { if( xTaskIncrementTick() != pdFALSE ) { taskYIELD(); } } portUNMASK_INTERRUPTS_FROM_KERNEL_ISR(); } /*-----------------------------------------------------------*/ uint32_t ulPortGetIPL( void ) { __asm volatile ( "MVFC PSW, R1 \n" \ "SHLR #24, R1 \n" \ "RTS " ); /* This will never get executed, but keeps the compiler from complaining. */ return 0; } /*-----------------------------------------------------------*/ void vPortSetIPL( uint32_t ulNewIPL ) { /* Avoid compiler warning about unreferenced parameter. */ ( void ) ulNewIPL; __asm volatile ( "PUSH R5 \n" \ "MVFC PSW, R5 \n" \ "SHLL #24, R1 \n" \ "AND #-0F000001H, R5 \n" \ "OR R1, R5 \n" \ "MVTC R5, PSW \n" \ "POP R5 \n" \ "RTS " ); } /*-----------------------------------------------------------*/ #if( configUSE_TASK_DPFPU_SUPPORT == 1 ) void vPortTaskUsesDPFPU( void ) { /* A task is registering the fact that it needs a DPFPU context. Set the DPFPU flag (which is saved as part of the task context). */ ulPortTaskHasDPFPUContext = pdTRUE; } #endif /* configUSE_TASK_DPFPU_SUPPORT */ /*-----------------------------------------------------------*/