#include "task_function.h" /* Start user code for import. Do not edit comment generated here */ #include "freertos_start.h" #include "platform.h" #include "tbrx65ndef.h" /* End user code. Do not edit comment generated here */ void task_LED0(void * pvParameters) { /* Start user code for function. Do not edit comment generated here */ INTERNAL_NOT_USED( pvParameters ); LED0 = LED_ON; for (;;) { #if defined(RENESAS_SIMULATOR_DEBUGGING) if (IsRenesasSimDebugMode()) { /* Renesas RX Simulator */ vTaskDelay( pdMS_TO_TICKS( 50/*ms(as of the simulation time)*/ ) ); } else #endif { /* Hardware */ vTaskDelay( pdMS_TO_TICKS( 500/*ms*/ ) ); } LED0 = ~LED0; } /* End user code. Do not edit comment generated here */ } /* Start user code for other. Do not edit comment generated here */ /* End user code. Do not edit comment generated here */