GR-SAKURA
GR-KURUMI
GR-COTTON
GR-CITRUS
GR-PEACH
GR-KAEDE
GR-ADZUKI
GR-LYCHEE
GR-ROSE
GR-MANGO(*)
SNShield
Web Compiler
IDE for GR
TOPPERS関連
女子美コラボ
その他
※プロデューサミーティング中
作り方使い方資料
イベント関連
作品記事
体験記事
ライブラリ
ツール
その他・過去ファイル
がじぇるね岡宮です。
GR-ROSEにはPMOD用インタフェースがありますが、OLED RGB (96x64)を動作させてみました。
リンク:秋月、Digilent
以下のAdafruit_SSD1331のライブラリを使ってます。なおAdafruit_GFX_LibraryはGR-ROSEの標準ライブラリに含まれているため、インポートの必要はありません。
https://github.com/adafruit/Adafruit-SSD1331-OLED-Driver-Library-for-Arduino
GR-ROSEにこのモジュールを接続した場合、VCCENがピン20、PMODENがピン21に割り当たっており、これらをHIGHにする必要があるため、デフォルトのサンプルに対して、その点だけ変更を加えたものを実行してみました。とりあえず動いたので、ご報告までです。しかし、そのまま接続すると垂直方向に立ってしまうのですよね。かといってPMOD用のライトアングルピンヘッダ 6x2も手に入れにくいというのが微妙・・・。延長ケーブルか、ワイヤーをPin to Pinでつなぐかといったところですね。
/*************************************************** This is a example sketch demonstrating the graphics capabilities of the SSD1331 library for the 0.96" 16-bit Color OLED with SSD1331 driver chip Pick one up today in the adafruit shop! ------> www.adafruit.com/.../684 These displays use SPI to communicate, 4 or 5 pins are required to interface Adafruit invests time and resources providing this open source code, please support Adafruit and open-source hardware by purchasing products from Adafruit! Written by Limor Fried/Ladyada for Adafruit Industries. BSD license, all text above must be included in any redistribution ****************************************************/#include <Adafruit_GFX.h>#include <Adafruit_SSD1331.h>#include <SPI.h>// You can use any (4 or) 5 pins#define sclk 13#define mosi 11#define cs 10#define rst 9#define dc 8#define vccen 20#define pmoden 21// Color definitions#define BLACK 0x0000#define BLUE 0x001F#define RED 0xF800#define GREEN 0x07E0#define CYAN 0x07FF#define MAGENTA 0xF81F#define YELLOW 0xFFE0#define WHITE 0xFFFF// Option 1: use any pins but a little slower//Adafruit_SSD1331 display = Adafruit_SSD1331(cs, dc, mosi, sclk, rst);// Option 2: must use the hardware SPI pins// (for UNO thats sclk = 13 and sid = 11) and pin 10 must be// an output. This is much faster - also required if you want// to use the microSD card (see the image drawing example)Adafruit_SSD1331 display = Adafruit_SSD1331(&SPI, cs, dc, rst);float p = 3.1415926;void setup(void) { Serial.begin(9600); Serial.print("hello!"); pinMode(vccen, OUTPUT); digitalWrite(vccen, HIGH); pinMode(pmoden, OUTPUT); digitalWrite(pmoden, HIGH); display.begin(); Serial.println("init"); uint16_t time = millis(); display.fillScreen(BLACK); time = millis() - time; Serial.println(time, DEC); delay(500); lcdTestPattern(); delay(1000); display.fillScreen(BLACK); display.setCursor(0,0); display.print("Lorem ipsum dolor sit amet, consectetur adipiscing elit. Curabitur adipiscing ante sed nibh tincidunt feugiat. Maecenas enim massa"); delay(1000); // tft print function! tftPrintTest(); delay(2000); //a single pixel display.drawPixel(display.width()/2, display.height()/2, GREEN); delay(500); // line draw test testlines(YELLOW); delay(500); // optimized lines testfastlines(RED, BLUE); delay(500); testdrawrects(GREEN); delay(1000); testfillrects(YELLOW, MAGENTA); delay(1000); display.fillScreen(BLACK); testfillcircles(10, BLUE); testdrawcircles(10, WHITE); delay(1000); testroundrects(); delay(500); testtriangles(); delay(500); Serial.println("done"); delay(1000);}void loop() {}void testlines(uint16_t color) { display.fillScreen(BLACK); for (int16_t x=0; x < display.width()-1; x+=6) { display.drawLine(0, 0, x, display.height()-1, color); } for (int16_t y=0; y < display.height()-1; y+=6) { display.drawLine(0, 0, display.width()-1, y, color); } display.fillScreen(BLACK); for (int16_t x=0; x < display.width()-1; x+=6) { display.drawLine(display.width()-1, 0, x, display.height()-1, color); } for (int16_t y=0; y < display.height()-1; y+=6) { display.drawLine(display.width()-1, 0, 0, y, color); } // To avoid ESP8266 watchdog timer resets when not using the hardware SPI pins delay(0); display.fillScreen(BLACK); for (int16_t x=0; x < display.width()-1; x+=6) { display.drawLine(0, display.height()-1, x, 0, color); } for (int16_t y=0; y < display.height()-1; y+=6) { display.drawLine(0, display.height()-1, display.width()-1, y, color); } display.fillScreen(BLACK); for (int16_t x=0; x < display.width()-1; x+=6) { display.drawLine(display.width()-1, display.height()-1, x, 0, color); } for (int16_t y=0; y < display.height()-1; y+=6) { display.drawLine(display.width()-1, display.height()-1, 0, y, color); }}void testdrawtext(char *text, uint16_t color) { display.setTextSize(1); display.setTextColor(WHITE); display.setCursor(0,0); for (uint8_t i=0; i < 168; i++) { if (i == '\n') continue; display.write(i); if ((i > 0) && (i % 21 == 0)) display.println(); }}void testfastlines(uint16_t color1, uint16_t color2) { display.fillScreen(BLACK); for (int16_t y=0; y < display.height()-1; y+=5) { display.drawFastHLine(0, y, display.width()-1, color1); } for (int16_t x=0; x < display.width()-1; x+=5) { display.drawFastVLine(x, 0, display.height()-1, color2); }}void testdrawrects(uint16_t color) { display.fillScreen(BLACK); for (int16_t x=0; x < display.height()-1; x+=6) { display.drawRect((display.width()-1)/2 -x/2, (display.height()-1)/2 -x/2 , x, x, color); }}void testfillrects(uint16_t color1, uint16_t color2) { display.fillScreen(BLACK); for (int16_t x=display.height()-1; x > 6; x-=6) { display.fillRect((display.width()-1)/2 -x/2, (display.height()-1)/2 -x/2 , x, x, color1); display.drawRect((display.width()-1)/2 -x/2, (display.height()-1)/2 -x/2 , x, x, color2); }}void testfillcircles(uint8_t radius, uint16_t color) { for (uint8_t x=radius; x < display.width()-1; x+=radius*2) { for (uint8_t y=radius; y < display.height()-1; y+=radius*2) { display.fillCircle(x, y, radius, color); } }}void testdrawcircles(uint8_t radius, uint16_t color) { for (int16_t x=0; x < display.width()-1+radius; x+=radius*2) { for (int16_t y=0; y < display.height()-1+radius; y+=radius*2) { display.drawCircle(x, y, radius, color); } }}void testtriangles() { display.fillScreen(BLACK); int color = 0xF800; int t; int w = display.width()/2; int x = display.height(); int y = 0; int z = display.width(); for (t = 0 ; t <= 15; t+=1) { display.drawTriangle(w, y, y, x, z, x, color); x-=4; y+=4; z-=4; color+=100; }}void testroundrects() { display.fillScreen(BLACK); int color = 100; int i; int t; for(t = 0 ; t <= 4; t+=1) { int x = 0; int y = 0; int w = display.width(); int h = display.height(); for(i = 0 ; i <= 8; i+=1) { display.drawRoundRect(x, y, w, h, 5, color); x+=2; y+=3; w-=4; h-=6; color+=1100; } color+=100; }}void tftPrintTest() { display.fillScreen(BLACK); display.setCursor(0, 5); display.setTextColor(RED); display.setTextSize(1); display.println("Hello World!"); display.setTextColor(YELLOW, GREEN); display.setTextSize(2); display.print("Hello Wo"); display.setTextColor(BLUE); display.setTextSize(3); display.print(1234.567); delay(1500); display.setCursor(0, 5); display.fillScreen(BLACK); display.setTextColor(WHITE); display.setTextSize(0); display.println("Hello World!"); display.setTextSize(1); display.setTextColor(GREEN); display.print(p, 5); display.println(" Want pi?"); display.print(8675309, HEX); // print 8,675,309 out in HEX! display.print(" Print HEX"); display.setTextColor(WHITE); display.println("Sketch has been"); display.println("running for: "); display.setTextColor(MAGENTA); display.print(millis() / 1000); display.setTextColor(WHITE); display.print(" seconds.");}void mediabuttons() { // play display.fillScreen(BLACK); display.fillRoundRect(25, 10, 78, 60, 8, WHITE); display.fillTriangle(42, 20, 42, 60, 90, 40, RED); delay(500); // pause display.fillRoundRect(25, 90, 78, 60, 8, WHITE); display.fillRoundRect(39, 98, 20, 45, 5, GREEN); display.fillRoundRect(69, 98, 20, 45, 5, GREEN); delay(500); // play color display.fillTriangle(42, 20, 42, 60, 90, 40, BLUE); delay(50); // pause color display.fillRoundRect(39, 98, 20, 45, 5, RED); display.fillRoundRect(69, 98, 20, 45, 5, RED); // play color display.fillTriangle(42, 20, 42, 60, 90, 40, GREEN);}/**************************************************************************//*! @brief Renders a simple test pattern on the LCD*//**************************************************************************/void lcdTestPattern(void){ uint8_t w,h; display.setAddrWindow(0, 0, 96, 64); for (h = 0; h < 64; h++) { for (w = 0; w < 96; w++) { if (w > 83) { display.writePixel(w, h, WHITE); } else if (w > 71) { display.writePixel(w, h, BLUE); } else if (w > 59) { display.writePixel(w, h, GREEN); } else if (w > 47) { display.writePixel(w, h, CYAN); } else if (w > 35) { display.writePixel(w, h, RED); } else if (w > 23) { display.writePixel(w, h, MAGENTA); } else if (w > 11) { display.writePixel(w, h, YELLOW); } else { display.writePixel(w, h, BLACK); } } } display.endWrite();}