我修改了14580跟flash的引脚配置(图一),同时也修改了SDK程序中的“flash_programmer”文件相关参数(图二),并且替换.bin文件,运行官方软件SmartSnippets,使用j-link连接,开始访问flash,软件可以访问、擦除、读取和烧录程序到FLASH中,但是,硬件复位后,代码貌似不能正常运行,因为亮灯效果并没有出现。代码本身没有问题,我使用j-link连接硬件电路,KEIL软件仿真,程序可以正常运行,硬件板上对应灯光也受程序控制。这是什么问题导致的呢?
Hi liangxie,
DA14580已停产,并且无法提供相应的支持。
后续的产品设计请更换为DA14531。
Br
Martin