DA14531需要工作在ADV_DIRECT_IND模式

您好,

      我们打算用DA14531开发门磁报警器,门窗报警从机采用14531以ADV_DIRECT_IND模式发送广播数据,主机也采用14531接收广播数据并与从机建立连接,最后进行双向身份验证(避免恶意者伪造从机,引起主机误报)。

      为了尽可能延长主从机的使用时间(二者都采用CR2032纽扣电池供电),需要使用ADV_DIRECT_IND广播模式,请问您能提供一个相应的主从机的DEMO代码吗?

      我的邮箱:[email protected] 

                                                                    谢谢!

Parents Reply Children
No Data