使用瑞萨的Rx72m,进行CAN通信,使用一个单板,进入内部回环自测,即设置api_status = R_CAN_PortSet(g_can_channel, CANPORT_TEST_1_INT_LOOPBACK);
然后报文可以发送,参考了官方的例程,但报文不能实现接收
/*** RECEIVED any frames? */ api_status = R_CAN_RxPoll(g_can_channel, CANBOX_RX); if (api_status == R_CAN_OK) { nr_frames_rx++; //这里,数值没有任何的变化
/* Read CAN data and show. */ api_status = R_CAN_RxRead(g_can_channel, g_mb_mode, CANBOX_RX, &rx_dataframe);
/* You can set BP here and check the received data in debugger. */ R_BSP_NOP();
#if BSP_CFG_IO_LIB_ENABLE printf("Received CAN ID 0x%X, nr_frames_rx = %d.\n", rx_dataframe.id, nr_frames_rx); #endif if (api_status == R_CAN_MSGLOST) { #if BSP_CFG_IO_LIB_ENABLE printf( "MSGLOST\n"); #endif R_BSP_NOP(); } }
Hello,
I'm an admin of Japanese Forum.Please post this question in the Chinese forum below.
community-ja.renesas.com/.../forum
regards,