こんにちは、クラウドです。
RL78/G13スターターキットとCS+で、組込みプログラミングを勉強中です。I2Cを使って読み出したデータを、スターターキットのLCDに表示させようと考えています。外部デバイスの接続について教えてください。
I2Cの操作のために、チョコさんのサンプルプログラム(https://japan.renesasrulz.com/cafe_rene/m/sample_program/292)を参考に、接続するデバイス(温度センサ)のレジスタ読み書きを行い、読み出し値をスターターキットのLCDに表示させます。
ハードウェアマニュアルからピンの番号を探したのですが、今後、ソフトを書き換えてI2C機能を別のチャネルやSAUに移した時、再びマニュアルを参照しなければならないのでしょうか。ユニットの機能を定義した時に「この信号は、このピン」とリストのようなものを出力することはできませんでしょうか。何か、簡単な方法はありますか。よろしくお願いします。
Hi make, I recommend to post this issue to the following forum for English Language.https://renesasrulz.com/gadget_renesas_user_forum/Best regards,NoMaY
Hi make,Sorry, you already did it.Best regards,NoMaY