こんにちは。NoMaYです。TB-RX65N/RX130/RX231のCS+のサンプルプログラムです。まずはデバッグコンソール出力のサンプルです。(サンプルプログラム置き場とGitHubに置きました。)japan.renesasrulz.com/cafe_rene/m/sample_program/460github.com/NoMaY-jp/RX_SmartConfigurator_examples_RXTB_CSplus/tree/cafe_rene/10_DebugConsole_printf
int main(void){ LED0 = LED_ON; for (;;) { printf( "Hello World\r\n" ); R_BSP_SoftwareDelay( 1000, BSP_DELAY_MILLISECS ); LED0 = ~LED0; R_BSP_SoftwareDelay( 1000, BSP_DELAY_MILLISECS ); LED0 = ~LED0; }}
こんにちは。NoMaYです。投稿したサンプルプログラムですが、時間待ちをするのに、FITのBSPモジュールのR_BSP_SoftwareDelay()というAPIを使っています。この場合、時間待ちをしている間は何も出来なくなります。そうでは無くて、ループを回しながら時間待ちをしたい場合には、以下のスレッドの投稿のような方法を試してみて下さい。タイマーと配列japan.renesasrulz.com/cafe_rene/f/002-2095199602/7247/thread/38656#38656