将BOOT程序地址从0X0000改为0X8000后,报错E0562320:部分地址溢出范围:“.const”
This FAQ may help you:FAQ - E0562320 Error Message (RL78 CC-RL)https://en-support.renesas.com/knowledgeBase/16978833
上方连接的方法试过后,没有解决问题
.const should be located within mirror area.Too big .text may cause this problem if exceed 0xb000. I suppose you should move .const in lower address than .text, or just move start address of data sections with far ROM option.
还有一个问题想请教一下,程序相同并且没有错误但是起始地址不同的两个BOOT程序,同时烧录到FLASH,为什么从0x0000跳转到0x8000的BOOT程序后不能运行呢?
Then you should use -far_rom option or add __far for all const variables.Once try downgrading E0562320 to warning with -CHange_message option to see how the sections are overwrapped in map file.