お世話になります初心者IKUZOと申しますRL78/G1EのTO00でパルス出力8個のみ出力したいと思いますR_TAU0_Channel0_Start();からたぶんINTTM00割込みハンドラーにてカウンター確認しましてR_TAU0_Channel0_Stop();を呼ぶような処理ではないかと思いますが1.INTTM00割込みハンドラーはどのファイルになりますでしょうか?2.その中でカウンターが8になっているかどうかは、どのように確認するのでしょうか?