お世話になります初心者IKUZOと申しますRL78/G1Eで高速にA/D変換できないかと考えております下図のように設定しましたが、大丈夫なんでしょうかわからないことがありましてハードウェアトリガーでINTTM01から起動にしましてだいたいこれでいいのでしょうか?入力がANI0とANI22があるのが疑問ですやりたいのはANI0を10uS以内で8ビットに変換して判断したいのですGAIN_AMP→DC→抵抗分圧→ANI0→A/D変換のようにしたいです変換時間が赤く表示されているのは、エラーなんでしょうか?変換結果も設定はどうしたら良いのでしょうか?