2023-10のe2studioをUbuntuにインストールしてRXとRAの開発をしようと考えていました。RAはELFが出力されるところまで確認できました(評価ボードが届くのは来週)。ところがRXマイコン、ツールチェーンの登録ができません。e2studioインストール時にGCCのRX版がインストール項目にないのですが別途下記のところからGCCをインストールしてあります。https://llvm-gcc-renesas.com/ja/rx-download-toolchains/何かプラグインなどを入れることで対応可能でしょうか?同じバージョンのWindows版ではGNURXでLED点滅(CMT0の割り込み駆動)の実機確認まで済んでいます。
ツールチェーンの登録ですが自力で解決しました。メニューのHelpにツールチェーン追加があり、ツールチェーンタイプに合わせたインストールしたクロスコンパイラのフォルダをADDから追加することでできました。これからLED点滅を試してみます。現在、FITモジュールをダウンロードしている最中です。ダウンロードが済むまでちょっと長そう。E2Liteが使えるか?これが心配です。使えればLinuxで開発環境が完結しそうです。