こんにちは。NoMaYです。今首を傾げているのですが、以下のドキュメントによると、e2 studio v7.5.0ではAmazon FreeRTOSプロジェクトに於いてスマートコンフィグレータでRTOS Objectコンポーネントというものが使用出来る/存在するらしいのですが、これは単なるFreeRTOSプロジェクトでは使用出来ない/存在しないものなのでしょうか?(スマートコンフィグレータウィンドウの、コンポーネントタブ上に表示されない&コンポーネント追加ダイアロにも表示されない、ので、そうなのかな、とは思っているのですが、Amazon FreeRTOSプロジェクトとFreeRTOSプロジェクトで、このような部分で違っているのが意外でしたので、、、)e2 studio 7.5.0 Release Notewww.renesas.com/jp/ja/doc/products/tool/doc/016/r20ut4556ee0101-e2studio.pdfPage 17 of 72「New Amazon FreeRTOS Configuration user interface provide within e2 studio 7.5 featuring:● Imported FreeRTOS project with pre-loaded FreeRTOS Components (Object, Kernel and Amazon Libraries).略o FreeRTOS Object configuration: allow user to be able to create, configure multiple FreeRTOS objects using GUI (Tasks, Semaphores, Queues, Software Timers, Event Groups, Message Buffers, Stream Buffers)o Create/Remove FreeRTOS Objects with user friendly UI.略」ちなみに、プロジェクトの生成では、コンパイラはCC-RX V3.01、デバイスはR5F565NEDxFP、に設定して試しました。
シェルティさん、こんにちは。NoMaYです。FreeRTOSのRenesas RXのポートレイヤのIAR版を見ていて気付いたのですが、IAR版はコンフィグレーションファイルがFreeRTOSConfig.hの他に(ポートレイヤのアセンブラソースの為)もう1つPriorityDefinitions.hがありますね。将来のRXスマートコンフィグレータでのIAR版のサポート(があると思っています)が、ちょっと面倒そうですね。(RXスマートコンフィグレータはIAR版に対して2つコンフィグレーションファイルを扱わなければならなくなるから。)何か対策を考えておられますか?もし、私の方でPriorityDefinitions.hを不要にするように改造したら、(うまくいくかどうかは今後の作業の結果次第として、) そちらで困った問題が発生するようなことはありますか?(あと、FreeRTOS.orgの方で受け入れられるかという点もありますが。)●CC-RX版のポートレイヤと関連ファイルport.cport_asm.srcportmacro.hFreeRTOSConfig.h●GNURX版のポートレイヤと関連ファイルport.cportmacro.hFreeRTOSConfig.h●IAR版のポートレイヤと関連ファイルport.cport_asm.sportmacro.hFreeRTOSConfig.hPriorityDefinitions.hなお、PriorityDefinitions.hは以下の通りでした。(定型のCopyrightの部分は省略しました。)
#ifndef PRIORITY_DEFINITIONS_H#define PRIORITY_DEFINITIONS_H#ifndef __IASMRX__ #error This file is only intended to be included from the FreeRTOS IAR port layer assembly file.#endif/* The interrupt priority used by the kernel itself for the tick interrupt andthe pended interrupt. This would normally be the lowest priority. */#define configKERNEL_INTERRUPT_PRIORITY 1/* The maximum interrupt priority from which FreeRTOS API calls can be made.Interrupts that use a priority above this will not be effected by anything thekernel is doing. */#define configMAX_SYSCALL_INTERRUPT_PRIORITY 4#endif /* PRIORITY_DEFINITIONS_H */