こんにちは。NoMaYです。今首を傾げているのですが、以下のドキュメントによると、e2 studio v7.5.0ではAmazon FreeRTOSプロジェクトに於いてスマートコンフィグレータでRTOS Objectコンポーネントというものが使用出来る/存在するらしいのですが、これは単なるFreeRTOSプロジェクトでは使用出来ない/存在しないものなのでしょうか?(スマートコンフィグレータウィンドウの、コンポーネントタブ上に表示されない&コンポーネント追加ダイアロにも表示されない、ので、そうなのかな、とは思っているのですが、Amazon FreeRTOSプロジェクトとFreeRTOSプロジェクトで、このような部分で違っているのが意外でしたので、、、)e2 studio 7.5.0 Release Notewww.renesas.com/jp/ja/doc/products/tool/doc/016/r20ut4556ee0101-e2studio.pdfPage 17 of 72「New Amazon FreeRTOS Configuration user interface provide within e2 studio 7.5 featuring:● Imported FreeRTOS project with pre-loaded FreeRTOS Components (Object, Kernel and Amazon Libraries).略o FreeRTOS Object configuration: allow user to be able to create, configure multiple FreeRTOS objects using GUI (Tasks, Semaphores, Queues, Software Timers, Event Groups, Message Buffers, Stream Buffers)o Create/Remove FreeRTOS Objects with user friendly UI.略」ちなみに、プロジェクトの生成では、コンパイラはCC-RX V3.01、デバイスはR5F565NEDxFP、に設定して試しました。
シェルティさん、こんにちは。NoMaYです。ポートレイヤに"RX"を新設してデモプロプログラムでそれを使用するソースコードに変更してみました。FreeRTOSポートレイヤ側github.com/renesas/FreeRTOS-Kernel/tree/b5c50f4fda0d49ac8ecdc9239eb9f337c0305e4c/portable/GCC/RX/IAR/RX/Renesas/RX/FreeRTOSデモプログラム側github.com/renesas/FreeRTOS/tree/ff999df66e59387aba3e194bbebe881809feca1c/FreeRTOS/Demo/RX100_RX130_TB_GCC_e2studio/RX100_RX130_TB_IAR_e2studio_EWRX/RX100_RX130_TB_Renesas_e2studio_CS+/RX200_RX231_TB_GCC_e2studio/RX200_RX231_TB_IAR_e2studio_EWRX/RX200_RX231_TB_Renesas_e2studio_CS+/RX600_RX65N_TB_GCC_e2studio/RX600_RX65N_TB_IAR_e2studio_EWRX/RX600_RX65N_TB_Renesas_e2studio_CS+/RX700_RX72N_EnvisionKit_GCC_e2studio/RX700_RX72N_EnvisionKit_IAR_e2studio_EWRX/RX700_RX72N_EnvisionKit_Renesas_e2studio_CS+/