在e2 studio工程里,有没有把一个外部xx.bin文件或者超大const数组指定编译到0x6000 0000地址范围内的方法?
你好billy, 使用Jlink是可以向RA系列MCU的外部QSPI烧录数据的,具体大小和烧录方法可以参考此文档
J-Link Multiple Flashloader - SEGGER Wiki
Tips:只有使用P305~P310的QSPI 可以使用Jlink烧录 (Only P305-P310 are currently supported by the J-Link driver to flash…
Tips:只有使用P305~P310的QSPI 可以使用Jlink烧录 (Only P305-P310 are currently supported by the J-Link driver to flash the QSPI.)