请问仿真监控占用的RAM的具体位置是在哪里?

G13系列芯片规格书上"Stack area for debugging",这4个字节具体位置是在哪里?是运行时一直在变化吗,还是编译后就固定一个地方?

规格书上描述的是:

Since this area is allocated immediately before the stack area, the address of this area varies depending on

the stack increase and decrease. That is, 4 extra bytes are consumed for the stack area used.

When using self-programming, 12 extra bytes are consumed for the stack area used.

Parents Reply Children
No Data