我更新了2023-04的e2studio,QE for Capactive touch是外置版本的,并不在e2studio,我导入工程到外置版本的QE for Capactive touch中start tuning时显示没法连接,用e2-cube2连接RX140,也试过RA2L1的也是无法连接。
请问您使用的是否是EZ-CUBE2,如果是,该型号的仿真器只能仿真RL78和RX系列的产品,不能仿真RA系列的产品,目前EZ-CUBE2已经停产
您当前的错误提示是未连接上串行接口,请检查一下仿真设置,RX140的仿真接口为Fine接口,串口可以用于通过RFP来进行编程
目前EZ-CUBE3已经量产,该仿真器可以仿真瑞萨目前所有系列的MCU
另外,QE for Capacitive Touch可以集成到E2 Studio中,在E2 Studio安装过程中可以选择安装,也可以通过 Renesas Views --> Renesas Software Installer来安装
1、RA的我没有用EZ-CUBE,开发板上有JLINK。2、RX140我连接的应该没有错误,,因为我用e2studio2022-10版本可以tuning。3、e2studio2023-04版本我安装过几次,每一次都选中了capactive工具,实际上安装出来并没有cap touch main的调试界面,但是实际上看安装细节显示已安装,所以我只能下载外置版本,但是外置版本使用不方便,而且出现上述连接不成功的现象。4、我用2022-10版本的captouch main调试界面是plung in版本的。5、目前我试过一些方法都没法安装进去
2023-10版的QE for Capacitive Touch 改界面了
你好 我这画面调出来就是空白
这种现象和Windows相关,您用的系统是Win10吗?
可以试试两个方法:
1. 重装Window10,有用户重装后就可以正常使用了
2. 删除这个QE的版本,重新装一个较低版本试试
在 Help --> About e2 studio --> Installation Details --> Installed Software
选中 Renesas QE for Capacitive Touch
然后删除
装 QE V3.1.0版本即可
Please download files from the following URL:<https://upload.hdedrive.com/ui/renesas.com/dl/SB1684486381-29c8f248-9164-4197-822b-e84ee3f9a845>
* This URL requires guest identity verification as well as download password authentication.Once the identity verification passed, the verification step can be skipped for up to 30 days in the same browser.
Download Password: APJG9!G72snb
This URL will expire on June 2, 2023 4:53 PM (UTC+08:00)
通过 Help --> Install New Software 来进行安装
QEV3.1.0是否支持RL78/G22,我是因为想用G22所以才安装最新的e2stuido,
G22 需要 QE V3.2.0版才行
IDE Ver 2023-01就行
请问2023-01是否有qe for capactive touch main调试界面
安装QE后都有,只是版本不同的名称不同,看您安装那个版本的QE
但是workflow那个我电脑显示不出来,captouch main那个我电脑才能用......
只有QE V3.2及以上的版本才能支持G22,您的这个问题我们有个别客户遇到过,这个问题应该和Windows相关,最后重装了Win10系统才解决