Questions about ECM

Hi,

      The chip I used was RH850-U2A, and I wanted to use ECM to monitor the DMA module. When I generated the ECM module using the latest version of SmartConfigurator, I selected an Error source sDMAC Transfer Error, number 182, and enabled the interrupt generation.
       Analyzing the generated code, I had two doubts:
1. I found that it only configured the ISCFG register to select the interrupt type, but did not configure the INCFG register, which means that the interrupt generation is not enabled
2. I do not want to use External Error Input0-3, numbered 183-187, but it is always configured with two pins ERRORIN0 and ERRORIN1, and I did not find the corresponding configuration in the ECM configuration

 Thanks

 Yin