Hi,
I used the Davinci Configurator tool to generate the configuration code for each module of MCAL. The MCAL version used before was the officially provided software package 43.02.00. I tried to use MCAL 43.03.00 and continued the previous configuration. The configuration code of all modules except CAN Everything can be generated normally, but CAN reported the following error:
ERR000023: The macro definition for macro is not found in <.\device\dr7f02301_0.h> device specific C Header File(s)
Thanks
Yin
Which part number do you use for your solution?