使用RSK+RZT2M开发板,EWARM编译环境,FSP1.0.0。用自带的 Jlink OB调试,无法进入main()函数,始终在system_init()函数

1.硬件环境:RSK+RZT2M开发板,主芯片R9A07G075M24GBG;使用RSK自带 Jlink OB调试(USB线连接J10),J9断开

2.软件环境:IAR 9.30,FSP1.0.0

3.按照r01an6434ej0105-rzt2-rzn2-fsp-getting-started.pdf中依次设置如下

SWX-1 SWX-2 SWX-3 SWX-4 SWX-5 SWX-6 SWX-7 SWX-8 SWX-9 SWX-0
SW4 ON OFF ON ON ON OFF ON OFF
SW5 OFF OFF ON OFF ON OFF OFF OFF ON OFF
SW6 OFF OFF OFF OFF OFF OFF OFF OFF OFF OFF

4.按照5.3.2Create a New Project 新建了FSP_Project,BSP内容如下:

5.IAR界面中option设置

6.build成功后,单击Down and Debug,出现如下界面

单击break后,

再点击GO,会有Warning提示

在main()函数中打断点,程序无法进入main()。

7.根据以上现象得出,程序一直在system_init()函数中的第1句运行,无法进入到main函数

8.有大神能解答一下吗。感谢!