基本情况介绍
给电池充电时,断开输入端停止充电,理论上输入电压会降低直至0V,但实际测得输入电压会一直保持不会降落至0V,是电池在向输入端反向供电。该现象不符合期望,我尝试了如下方案均无法解决问题:
问题现象测试波形如下
放大的图片如下,可以看见反向供电操作约400mS循环一次,输入电压和输出电流的波动很大。模块先反向供电,然后再正向充电,紧接着又反向供电。
请问在该应用中,断开输入时,如何让模块不反向供电,使输入电压降为0V。
我将下拉电阻改为47K设置成diode emulation mode,测试还是有相同的问题。查询了VCROSS=2mV,采样电阻用的0.005R,换算成电流大概在0.4A,我将输入端加入20R的负载,确定模块不会反向供电了,但是实际应用中不可能在输入加入这么大的耗电的负载。分析波形,看出模块在反复的正反向切换,蓝色波形的输入电压在10V时EN脚欠压保护,尝试在EN脚加入一个电容,以延时EN脚的电压随输入电压的变化…
I have the same problem. How can I solve it