Renesas Community
Search Community
User
Join or sign in
Site
Search Community
User
Renesas Engineering Community
FAQ
HELP
More
Cancel
团体和论坛
English Community
Japanese Community
More
Cancel
中文论坛
团体和论坛
Vault Archive
2020 NUEDC AITIC
More
Cancel
2020 NUEDC AITIC
2020NUEDC交流讨论区
imple ISP with background subtraction数据手册中参数
2020NUEDC交流讨论区
Notice-公告
Materials-参考资料
Tags
More
Cancel
New
Replies
5 replies
Subscribers
4 subscribers
Views
868 views
Users
0 members are here
Options
Share
More
Cancel
Related
imple ISP with background subtraction数据手册中参数
剑泪
over 3 years ago
dst2是背景模型的输入地址呢,还是输出地址呢?
这个和mean_img_init参数的设置有关嘛?
Parents
Renesas-AE
over 3 years ago
这个地址既作输入也作输出。
首先这个库的作用之一是根据【当前帧】和【历史帧】的差异找到运动的目标。
src指向【当前帧】,这个你是理解的。
dst2需要指向一块空的专用的buffer,称为【历史帧】。
在camera捕获第一帧图像的时候,【历史帧】是空的,此时需要给mean_img_init设置为0。
之后的每一帧图像,【历史帧】都不为空,此时mean_img_init固定写1就可以了。
Cancel
Up
0
Down
Reply
Cancel
剑泪
over 3 years ago
in reply to
Renesas-AE
非常感谢您的解答,我已经理解了这个参数的含义。
但是调试程序还是出现了一些问题,灰度显示的dst3没有问题,但是检测运动的二值化dst1却一直是黑的。我的参数设置如下:
历史帧初始化,参数设置如下:
p_input_bufadr = R_BCD_CameraGetFrameAddress(frame_buf_id);
R_MMU_VAtoPA((uint32_t)p_input_bufadr, &(param.src)); /* Convert pointer to uint32_t */
param.dst2 = mode_buffer[0];
param.width = R_BCD_CAMERA_WIDTH;
param.height = R_BCD_CAMERA_HEIGHT;
param.area1_offset_x = 0;
param.area1_offset_y = 0;
param.area1_width = R_BCD_CAMERA_WIDTH;
param.area1_height = R_BCD_CAMERA_HEIGHT;
param.area2_offset_x = 0;
param.area2_offset_y = 0;
param.area2_width = 0;
param.area2_height = 0;
param.area3_offset_x = 0;
param.area3_offset_y = 0;
param.area3_width = 0;
param.area3_height = 0;
param.component = 0x001; /* Accumlate ON */
param.bias_r = 0x00;
param.bias_g = -16;
param.bias_b = -16;
param.gain_r = 0x1D48;
param.gain_g = 0x123D;
param.gain_b = 0x1CCC;
param.blend = 0x000;
param.strength = 50;//Sharpening filter emphasis value (0 to 255)
param.coring = 50; //Sharpening filter coring value (0 to 255)
param.gamma = 0; //1: Perform gamma correction;0: Do not perform gamma correction
param.table = 0;
param.mean_img_init = 0; //1: The background model is initialized. 0: The background model is not initialized.
param.alpha = 0; //The weight of input image at the time of updating the background model (0 to 255)
param.threshold_latest = 50; //Binarization threshold for input image (0 to 255)
param.threshold_diff = 30; //Binarization threshold of the difference image between the input image and background
进入循环后,参数设置(改变了的)如下:
p_output_bufadr = R_BCD_LcdGetVramAddress();
R_MMU_VAtoPA((uint32_t)p_output_bufadr, &(param.dst1)); /* Convert pointer to uint32_t */
param.dst2 = mode_buffer[0];
R_MMU_VAtoPA((uint32_t)ave_result, &(param.accumulate)); /* Convert pointer to uint32_t */
param.dst3 = param.dst1+R_BCD_CAMERA_WIDTH*R_BCD_CAMERA_HEIGHT;
param.mean_img_init = 1; //1: The background model is initialized. 0: The background model is not initialized.
Cancel
Up
0
Down
Reply
Cancel
Renesas-AE
over 3 years ago
in reply to
剑泪
你的代码里边,dst1做了地址转换,但是dst2和dst3都没做,可能是一个隐患。
再一点是,dst2初始化一次之后,循环中不需要重新赋值了,毕竟地址不会变。
另外,你拿到了LCD的显示buffer地址给了dst1,这一步没有问题;
然后把上述地址做了一帧的偏移给了dst3,这一步我不太明白,你是想让dst3指向哪里?
Cancel
Up
0
Down
Reply
Cancel
剑泪
over 3 years ago
in reply to
Renesas-AE
非常感谢,关于dst3的指向,我是通过实验理解的,可能有误。我想要在一个显示屏上分屏输出两个图像,第一个图像的地址是lcd的显示buffer,第二个就是做一帧偏移之后得到的。关于这一点,我是在hsv detection里面实验得到的(主要原因是我按照数据手册把dst3赋值为0,显示屏关于dst3的那个半屏无法消失,我也不知道应该通过什么方式给dst3赋值)。
我按照您的意见,修改程序后,结果还是没有变化,可能是dst3的问题吗?dst3应该怎么设置啊?
Cancel
Up
0
Down
Reply
Cancel
Renesas-AE
over 3 years ago
in reply to
剑泪
你试着单独给dst3一块buffer,看看里边的数据对不对。
或者把LCD的显示buffer给了dst3单独做个测试。
Cancel
Up
0
Down
Reply
Cancel
Reply
Renesas-AE
over 3 years ago
in reply to
剑泪
你试着单独给dst3一块buffer,看看里边的数据对不对。
或者把LCD的显示buffer给了dst3单独做个测试。
Cancel
Up
0
Down
Reply
Cancel
Children
No Data