你好,我最近在将我的14580工程移植到14531上,目前发现一个问题,DA14531的MTU需要修改哪些内容才能正确完成呢?我按照14580的修改方式,修改了user_config.h中的.max_mtu = 67, //***+3; .max_txoctets = 251,;.max_txtime = 2120,;da1458x_config_advanced.h中的CFG_MAX_TX_PACKET_LENGTH,CFG_MAX_RX_PACKET_LENGTH也均设置为251;可是我实测发现当我想通过ble调试软件写入cmd至da14531时,仍然最大只能写入20字节数据,我还应该修改哪些?
你好,正如我开始所说,这个参数值,我已经修改了,但是仍然无法发送超过20字节的内容至DA14531。14580的程序里,我修改这里是可以的,14531是否有什么其他的改动地方呢?