I have two da14580 one is advertising and another is listening.
If the two Da14580 know each other device name or advertiser address, is there anyway for the two to get connected in a quick way?
Can I use app_connect directly without scanning?
Thanks
Benjamin
Yes, you can try to directly connect to a device with known address