はじめまして、初めて投稿させて頂きます。現在、RXシリーズの使用を検討しているのですが、使用したい用途として、シリアル通信(RS485等)を複数同時に動かそうとしております。RXマイコン(例としてRX63Nの144pin)のデータシートを確認しましたところ、SCIは13チャネル(SCIc x 12、SCId x 1)が利用可能と記載されておりましたが、pin割り当てを確認しましたところ、いくつかのSCI用のpinが同じpin上に重なっているようでした。例)pin No.25:SCK6/SCK0/USB0_DPRPDpin No.82:SCK4/SCK6/ET_RX_ER/RMII_RX_ERもし上記のSCK6とSCK0/4のようにどれかと重複していて同時に使用できないような場合、同時に(独立して)使用できる最大数というのはいくつになるのでしょうか?そのような情報はどこかに記載されておりますでしょうか?【参照データシート】https://www.renesas.com/us/en/doc/products/mpumcu/doc/rx_family/r01ds0098ej0180_rx63n631.pdfp.51以上、マイコン選びに慣れていませんが、ご指南のほど宜しくお願い致します。