こんにちは。NoMaYです。別スレッド『Amazon AWSのFreeRTOS Kernel Developer GuideのサンプルコードをRenesas RX SimulatorのDebug Consoleで試せるようにしてみた』で気付いたことですが、FreeRTOSでは、ポートレイヤーの実装に内蔵周辺のソフトウェア割り込み機能(これはCPUのソフトウェア割り込み命令のことでは無いです)を使用することで、素朴に簡単に割り込みルーチンからFreeRTOS APIを呼び出せるようになることに気付きました。そこで、FreeRTOS v10.2.1 RL78ポートレイヤーをそのように改変してみました。以下、プロジェクトのファイル一式です。(CC-RL版はCS+ V8.01/e2 stuiod v7.40+CC-RL V1.02でビルド(e2 studio用.project/.cproject等を同梱))(GNURL78版はe2 studio v7.40+GNURL78 2019q2(4.9.2.201902)でビルド)(共にzipファイルをe2 studioに直接インポート可能) プロジェクト構造は極力RX版と同じにしてあります。([追記] すみません。以下に含まれるMAPファイルが別のものでした。タスク側のクリティカルセクションが以前のままのものでした。この投稿の末尾に追加したMOTファイルのzipファイルには訂正版を入れてあります。)sim_rl78_freertos_full_demo_ccrl_c_csplus_20190705.zip 628KBsim_rl78_freertos_full_demo_gnurl78_c_e2v740_20190705.zip 582KBそのスレッドに投稿していたRL78ポートレイヤー(これもFreeRTOS v10.2.1 RL78ポートレイヤーを改変したものです)では、割り込みルーチンからFreeRTOS APIを呼び出すには以下のような特別なおまじないを記述する必要がありました。(以下はCC-RLの場合のものですがGNURL78でも同様です。)
#pragma interrupt r_intc3_interrupt(vect=INTP3)/* Start user code for pragma. Do not edit comment generated here */R_PRAGMA_FREERTOS_INTERRUPT(r_intc3_interrupt)#define r_intc3_interrupt _r_intc3_interrupt/* End user code. Do not edit comment generated here */
そのスレッドにはRXポートレイヤーの改変についても投稿していたのですが、その時、最初に書いたことに気付きました。RL78の内蔵周辺には専用のソフトウェア割り込み機能はありませんが、以下のハードウェアマニュアルに記載されている通り、プログラムで割り込み要求フラグをセットすると割り込みを発生させることが出来ますので、実質的に任意の空き割り込みをソフトウェア割り込み機能として使うことが出来ます。(今回は、とりあえず、ウォッチドッグタイマのオーバフロー時間の75%到達のインターバル割り込みを使用してみました。) RL78/G13 ユーザーズマニュアル ハードウェア編からの抜粋www.renesas.com/ja-jp/doc/products/mpumcu/doc/rl78/r01uh0146jj0340_rl78g13.pdfなお、今回のRL78ポートレイヤーの改変で、先ほどの特別なおまじないを記述する必要は無くなりますが、割り込みルーチンからFreeRTOS APIを呼び出してブロック解除待ちタスクをブロック解除する場合のタスク切り替えの遅延時間が以下のRenesas RL78 SimulatorのSimulator GUIの画面コピーのように数十クロックほど(32MHz動作では600nsほど)延びます。(以下はCC-RLの場合のものですがGNURL78でも同様(ただし数百nsほど長い)です。) ちなみに、タスク側のクリティカルセクション(その区間では割り込み禁止となる)への出入りによるタイミングへの影響を避ける為、今回はクリティカルセクションとして扱うことしていませんので、以下の画面コピーでは別スレッドの画面コピーよりもポート出力トグルの速さが速くなっています。今回の改変前:今回の改変後:以下、今回のRL78ポートレイヤの改変内容です。コメントの訂正や不要になったルーチンの削除は省略しています。(以下はCC-RLの場合のものですがGNURL78でも同様です。)src/FreeRTOS/Source/portable/Renesas/RL78/portmacro.h今回の改変前:
/* Task utilities. */#define portYIELD() __brk()#define portYIELD_FROM_ISR( xHigherPriorityTaskWoken ) if( xHigherPriorityTaskWoken ) vTaskSwitchContext()#define portNOP() __nop()
今回の改変後: 赤文字行を追加/変更
#include "iodefine.h"
/* Task utilities. */#define portYIELD() do{ WDTIIF = 1; } while (0)#define portYIELD_FROM_ISR( xHigherPriorityTaskWoken ) if( xHigherPriorityTaskWoken ) portYIELD()#define portNOP() __nop()
src/FreeRTOS/Source/portable/Renesas/RL78/port.c今回の改変後: 赤文字行を追加
BaseType_t xPortStartScheduler( void ){ /* Setup the hardware to generate the tick. Interrupts are disabled when this function is called. */ configSETUP_TICK_INTERRUPT(); /* Setup the hardware to generate the yield interrupt. */ WDTIPR1 = 1; WDTIPR0 = 1; WDTIMK = 0; /* Restore the context of the first task that is going to run. */ vPortStartFirstTask(); /* Execution should not reach here as the tasks are now running! */ return pdTRUE;}
src/FreeRTOS/Source/portable/Renesas/RL78/portasm.asm今回の改変前:
_vPortYield: portSAVE_CONTEXT ; Save the context of the current task. call@ _vTaskSwitchContext ; Call the scheduler to select the next task. portRESTORE_CONTEXT ; Restore the context of the next task to run. retb
_vPortYield .VECTOR 0x7E
今回の改変後: 赤文字行を変更
_vPortYield: portSAVE_CONTEXT ; Save the context of the current task. call@ _vTaskSwitchContext ; Call the scheduler to select the next task. portRESTORE_CONTEXT ; Restore the context of the next task to run. reti
_vPortYield .VECTOR 0x04
以下、今回のタスク側のプログラムです。先ほど書いた通り、今回は各タスクのポート出力をトグルさせる部分をクリティカルセクションとして扱うことしていません。(なお、src/frtos_config/FreeRTOSConfig.hの#define FREERTOS_USER_MAIN 0の行で0→1の変更を行うことで以下が実行されるようになります。)src/user_main.c
void main_task(void *pvParameters){ (void) pvParameters; while (1) { P1_bit.no6 = !P1_bit.no6; }}void second_task(void *pvParameters){ (void) pvParameters; while (1) { P1_bit.no5 = !P1_bit.no5; }}void third_task(void *pvParameters){ (void) pvParameters; while (1) { P1_bit.no4 = !P1_bit.no4; }}void intp3_task(void *pvParameters){ (void) pvParameters; R_INTC3_Start(); LED_INIT(); while (1) { xSemaphoreTake( xSemaphoreINTP3, portMAX_DELAY ); LED_BIT = !LED_BIT; }}
[追記]MOTファイルsim_rl78_freertos_full_demo_ccrl_c_csplus_20190705_mot.zip 2019/07/12追加sim_rl78_freertos_full_demo_gnurl78_c_e2v740_20190705_mot.zip 2019/07/24追加
こんにちは。NoMaYです。#4連投の2つ目です。今回、先日このスレッドに投稿したFreeRTOSのタスク通知のAPI関数を使用する時の小技に関して、以下のラッパー関数を自作してみました。(小技に関する部分を赤文字にしています。)src/frtos_startup/freertos_start.c
void vTaskNotifyGiveFromISR_R_Helper(TaskHandle_t *pxTask){ if (NULL != *pxTask)[ { BaseType_t sHigherPriorityTaskWoken = pdFALSE; /* Notify the task that the interrupt/callback is complete. */ vTaskNotifyGiveFromISR( *pxTask, &sHigherPriorityTaskWoken ); /* There are no interrupt/callback in progress, so no tasks to notify. */ *pxTask = NULL; portYIELD_FROM_ISR( sHigherPriorityTaskWoken ); }} /* End of function vTaskNotifyGiveFromISR_R_Helper() */ TaskHandle_t xTaskGetCurrentTaskHandle_R_Helper(void){ /* Ensure the calling task does not already have a notification pending. */ ulTaskNotifyTake( pdTRUE, 0 ); /* Return the handle of the calling task. */ return xTaskGetCurrentTaskHandle();} /* End of function xTaskGetCurrentTaskHandle_R_Helper() */
なお、併せて、API関数呼び出しの簡略化の為に(といっても引数を1つ省略する為だけなのですが)、以下のラッパー関数も作成しています。src/frtos_startup/freertos_start.c
uint32_t ulTaskNotifyTake_R_Helper(TickType_t xTicksToWait){ /* Wait to be notified that the interrupt/callback is complete. */ return ulTaskNotifyTake( pdTRUE, xTicksToWait );} /* End of function ulTaskNotifyTake_R_Helper() */
LED1タスクのソースは以下の通りです。今回はFreeRTOSのAPI関数(のラッパー関数)をタスク側ソースではなくコード生成側ソースで呼ぶようにしています。(コード生成側ソースの関数を呼び出している箇所を青文字にしています。)src/frtos_skeleton/task_LED1.c
void task_LED1(void * pvParameters){/* ...略... */ INTERNAL_NOT_USED( pvParameters ); R_INTC0_Start(); LED1 = LED_OFF; for (;;) { U_INTC0_Wait(); /* Remove mechanical switch chattering */ vTaskDelay( SW1_REMOVE_CHATTERING_PERIOD_MS ); if (SW1_PUSH == SW1) { if (true == g_task_CONIO_error) { /* Clear error */ g_task_CONIO_error = false; } else { /* Toggle LED1 */ LED1 = ~LED1; } } }/* ...略... */}
コード生成された外部割込み処理のユーザ記述部のソースは以下の通りです。(FreeRTOSのAPI関数(のラッパー関数)を呼び出している箇所を赤文字にしています。)src/r_cg_intc.c
/* Start user code for adding. Do not edit comment generated here */...略...void U_INTC0_Wait(void){ g_intc0_task = xTaskGetCurrentTaskHandle_R_Helper(); /* Wait for a notification from the interrupt/callback */ ulTaskNotifyTake_R_Helper( portMAX_DELAY );[1行}/* End user code. Do not edit comment generated here */
src/r_cg_intc_user.c
void r_intc0_interrupt(void){ /* Start user code. Do not edit comment generated here */ vTaskNotifyGiveFromISR_R_Helper( &g_intc0_task ); /* End user code. Do not edit comment generated here */}