你好,
同一个RL78工程,用E1能够正常调试,换E2 lite后会报以下错误:
[Direct Error Cause]No response from the emulation CPU. Please confirm the signal of the CLOCK or RESET,WAIT and so on.(E1200416)
是需要进行什么设置吗
CS+ V8.08.00 Integrated Development Environment User's Manual: Message (renesas.cn)
您好,请问上述问题解决没,我使用E2遇到了同样的问题
解决了,
我是这样接的:
VDD(PIN8)
GND(PIN2、PIN12、PIN14并联在一起作为GND)
TOOL0(PIN5)
RESET(PIN10、PIN13并联在一起作为RESET)