問一下DA7218的問題

我現在想要的功能:輸出數據到另一個mcu

mic input : 2個differential連接的mic

mcu master DAI

mclk : 3 MHz , sample rate:大概12kHz(因為是12M crystal除出來的)

i2s data type , 16bit word length ,16bit channel length


現在我可以設和讀那個i2c了,比對讀出來的數值也是對的

但是不知道是甚麼問題,有時候會有數據,但micbias只有0.2V左右的輸出

環境聲音加大也沒有影響到數值高低

但用手碰mic會干擾到提高輸出

有時候更加是沒有數據 micbias沒有輸出

我設定完system也沒有active

下面是我用canvas gui設好再抄出來,嘗試把所有寄存器都設一次的設定
但是還是不行,麻煩看看有甚麼問題

(P.S. 因為剛才發現用canvas gui抄的好像有點問題,修改了一下)

現在情況是左聲道數值在-1200左右,右聲道是在個位數左右

但mic bias1跟2依然沒有反應

會不會是input filter設定問題?
因為我是看著datasheet 選1L(Left)+2L(Right)的

再更新一次

現在一邊channel 是負900-1400 另一邊是正900-1400


   i2c_write_reg(0x09, 0x80);//software reset
    i2c_write_reg(0x10, 0x00);//i2c set no timeout
    i2c_write_reg(0x00, 0x01);//System active
    i2c_write_reg(0x01, 0x01);//i2c repeat mode
    i2c_write_reg(0x0B, 0x33);//12kHz sample rate on adc and dac
    i2c_write_reg(0x0C, 0x02);//resync dai ,auto resynce , no free run (if adc feeding to dac direct set 1 to bit 0)
    i2c_write_reg(0x0D, 0x00);//gain ramp speed
    i2c_write_reg(0x14, 0xFC);//input enable adcl12/r12 / mic1/2 , bit 0 submit
    i2c_write_reg(0x15, 0x0D);//output disselect hpl/r ,  bit 0 submit
    i2c_write_reg(0x18, 0xA0);//in 1L filter enable
    i2c_write_reg(0x19, 0xA0);//in 1R filter enable
    i2c_write_reg(0x1A, 0xA0);//in 2L filter enable
    i2c_write_reg(0x1B, 0xA0);//in 2R filter enable
    i2c_write_reg(0x20, 0x40);//DAC_L disable
    i2c_write_reg(0x21, 0x40);//DAC_R disable
    i2c_write_reg(0x24, 0x00);//output high pass , voice filter disable
    i2c_write_reg(0x25, 0x77);//default value 5 band eq(band 1 2)
    i2c_write_reg(0x26, 0x77);//default value 5 band eq(band 3 4)
    i2c_write_reg(0x27, 0x07);//disable 5 bnad eq ;default value 5 band eq(band 5)
    i2c_write_reg(0x28, 0x40);//5-stage biquad disable and mute
    i2c_write_reg(0x29, 0x00);//5-stage biquad default data
    i2c_write_reg(0x2A, 0x00);//5-stage biquad default addr
    i2c_write_reg(0x2C, 0xA8);//enable mixin_1
    i2c_write_reg(0x2D, 0x0F);//mixin_1 max gain
    i2c_write_reg(0x2E, 0xA8);//enable mixin_2
    i2c_write_reg(0x2F, 0x0F);//mixin_2 max gain
    i2c_write_reg(0x30, 0x00);//disable ALC
    i2c_write_reg(0x31, 0x00);//default value alc
    i2c_write_reg(0x32, 0x00);//default value alc
    i2c_write_reg(0x33, 0x3F);//default value alc
    i2c_write_reg(0x34, 0x3F);//default value alc
    i2c_write_reg(0x35, 0x00);//default value alc
    i2c_write_reg(0x36, 0xFF);//default value alc
    i2c_write_reg(0x37, 0x71);//default value alc
    i2c_write_reg(0x38, 0x00);//default value alc
    i2c_write_reg(0x3C, 0x00);//disable adc gain swap(AGS)
    i2c_write_reg(0x3D, 0x09);//default value AGS
    i2c_write_reg(0x3E, 0x00);//default value AGS
    i2c_write_reg(0x3F, 0x00);//default value AGS
    i2c_write_reg(0x40, 0x00);//default value AGS
    i2c_write_reg(0x44, 0x00);//default value Calibration
    i2c_write_reg(0x4C, 0x00);//defuult value for inputsignal envelope
    i2c_write_reg(0x50, 0x00);//disable level detect to all channel
    i2c_write_reg(0x51, 0x7F);//default value lvl det
    i2c_write_reg(0x54, 0x24);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x55, 0x00);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x56, 0x50);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x57, 0xA3);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x58, 0x31);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x59, 0x11);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x5A, 0x01);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x5B, 0x74);//default value DAC Gain Swap(DGS)
    i2c_write_reg(0x5C, 0x01);//OUTDAI 1L select input 1L
    i2c_write_reg(0x5D, 0x1F);//max gain input filter 1L > OUTDAI 1L
    i2c_write_reg(0x5E, 0x00);//min gain input filter 1R > OUTDAI 1L
    i2c_write_reg(0x5F, 0x00);//min gain input filter 2L > OUTDAI 1L
    i2c_write_reg(0x60, 0x00);//min gain input filter 2R > OUTDAI 1L
    i2c_write_reg(0x61, 0x00);//min gain TONEGEN > OUTDAI 1L
    i2c_write_reg(0x62, 0x00);//min gain INDAI 1L > OUTDAI 1L
    i2c_write_reg(0x63, 0x00);//min gain INDAI 1R > OUTDAI 1L
    i2c_write_reg(0x64, 0x04);//OUTDAI 1R select input 2L
    i2c_write_reg(0x65, 0x00);//min gain input filter 1L > OUTDAI 1R
    i2c_write_reg(0x66, 0x00);//min gain input filter 1R > OUTDAI 1R
    i2c_write_reg(0x67, 0x1F);//max gain input filter 2L > OUTDAI 1R
    i2c_write_reg(0x68, 0x00);//min gain input filter 2R > OUTDAI 1R
    i2c_write_reg(0x69, 0x00);//min gain TONEGEN > OUTDAI 1R
    i2c_write_reg(0x6A, 0x00);//min gain INDAI 1L > OUTDAI 1R
    i2c_write_reg(0x6B, 0x00);//min gain INDAI 1R > OUTDAI 1R
    i2c_write_reg(0x6C, 0x00);//no input select for outfilt_1L
    i2c_write_reg(0x6D, 0x00);//min gain input filter 1L
    i2c_write_reg(0x6E, 0x00);//min gain input filter 1R
    i2c_write_reg(0x6F, 0x00);//min gain input filter 2L
    i2c_write_reg(0x70, 0x00);//min gain input filter 2R
    i2c_write_reg(0x71, 0x00);//min gain TONEGEN
    i2c_write_reg(0x72, 0x00);//min gain INDAI 1L
    i2c_write_reg(0x73, 0x00);//min gain INDAI 1R
    i2c_write_reg(0x74, 0x00);//no input select for outfilt_1R
    i2c_write_reg(0x75, 0x00);//min gain input filter 1L
    i2c_write_reg(0x76, 0x00);//min gain input filter 1R
    i2c_write_reg(0x77, 0x00);//min gain input filter 2L
    i2c_write_reg(0x78, 0x00);//min gain input filter 2R
    i2c_write_reg(0x79, 0x00);//min gain TONEGEN
    i2c_write_reg(0x7A, 0x00);//min gain INDAI 1L
    i2c_write_reg(0x7B, 0x00);//min gain INDAI 1R
    i2c_write_reg(0x7C, 0x00);//no input select for outfilt_2L
    i2c_write_reg(0x7D, 0x00);//min gain input filter 1L
    i2c_write_reg(0x7E, 0x00);//min gain input filter 1R
    i2c_write_reg(0x7F, 0x00);//min gain input filter 2L
    i2c_write_reg(0x80, 0x00);//min gain input filter 2R
    i2c_write_reg(0x81, 0x00);//min gain TONEGEN
    i2c_write_reg(0x82, 0x00);//min gain INDAI 1L
    i2c_write_reg(0x83, 0x00);//min gain INDAI 1R
    i2c_write_reg(0x84, 0x00);//no input select for outfilt_2R
    i2c_write_reg(0x85, 0x00);//min gain input filter 1L
    i2c_write_reg(0x86, 0x00);//min gain input filter 1R
    i2c_write_reg(0x87, 0x00);//min gain input filter 2L
    i2c_write_reg(0x88, 0x00);//min gain input filter 2R
    i2c_write_reg(0x89, 0x00);//min gain TONEGEN
    i2c_write_reg(0x8A, 0x00);//min gain INDAI 1L
    i2c_write_reg(0x8B, 0x00);//min gain INDAI 1R
    i2c_write_reg(0x8C, 0xA0);//DAI enable .channel 1L + 1R ,16 bits/chn, i2s
    i2c_write_reg(0x8D, 0x40);//no TDM mode ,datout driven when required
    i2c_write_reg(0x8E, 0x00);//dai no data offset
    i2c_write_reg(0x8F, 0x00);//dai no data offset
    i2c_write_reg(0x90, 0x00);//DAI Slave , 32bclk per wclk
    
    i2c_write_reg(0x91, 0x00);//pll mode reset
    i2c_write_reg(0x94, 0x20);//by apply to pll integer
    i2c_write_reg(0x91, 0x90);//SRM mode
    
    i2c_write_reg(0x92, 0x00);//pll_frac_top(default value)
    i2c_write_reg(0x93, 0x00);//pll_frac_bot(default value)
    
    i2c_write_reg(0x98, 0x00);//reference oscillator
    i2c_write_reg(0x9C, 0x00);//dac noise gate disable
    i2c_write_reg(0x9D, 0x00);//default value dac noise gate
    
    i2c_write_reg(0x9E, 0x00);//default value dac noise gate
    i2c_write_reg(0x9F, 0x00);//default value dac noise gate
    i2c_write_reg(0xA0, 0x00);//tonegen control
    i2c_write_reg(0xA1, 0x00);//default value tonegen
    i2c_write_reg(0xA2, 0x55);//default value tonegen
    i2c_write_reg(0xA3, 0x15);//default value tonegen
    i2c_write_reg(0xA4, 0x00);//default value tonegen
    i2c_write_reg(0xA5, 0x40);//default value tonegen
    i2c_write_reg(0xA6, 0x00);//default value tonegen
    i2c_write_reg(0xA7, 0x02);//default value tonegen
    i2c_write_reg(0xA8, 0x01);//default value tonegen
    i2c_write_reg(0xAC, 0x8c);//charge pump enable , level = cpvdd/1 , low power disabled
    i2c_write_reg(0xAD, 0x21);//default value charge pump
    i2c_write_reg(0xAE, 0x0E);//default value charge pump
    i2c_write_reg(0xB4, 0x80);//mic 1 amp enable and unmuted
    i2c_write_reg(0xB5, 0x07);//mic 1 max gain
    i2c_write_reg(0xB7, 0x00);//mic 1 input source :differential
    i2c_write_reg(0xB8, 0x80);//mic 2 amp enable and unmuted
    i2c_write_reg(0xB9, 0x07);//mic 2 max gain
    i2c_write_reg(0xBB, 0x00);//mic 2 input source :differential
    i2c_write_reg(0xBC, 0x00);//in 1 , adc high pass ,voice filter disable
    i2c_write_reg(0xBD, 0x00);//in 2 , adc high pass ,voice filter disable
    i2c_write_reg(0xC0, 0x04);//adc 1 anti-alias enable
    i2c_write_reg(0xC1, 0x04);//adc 2 anti-alias enable
    i2c_write_reg(0xC2, 0x00);//adc lvl det ,low power disable
    i2c_write_reg(0xCC, 0x00);//mixout_L disable
    i2c_write_reg(0xCD, 0x01);//min gain mixout_L
    i2c_write_reg(0xCE, 0x00);//mixout_R disable
    i2c_write_reg(0xCF, 0x03);//min gain mixout_R
    i2c_write_reg(0xD0, 0x40);//headphone amp L disable
    i2c_write_reg(0xD1, 0x15);//min gain headphone amp L
    i2c_write_reg(0xD2, 0x40);//headphone amp R disable
    i2c_write_reg(0xD3, 0x15);//min gain headphone amp L
    i2c_write_reg(0xD4, 0x00);//headphone det
    i2c_write_reg(0xD5, 0x00);//headphone differential select
    i2c_write_reg(0xD8, 0x0B);//accessory detect jack
    i2c_write_reg(0xD9, 0x00);//disable auto discharge micbias
    i2c_write_reg(0xDC, 0x08);//master bias enable
    i2c_write_reg(0xE0, 0x00);//io voltage range . 2.5 to 3.6 V
    i2c_write_reg(0xE1, 0x00);//LDO Bypassed
    i2c_write_reg(0xE4, 0x40);//sidetone disable
    i2c_write_reg(0xE5, 0x00);//no select adc for sidetone
    i2c_write_reg(0xE6, 0x1C);//default value sidetone
    i2c_write_reg(0xE8, 0x00);//default value sidetone
    i2c_write_reg(0xE9, 0x00);//default value sidetone
    i2c_write_reg(0xEA, 0x00);//default value sidetone
    i2c_write_reg(0xEB, 0x00);//default value sidetone
    i2c_write_reg(0xED, 0x00);//write 1 to clear hp det /lvl det
    i2c_write_reg(0xEE, 0x00);//event disable
    i2c_write_reg(0xF0, 0x00);//dmic1 disable
    i2c_write_reg(0xF1, 0x00);//dmic2 disable
    i2c_write_reg(0xF4, 0x7F);//max gain in 1L
    i2c_write_reg(0xF5, 0x00);//min gain in 1R
    i2c_write_reg(0xF6, 0x7F);//max gain in 2L
    i2c_write_reg(0xF7, 0x00);//min gain in 2R
    i2c_write_reg(0xF8, 0x00);//min gain out 1L
    i2c_write_reg(0xF9, 0x00);//min gain out 1R
    i2c_write_reg(0xFC, 0x77);//bias1,2 low power mode disable , level 3.0V
    i2c_write_reg(0xFD, 0x11);//enable bias 1,2

Parents Reply Children
  • the staff from the forum has contacted me.
    my mic bias were not powered as i want to use the another bypass mode DA7218 to provide the micbias
    but my i2c communication is messed up. the bypass mode DA7218 was unable to be set to power up the micbias

    now everything should be fine. and i am trying to test out the ALC function if it can fit my need

    my setting above have some mistake though and not need to write the register that no use