Hi,
We are trying to have the image of the DA14580 part of the external microcontroller. In your projects you are saving the image in form of an array - "static const char program_t[IMAGE_SIZE] __attribute__((aligned(***))) = {" Is there a tool to convert a .bin file to such an array? How can I produce the array to store in my microcontroller
sir
你能不用中文描述下你的用法呢?
I am looking for a tool to convert the Intel Hex file into a array, as the array can be used for serial bootloading. As shown in the SDK 5.0.4 example code
SDK 5.0.4\DA1458x_SDK_5.0.4\DA1458x_SDK\5.0.4\projects\host_apps\da1458x\proximity\reporter\include\prox_reporter_ext.h file.
Hi Sir
it's easy to find a Hex2bin, actually our utlitiy: utilities\mkimage, this tool convert a Hex file to bin and then add some header and more info and eventually create a image file, I think you can take use of this project and get what you want
This file gives me an image file. I am looking for formatting the output hex file into a file shown in prox_reporter_ext.h as given in \SDK 5.0.4\DA1458x_SDK_5.0.4\DA1458x_SDK\5.0.4\projects\host_apps\da1458x\proximity\reporter\include
which will be used by the external processor to serially bootload the Dialog chip.
Excerpt of prox_reporter_ext.h file as follows -
#define IMAGE_SIZE 16268 // Image size in bytes
// Image data - MUST BE ALIGNED(***) static const char program_t[IMAGE_SIZE] __attribute__((aligned(***))) = { 0x00,0x98,0x00,0x20,0xa1,0x04,0x00,0x20,0xa9,0x04,0x00,0x20,0xc1,0x04,0x00, 0x20,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, 0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0xd9, 0x04,0x00,0x20,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0xf1,0x04,0x00,0x20, 0xf3,0x04,0x00,0x20,0xab,0x28,0x00,0x20,0x9f,0x29,0x00,0x20,0x0d,0x31,0x03, 0x00,0x8d,0x29,0x00,0x20,0x13,0x29,0x00,0x20,0x8d,0x31,0x03,0x00,0xb1,0x29, 0x00,0x20,0xb9,0x29,0x00,0x20,0xf5,0x04,0x00,0x20,0x4b,0x23,0x00,0x20,0xd1, 0x29,0x00,0x20,0xad,0x31,0x03,0x00,0x57,0x81,0x02,0x00,0xf5,0x04,0x00,0x20, 0xf5,0x04,0x00,0x20,0x93,0x22,0x00,0x20,0xf5,0x04,0x00,0x20,0xf5,0x04,0x00, 0x20,0xf5,0x04,0x00,0x20,0x95,0x20,0x00,0x20,0x99,0x20,0x00,0x20,0x9d,0x20, 0x00,0x20,0xa1,0x20,0x00,0x20,0xa5,0x20,0x00,0x20,0xff,0xff,0xff,0xff,0xff, 0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,
Hi, Vivek,
The tool you need can be easily found online. Check this post for example:
http://www.keil.com/support/docs/2218.htm
Also, please post in the English forum if you're native English speaker :)